<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic settings for ITCM=0 not accepted by mcuxpresso? in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/settings-for-ITCM-0-not-accepted-by-mcuxpresso/m-p/1209830#M12122</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;My project is not using any ITCM and so I want to set that to 0, and instead use all of the flexRAM for DTCM.&lt;/P&gt;&lt;P&gt;But when I try and set ITCM to 0 in the MCU settings window of mcuxpresso, it gives an error saying "Invalid memory configuration. SRAM_ITC has zero size". This is despite the fact that there is 0 usage of this memory region in the project.&lt;/P&gt;&lt;P&gt;How do I set ITCM size = 0 in mcuxpresso please?&lt;/P&gt;&lt;P&gt;thanks!&lt;BR /&gt;-Nick&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 11 Jan 2021 18:14:58 GMT</pubDate>
    <dc:creator>nickwallis</dc:creator>
    <dc:date>2021-01-11T18:14:58Z</dc:date>
    <item>
      <title>settings for ITCM=0 not accepted by mcuxpresso?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/settings-for-ITCM-0-not-accepted-by-mcuxpresso/m-p/1209830#M12122</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;My project is not using any ITCM and so I want to set that to 0, and instead use all of the flexRAM for DTCM.&lt;/P&gt;&lt;P&gt;But when I try and set ITCM to 0 in the MCU settings window of mcuxpresso, it gives an error saying "Invalid memory configuration. SRAM_ITC has zero size". This is despite the fact that there is 0 usage of this memory region in the project.&lt;/P&gt;&lt;P&gt;How do I set ITCM size = 0 in mcuxpresso please?&lt;/P&gt;&lt;P&gt;thanks!&lt;BR /&gt;-Nick&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 18:14:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/settings-for-ITCM-0-not-accepted-by-mcuxpresso/m-p/1209830#M12122</guid>
      <dc:creator>nickwallis</dc:creator>
      <dc:date>2021-01-11T18:14:58Z</dc:date>
    </item>
    <item>
      <title>Re: settings for ITCM=0 not accepted by mcuxpresso?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/settings-for-ITCM-0-not-accepted-by-mcuxpresso/m-p/1209912#M12124</link>
      <description>&lt;P&gt;Hello Nick,&lt;/P&gt;
&lt;P&gt;If you want to have ITCM as zero you would need to actually delete that memory region as you cannot define a memory area with a zero size.&lt;/P&gt;
&lt;P&gt;In some i.MXRT Crossover Microcontrollers like in the i.MX1060, only part of the RAM can be reallocated. You can find more information on the link below:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Reallocating-the-FlexRAM/ta-p/1117649" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Reallocating-the-FlexRAM/ta-p/1117649&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I hope that this helps!&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 23:48:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/settings-for-ITCM-0-not-accepted-by-mcuxpresso/m-p/1209912#M12124</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2021-01-11T23:48:53Z</dc:date>
    </item>
    <item>
      <title>Re: settings for ITCM=0 not accepted by mcuxpresso?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/settings-for-ITCM-0-not-accepted-by-mcuxpresso/m-p/1210426#M12135</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/40799"&gt;@gusarambula&lt;/a&gt;&amp;nbsp;of course, don't know why I didn't think of that! Thank you.&lt;/P&gt;&lt;P&gt;-Nick&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jan 2021 13:54:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/settings-for-ITCM-0-not-accepted-by-mcuxpresso/m-p/1210426#M12135</guid>
      <dc:creator>nickwallis</dc:creator>
      <dc:date>2021-01-12T13:54:10Z</dc:date>
    </item>
  </channel>
</rss>