<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 flexio uart with hardware flow control</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/flexio-uart-with-hardware-flow-control/m-p/1208697#M12088</link>
    <description>&lt;P&gt;Are there any examples/documentation on how to achieve UART with hardware flow control on FLEXIO if it is possible? The SDK examples does not appear to include this&lt;/P&gt;</description>
    <pubDate>Fri, 08 Jan 2021 04:40:48 GMT</pubDate>
    <dc:creator>sheng_cao</dc:creator>
    <dc:date>2021-01-08T04:40:48Z</dc:date>
    <item>
      <title>flexio uart with hardware flow control</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/flexio-uart-with-hardware-flow-control/m-p/1208697#M12088</link>
      <description>&lt;P&gt;Are there any examples/documentation on how to achieve UART with hardware flow control on FLEXIO if it is possible? The SDK examples does not appear to include this&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jan 2021 04:40:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/flexio-uart-with-hardware-flow-control/m-p/1208697#M12088</guid>
      <dc:creator>sheng_cao</dc:creator>
      <dc:date>2021-01-08T04:40:48Z</dc:date>
    </item>
    <item>
      <title>Re: flexio uart with hardware flow control</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/flexio-uart-with-hardware-flow-control/m-p/1209297#M12112</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;One may refer to the application note for it.&lt;/P&gt;
&lt;P&gt;URL:&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12772.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN12772.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it help you. Have a nice day&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 01:42:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/flexio-uart-with-hardware-flow-control/m-p/1209297#M12112</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2021-01-11T01:42:48Z</dc:date>
    </item>
  </channel>
</rss>