<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: External Memory Controller</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/External-Memory-Controller/m-p/1205859#M11978</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;RT1020 SEMC module can run at 166MHz, so the SDRAM should be able to run at 166MHz. But the IO has overshoot problem. It will have EMI/EMC problem if hardware design is not very perfect. It is strongly recommended to follow the hardware development guide.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
    <pubDate>Mon, 04 Jan 2021 07:11:00 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2021-01-04T07:11:00Z</dc:date>
    <item>
      <title>External Memory Controller</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/External-Memory-Controller/m-p/1205702#M11972</link>
      <description>&lt;P&gt;The speed at which EMC connects to SDRAM is different from the description in the RT1020 reference manual and user manual. Which one is correct?&lt;/P&gt;</description>
      <pubDate>Mon, 04 Jan 2021 02:26:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/External-Memory-Controller/m-p/1205702#M11972</guid>
      <dc:creator>13692631114</dc:creator>
      <dc:date>2021-01-04T02:26:40Z</dc:date>
    </item>
    <item>
      <title>Re: External Memory Controller</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/External-Memory-Controller/m-p/1205859#M11978</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;RT1020 SEMC module can run at 166MHz, so the SDRAM should be able to run at 166MHz. But the IO has overshoot problem. It will have EMI/EMC problem if hardware design is not very perfect. It is strongly recommended to follow the hardware development guide.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Mon, 04 Jan 2021 07:11:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/External-Memory-Controller/m-p/1205859#M11978</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-01-04T07:11:00Z</dc:date>
    </item>
  </channel>
</rss>