<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SPI interface with NOR Flash MX25L4006E in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-interface-with-NOR-Flash-MX25L4006E/m-p/1202626#M11799</link>
    <description>&lt;P&gt;Please see attached screen shot:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to send a sequence of bytes from 0x00 to 0x09. It looks like the SPI driver takes the first 4 bytes and send them starting from the MSB byte and then takes the next 4 bytes and so on..&lt;/P&gt;&lt;P&gt;I need to send Byte by Bytes starting either from the MSB byte or LSB bytes in the array. How do I need to set up my SPI to get what I want.&lt;/P&gt;&lt;P&gt;Your help is urgently needed!&lt;/P&gt;</description>
    <pubDate>Mon, 21 Dec 2020 19:43:57 GMT</pubDate>
    <dc:creator>fmabrouk</dc:creator>
    <dc:date>2020-12-21T19:43:57Z</dc:date>
    <item>
      <title>SPI interface with NOR Flash MX25L4006E</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-interface-with-NOR-Flash-MX25L4006E/m-p/1202006#M11768</link>
      <description>&lt;P&gt;I am trying to interface with this LPSPI flash: &lt;A href="https://static6.arrow.com/aropdfconversion/74f71a4d24defb900f21183aac8a0329d8ea28d0/mx25l4006e203v204mb20v1.7.pdf%5C" target="_blank" rel="noopener"&gt;https://static6.arrow.com/aropdfconversion/74f71a4d24defb900f21183aac8a0329d8ea28d0/mx25l4006e203v204mb20v1.7.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;using LPSPI on IMX RT1062. I need to send 256 bytes of data plus 4 bytes of command ( as per page 41 figure 22 of the datasheet). I figured I need to have 2080 bits per frame ( 2080 spi clock cycles): masterConfig-&amp;gt;bitsPerFrame = 2080.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;but this does not seem to work. When I look at the data I want to send on the scope, it appears it somehow changed: not correct&lt;/P&gt;&lt;P&gt;Is it even possible to send a total of 260 bytes in a single transfer? if so please advise how?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://static6.arrow.com/aropdfconversion/74f71a4d24defb900f21183aac8a0329d8ea28d0/mx25l4006e203v204mb20v1.7.pdf" target="_blank" rel="noopener"&gt;https://static6.arrow.com/aropdfconversion/74f71a4d24defb900f21183aac8a0329d8ea28d0/mx25l4006e203v204mb20v1.7.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Sun, 20 Dec 2020 07:07:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-interface-with-NOR-Flash-MX25L4006E/m-p/1202006#M11768</guid>
      <dc:creator>farid_mabrouk</dc:creator>
      <dc:date>2020-12-20T07:07:03Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface with NOR Flash MX25L4006E</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-interface-with-NOR-Flash-MX25L4006E/m-p/1202159#M11778</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;To provide the fastest possible support, I'd highly recommend you refer to the LSPI demo in the SDK library to do that.&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 21 Dec 2020 02:59:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-interface-with-NOR-Flash-MX25L4006E/m-p/1202159#M11778</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2020-12-21T02:59:53Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface with NOR Flash MX25L4006E</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-interface-with-NOR-Flash-MX25L4006E/m-p/1202229#M11786</link>
      <description>&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;I looked at the example code you have for LPSPI and I even implemented SPI interfaces for 4 bytes transfer in the past, I want to know how you send 64 bytes in a single transfer. can you send some psuedo code?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Dec 2020 06:05:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-interface-with-NOR-Flash-MX25L4006E/m-p/1202229#M11786</guid>
      <dc:creator>farid_mabrouk</dc:creator>
      <dc:date>2020-12-21T06:05:02Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface with NOR Flash MX25L4006E</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-interface-with-NOR-Flash-MX25L4006E/m-p/1202626#M11799</link>
      <description>&lt;P&gt;Please see attached screen shot:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to send a sequence of bytes from 0x00 to 0x09. It looks like the SPI driver takes the first 4 bytes and send them starting from the MSB byte and then takes the next 4 bytes and so on..&lt;/P&gt;&lt;P&gt;I need to send Byte by Bytes starting either from the MSB byte or LSB bytes in the array. How do I need to set up my SPI to get what I want.&lt;/P&gt;&lt;P&gt;Your help is urgently needed!&lt;/P&gt;</description>
      <pubDate>Mon, 21 Dec 2020 19:43:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-interface-with-NOR-Flash-MX25L4006E/m-p/1202626#M11799</guid>
      <dc:creator>fmabrouk</dc:creator>
      <dc:date>2020-12-21T19:43:57Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface with NOR Flash MX25L4006E</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-interface-with-NOR-Flash-MX25L4006E/m-p/1203002#M11805</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thanks for your reply.&lt;BR /&gt;According to your statement, you want to continue to transfer a series of data while keeping PCS asserted, isn't my understand right?&lt;BR /&gt;If yes, the LPSPI supports this continuous transfer feature, the below figure shows the continuous transfer state, it indicates the dynamic signals when the MCU run the lpspi_edma_b2b_transfer_master demo.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jeremyzhou_0-1608629411531.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133279i1E9513B1CDE179EA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jeremyzhou_0-1608629411531.png" alt="jeremyzhou_0-1608629411531.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 22 Dec 2020 09:31:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-interface-with-NOR-Flash-MX25L4006E/m-p/1203002#M11805</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2020-12-22T09:31:13Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface with NOR Flash MX25L4006E</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-interface-with-NOR-Flash-MX25L4006E/m-p/1203190#M11812</link>
      <description>&lt;P&gt;Great! I fixed my issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;what is the maximum clock frequency this LPSP peripheral support?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Farid&lt;/P&gt;</description>
      <pubDate>Tue, 22 Dec 2020 18:02:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-interface-with-NOR-Flash-MX25L4006E/m-p/1203190#M11812</guid>
      <dc:creator>fmabrouk</dc:creator>
      <dc:date>2020-12-22T18:02:19Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface with NOR Flash MX25L4006E</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-interface-with-NOR-Flash-MX25L4006E/m-p/1203342#M11817</link>
      <description>&lt;P&gt;Hi, &lt;BR /&gt;Thanks for your reply.&lt;BR /&gt;1) What is the maximum clock frequency this LPSP peripheral support?&lt;BR /&gt;-- The maximum clock frequency of LPSPI is 30 MHz, it mustn't exceed this frequency.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 23 Dec 2020 02:24:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-interface-with-NOR-Flash-MX25L4006E/m-p/1203342#M11817</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2020-12-23T02:24:05Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface with NOR Flash MX25L4006E</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-interface-with-NOR-Flash-MX25L4006E/m-p/1206273#M12001</link>
      <description>&lt;P&gt;Thank you for your help!&lt;/P&gt;</description>
      <pubDate>Mon, 04 Jan 2021 20:52:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SPI-interface-with-NOR-Flash-MX25L4006E/m-p/1206273#M12001</guid>
      <dc:creator>fmabrouk</dc:creator>
      <dc:date>2021-01-04T20:52:58Z</dc:date>
    </item>
  </channel>
</rss>