<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Re: When program link to sdram, download failed</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/When-program-link-to-sdram-download-failed/m-p/1200956#M11725</link>
    <description>&lt;P&gt;Hi huijieshen,&lt;/P&gt;
&lt;P&gt;Please refer to this link.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT/RT1020-SDRAM-and-SWD-debugging-problems/m-p/1057852" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT/RT1020-SDRAM-and-SWD-debugging-problems/m-p/1057852&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
    <pubDate>Thu, 17 Dec 2020 06:02:00 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2020-12-17T06:02:00Z</dc:date>
    <item>
      <title>When program link to sdram, download failed</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/When-program-link-to-sdram-download-failed/m-p/1199513#M11687</link>
      <description>&lt;P&gt;Dear :&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use&amp;nbsp; MCUExpresso which run Linux to debug my RT1052 board. I use on DAPlink to connect my linux&amp;nbsp;computer to the RT1050 board. The problem is as followings:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I can download the my program to RT1052 when I link the code to FlexRAM D-TCM. And I can also debug my code in this case.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &lt;FONT face="arial black,avant garde"&gt;But&lt;/FONT&gt; when I link the code to SDRAM, I downloaded the code to the board, no error reported. But&amp;nbsp;the code doesn't work at all. Of couse I can't debug use the DAPLink yet.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I think the problem may lies in the SDRAM is not initialed. (? Am I correct) .&amp;nbsp; So I try to merge the dcd.c register contents to RT1052_connect.scp. But When I read the dcd. I find it seems that the dcd.c is not just register writing.&amp;nbsp; I can't know code means like&amp;nbsp;&lt;/P&gt;&lt;P&gt;/* #8, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */&lt;BR /&gt;0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;So I think I need help to make me success in downloading code to RT1052 SDRAM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Dec 2020 08:51:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/When-program-link-to-sdram-download-failed/m-p/1199513#M11687</guid>
      <dc:creator>huijieshen</dc:creator>
      <dc:date>2020-12-15T08:51:08Z</dc:date>
    </item>
    <item>
      <title>Re: When program link to sdram, download failed</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/When-program-link-to-sdram-download-failed/m-p/1200956#M11725</link>
      <description>&lt;P&gt;Hi huijieshen,&lt;/P&gt;
&lt;P&gt;Please refer to this link.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT/RT1020-SDRAM-and-SWD-debugging-problems/m-p/1057852" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT/RT1020-SDRAM-and-SWD-debugging-problems/m-p/1057852&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Thu, 17 Dec 2020 06:02:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/When-program-link-to-sdram-download-failed/m-p/1200956#M11725</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2020-12-17T06:02:00Z</dc:date>
    </item>
    <item>
      <title>Re: When program link to sdram, download failed</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/When-program-link-to-sdram-download-failed/m-p/1201736#M11760</link>
      <description>&lt;P&gt;Thank you for your information.&lt;/P&gt;&lt;P&gt;The problem is that I use RT1052 instead of RT1020 so the 1020 connect script is unusable to me.&lt;/P&gt;&lt;P&gt;Some time I can download the code to SDRAM, but when the code runs, the hardware fault will bounce out of the IDE. It will says I will try to access memory address such as 0xfffffffe. So I think the main reason should be in SDRAM is not initialed, So&amp;nbsp; I need a way of transform dcd to connect script.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need to know how to process the things as following when I writing connect script :&lt;/P&gt;&lt;P&gt;/* #2, command: check_any_bit_set, address: SEMC_INTR, value: 0x01, size: 4 */&lt;BR /&gt;0xCF, 0x00, 0x0C, 0x1C, 0x40, 0x2F, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x01,&lt;/P&gt;&lt;P&gt;can I just ignore them.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;</description>
      <pubDate>Fri, 18 Dec 2020 09:33:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/When-program-link-to-sdram-download-failed/m-p/1201736#M11760</guid>
      <dc:creator>huijieshen</dc:creator>
      <dc:date>2020-12-18T09:33:31Z</dc:date>
    </item>
    <item>
      <title>Re: When program link to sdram, download failed</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/When-program-link-to-sdram-download-failed/m-p/1202153#M11777</link>
      <description>&lt;P&gt;Hi huijieshen,&lt;/P&gt;
&lt;P&gt;There is a RT1050_SDRAM_init.scp. You can download from here.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MCUXpresso-Community-Articles/Overview-of-using-the-MIMXRT1050-EVK-B-with-MCUXpresso-IDE/ba-p/1131013" target="_blank"&gt;https://community.nxp.com/t5/MCUXpresso-Community-Articles/Overview-of-using-the-MIMXRT1050-EVK-B-with-MCUXpresso-IDE/ba-p/1131013&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Mon, 21 Dec 2020 02:45:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/When-program-link-to-sdram-download-failed/m-p/1202153#M11777</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2020-12-21T02:45:18Z</dc:date>
    </item>
  </channel>
</rss>