<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMXRT1020EVK booting from SDRAM USB Host not working. in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1020EVK-booting-from-SDRAM-USB-Host-not-working/m-p/1198334#M11636</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer to below link&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-NonCached-Memory-on-i-MXRT/ta-p/1183369" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-NonCached-Memory-on-i-MXRT/ta-p/1183369&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I&amp;nbsp; hope it helps&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
    <pubDate>Sat, 12 Dec 2020 08:46:58 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2020-12-12T08:46:58Z</dc:date>
    <item>
      <title>IMXRT1020EVK booting from SDRAM USB Host not working.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1020EVK-booting-from-SDRAM-USB-Host-not-working/m-p/1198269#M11633</link>
      <description>&lt;P&gt;Hi All, hope you are doing well, I was working with USB (host/device) examples of the SDK of the IMXRT1020EVK, I sucesfully mixed two usb apps host and device type.&lt;/P&gt;&lt;P&gt;I was trying to make a program that can handle both types and can boot from FlexSPI NOR FLash of the EVK, now this is working without problems.&lt;/P&gt;&lt;P&gt;The USB Host detect a pen drive and make a test, and when it starts like device a virtual com port is inicialized.&lt;/P&gt;&lt;P&gt;The idea is to use the same usb program and to generate an image to download in an SD card and then boot from SDRAM of the EVK using MCUBootUtility.&lt;/P&gt;&lt;P&gt;Right now I can sucesfully download an image to SD card and then boot from SDRAM, using DCD file and MCUBootUtillity,&amp;nbsp; that is not a problem.&lt;/P&gt;&lt;P&gt;The problem is that after downloading the usb app into a SD card and booting from SDRAM only the usb device works fine, the usb host has enumeration problems.&lt;/P&gt;&lt;P&gt;The global variables are using the SRAM_DTC region (I read in another post that is important to not use the cacheable region of SRAM).&lt;/P&gt;&lt;P&gt;Why if I run from the external nor flash the usb host works fine, but if I run from SDRAM it not works? (In both cases usb device type works fine).&amp;nbsp;&lt;/P&gt;&lt;P&gt;I will appreciate yours ideas.&lt;/P&gt;&lt;P&gt;Many thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Dec 2020 22:19:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1020EVK-booting-from-SDRAM-USB-Host-not-working/m-p/1198269#M11633</guid>
      <dc:creator>nicolasmuratore</dc:creator>
      <dc:date>2020-12-11T22:19:28Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1020EVK booting from SDRAM USB Host not working.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1020EVK-booting-from-SDRAM-USB-Host-not-working/m-p/1198334#M11636</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer to below link&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-NonCached-Memory-on-i-MXRT/ta-p/1183369" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-NonCached-Memory-on-i-MXRT/ta-p/1183369&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I&amp;nbsp; hope it helps&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Sat, 12 Dec 2020 08:46:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1020EVK-booting-from-SDRAM-USB-Host-not-working/m-p/1198334#M11636</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2020-12-12T08:46:58Z</dc:date>
    </item>
  </channel>
</rss>