<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMXRT1060-EVK CAN-FD transfer example not working, CAN is. in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1060-EVK-CAN-FD-transfer-example-not-working-CAN-is/m-p/1198151#M11623</link>
    <description>&lt;P&gt;Aaaand... The issue is fixed elsewhere on this forum!&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT/CAN-FD-using-MIMXRT1064-EVK-and-PCAN-View-PC-software/m-p/1034847/highlight/true#M7330" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT/CAN-FD-using-MIMXRT1064-EVK-and-PCAN-View-PC-software/m-p/1034847/highlight/true#M7330&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Summary: FD ISO is disabled by default and needs to be manually enabled by editing the driver file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 11 Dec 2020 14:58:42 GMT</pubDate>
    <dc:creator>p_shep</dc:creator>
    <dc:date>2020-12-11T14:58:42Z</dc:date>
    <item>
      <title>IMXRT1060-EVK CAN-FD transfer example not working, CAN is.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1060-EVK-CAN-FD-transfer-example-not-working-CAN-is/m-p/1198137#M11622</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;As title, I have the IMXRT1060 devboard (just the one), trying to get CAN-FD working, and it point blank refuses to.&lt;/P&gt;&lt;P&gt;Got it hooked up to a PCAN device (rather then a 2nd EVK for the transfer example), and can verify the hardware is wired up correctly as I get the one-shot massage through for the CAN example ok.&lt;/P&gt;&lt;P&gt;But when I reconfigure the PCAN for the default 1/2Mbps and try the CAN-FD example, I get nothing.&lt;/P&gt;&lt;P&gt;Further, if I stop the debugger, it's trapped in the while (!txComplete) suggesting that the transfer hasn't actually occurred at all, and not just a bus speed issue.&lt;/P&gt;&lt;P&gt;It seems I'm the only one with this issue, as googling shows no useful results, hence asking here.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Suggestions?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 11 Dec 2020 14:23:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1060-EVK-CAN-FD-transfer-example-not-working-CAN-is/m-p/1198137#M11622</guid>
      <dc:creator>p_shep</dc:creator>
      <dc:date>2020-12-11T14:23:51Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1060-EVK CAN-FD transfer example not working, CAN is.</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1060-EVK-CAN-FD-transfer-example-not-working-CAN-is/m-p/1198151#M11623</link>
      <description>&lt;P&gt;Aaaand... The issue is fixed elsewhere on this forum!&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT/CAN-FD-using-MIMXRT1064-EVK-and-PCAN-View-PC-software/m-p/1034847/highlight/true#M7330" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT/CAN-FD-using-MIMXRT1064-EVK-and-PCAN-View-PC-software/m-p/1034847/highlight/true#M7330&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Summary: FD ISO is disabled by default and needs to be manually enabled by editing the driver file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Dec 2020 14:58:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1060-EVK-CAN-FD-transfer-example-not-working-CAN-is/m-p/1198151#M11623</guid>
      <dc:creator>p_shep</dc:creator>
      <dc:date>2020-12-11T14:58:42Z</dc:date>
    </item>
  </channel>
</rss>