<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: Serial manager - multiple interfaces</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Serial-manager-multiple-interfaces/m-p/1197689#M11613</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Is this intentional?&lt;BR /&gt;-- No, I guess it's still related to the software configuration.&lt;BR /&gt;2) Am I the only one with this requirement?&lt;BR /&gt;-- Yes, it seems like that.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Fri, 11 Dec 2020 00:07:44 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2020-12-11T00:07:44Z</dc:date>
    <item>
      <title>Serial manager - multiple interfaces</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Serial-manager-multiple-interfaces/m-p/1197386#M11607</link>
      <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I have a application for a custom board, and it runs fine with serial_manager for fsl_debug_console or fsl_shell.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But If I register both the USB and the UART Debug Console only the last one registered is actually active.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this intentional? All the code for serial manager is build very modular, so It should not be a big task to allow dual debug/shell interface.&lt;/P&gt;&lt;P&gt;Am I the only one with this requirement?&lt;/P&gt;&lt;P&gt;I have a plan implementing a interface for a network/telnet to the Serial Manager, but if serial manager does not support this, I mus find a different way.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Kasper&lt;/P&gt;</description>
      <pubDate>Thu, 10 Dec 2020 12:00:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Serial-manager-multiple-interfaces/m-p/1197386#M11607</guid>
      <dc:creator>kl</dc:creator>
      <dc:date>2020-12-10T12:00:53Z</dc:date>
    </item>
    <item>
      <title>Re: Serial manager - multiple interfaces</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Serial-manager-multiple-interfaces/m-p/1197689#M11613</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Is this intentional?&lt;BR /&gt;-- No, I guess it's still related to the software configuration.&lt;BR /&gt;2) Am I the only one with this requirement?&lt;BR /&gt;-- Yes, it seems like that.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 11 Dec 2020 00:07:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Serial-manager-multiple-interfaces/m-p/1197689#M11613</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2020-12-11T00:07:44Z</dc:date>
    </item>
  </channel>
</rss>