<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Re: How to create ivt_flashloader.bin?</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-create-ivt-flashloader-bin/m-p/1175171#M10995</link>
    <description>&lt;P&gt;Hi Jason,&lt;/P&gt;
&lt;P&gt;Flashloader runs in RAM. It hasn't IVT or other head.&lt;/P&gt;
&lt;P&gt;The BootROM solidified into the i.MX RT chip does not support programming the flash device and the eFuse register. For the two targets, ,n serial download mode the Flashloader image is downloaded to the i.MX RT internal RAM using SDPHost (communicates with the running BootROM) and takes over the device from the BootROM (by the jump-address command of SDPHost). Then it implements the program process (communicates with the blhost tool).&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please see AN12238 for more detail.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
    <pubDate>Thu, 29 Oct 2020 08:51:24 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2020-10-29T08:51:24Z</dc:date>
    <item>
      <title>How to create ivt_flashloader.bin?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-create-ivt-flashloader-bin/m-p/1175006#M10986</link>
      <description>&lt;P&gt;I imported the flashloader from RT1010 sdk and built the project without any change. Then I converted&amp;nbsp;evkmimxrt1010_flashloader.axf into ivt_flashloader.bin with elftosb.exe. But it didn't work. The .bd file used in elftosb is attached.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 29 Oct 2020 05:24:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-create-ivt-flashloader-bin/m-p/1175006#M10986</guid>
      <dc:creator>jasonedn</dc:creator>
      <dc:date>2020-10-29T05:24:15Z</dc:date>
    </item>
    <item>
      <title>Re: How to create ivt_flashloader.bin?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-create-ivt-flashloader-bin/m-p/1175171#M10995</link>
      <description>&lt;P&gt;Hi Jason,&lt;/P&gt;
&lt;P&gt;Flashloader runs in RAM. It hasn't IVT or other head.&lt;/P&gt;
&lt;P&gt;The BootROM solidified into the i.MX RT chip does not support programming the flash device and the eFuse register. For the two targets, ,n serial download mode the Flashloader image is downloaded to the i.MX RT internal RAM using SDPHost (communicates with the running BootROM) and takes over the device from the BootROM (by the jump-address command of SDPHost). Then it implements the program process (communicates with the blhost tool).&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please see AN12238 for more detail.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Thu, 29 Oct 2020 08:51:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-create-ivt-flashloader-bin/m-p/1175171#M10995</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2020-10-29T08:51:24Z</dc:date>
    </item>
    <item>
      <title>Re: How to create ivt_flashloader.bin?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-create-ivt-flashloader-bin/m-p/1178876#M11125</link>
      <description>&lt;P&gt;Hello Jing,&lt;/P&gt;&lt;P&gt;Thanks for your reply. I built the project "evkmimxrt1010_flashloader" and create the flashloader binary, but it failed to run after downloading with sdphost.exe. It's simple to re-produced it on the RT1010EVK.&lt;/P&gt;&lt;P&gt;1. Build the project&amp;nbsp;"evkmimxrt1010_flashloader".&lt;/P&gt;&lt;P&gt;2. Convert *.axf to *.bin&lt;/P&gt;&lt;P&gt;3. Download it onto SRAM with sdphost.exe&lt;/P&gt;&lt;P&gt;4. Jump to the application and it fails.&lt;/P&gt;&lt;P&gt;My question is how to make the built binary work. I made a new board with RT1010 and the JTAG didn't work so I want to use sdphost.exe to download this application to test. The original ivt_flashloader.bin from NXP did work when it's downloaded. But I want to add some debug information in the example project. But it didn't work even without any changes.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Jason&lt;/P&gt;</description>
      <pubDate>Thu, 05 Nov 2020 17:04:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/How-to-create-ivt-flashloader-bin/m-p/1178876#M11125</guid>
      <dc:creator>jasonedn</dc:creator>
      <dc:date>2020-11-05T17:04:28Z</dc:date>
    </item>
  </channel>
</rss>