<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 1060 API for EMMC in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/1060-API-for-EMMC/m-p/1167375#M10560</link>
    <description>&lt;P&gt;I am trying to use this example on USDHC2, in 8 bit mode so that we can boot from the part. We are testing the hardware of the board, how do I port the example from USDHC1, we have made some changes but I can see nothing on the logic analyser.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;</description>
    <pubDate>Wed, 14 Oct 2020 10:00:37 GMT</pubDate>
    <dc:creator>gredpath</dc:creator>
    <dc:date>2020-10-14T10:00:37Z</dc:date>
    <item>
      <title>1060 API for EMMC</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/1060-API-for-EMMC/m-p/1026068#M6991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN title=""&gt;Hello dear NXP team&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN title=""&gt;There is now an API for the 1060 board for the EMMC modules with examples.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN class="" title=""&gt;Thank you&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2020 13:03:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/1060-API-for-EMMC/m-p/1026068#M6991</guid>
      <dc:creator>sergunionline</dc:creator>
      <dc:date>2020-02-13T13:03:13Z</dc:date>
    </item>
    <item>
      <title>Re: 1060 API for EMMC</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/1060-API-for-EMMC/m-p/1026069#M6992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sergej,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;MCUXpresso SDK includes SDMMC drivers and examples in the following path:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;EM&gt;SDK_2.7.0_EVK-MIMXRT1060.zip\boards\evkmimxrt1060\sdmmc_examples&lt;/EM&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can download it from the following link:&amp;nbsp;&lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/welcome" title="https://mcuxpresso.nxp.com/en/welcome"&gt;Welcome | MCUXpresso SDK Builder&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2020 16:02:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/1060-API-for-EMMC/m-p/1026069#M6992</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2020-02-17T16:02:59Z</dc:date>
    </item>
    <item>
      <title>Re: 1060 API for EMMC</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/1060-API-for-EMMC/m-p/1167375#M10560</link>
      <description>&lt;P&gt;I am trying to use this example on USDHC2, in 8 bit mode so that we can boot from the part. We are testing the hardware of the board, how do I port the example from USDHC1, we have made some changes but I can see nothing on the logic analyser.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;</description>
      <pubDate>Wed, 14 Oct 2020 10:00:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/1060-API-for-EMMC/m-p/1167375#M10560</guid>
      <dc:creator>gredpath</dc:creator>
      <dc:date>2020-10-14T10:00:37Z</dc:date>
    </item>
  </channel>
</rss>