<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB CDC-ECM Support in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-CDC-ECM-Support/m-p/808595#M1046</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;On the MCUXpresso SDK v2.4.0 for EVKB-MIMXRT1050, it is available an CDC Host example under “usb_examples-&amp;gt;host_cdc_bm”. This example asks for a USB-UART Device, so, it will be required applying the proper changes to work with USB-Ethernet and with the desired functionality.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Nov 2018 19:41:17 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2018-11-12T19:41:17Z</dc:date>
    <item>
      <title>USB CDC-ECM Support</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-CDC-ECM-Support/m-p/808594#M1045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the Device Stack Reference I see mention of CDC ACM and CDC RNDIS (and RNDIS is build upon ACM)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the Host Stack Reference the CDC description seems to be more generic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to support CDC-ECM on the USB Host of the RT1050, is the host side typically a thin layer between the USB and a virtual Ethernet Interface on the IP Stack?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't expect to be able to support RNDIS since my host does not support the Microsoft NDIS protocol.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While less important, CDC-ECM Device support would be nice to have too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2018 12:03:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-CDC-ECM-Support/m-p/808594#M1045</guid>
      <dc:creator>w2vy</dc:creator>
      <dc:date>2018-11-06T12:03:47Z</dc:date>
    </item>
    <item>
      <title>Re: USB CDC-ECM Support</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-CDC-ECM-Support/m-p/808595#M1046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;On the MCUXpresso SDK v2.4.0 for EVKB-MIMXRT1050, it is available an CDC Host example under “usb_examples-&amp;gt;host_cdc_bm”. This example asks for a USB-UART Device, so, it will be required applying the proper changes to work with USB-Ethernet and with the desired functionality.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Nov 2018 19:41:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/USB-CDC-ECM-Support/m-p/808595#M1046</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2018-11-12T19:41:17Z</dc:date>
    </item>
  </channel>
</rss>