<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I.mxRT1020  GPIO_SD_B1_05 (Pin 26) HardFault in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/I-mxRT1020-GPIO-SD-B1-05-Pin-26-HardFault/m-p/1158925#M10269</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;You can still use the pin but with reduced FlexSPI speed of 60MHz. If the code is not large it should be running from internal instruction RAM anyway where it achieves 500MHz with zero wait states and thus much faster than XiP mode (with less radiation and power consumption too).&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;EM&gt;uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;BR /&gt;&lt;FONT color="#999999"&gt;Contact me by personal message or on the uTasker web site to discuss professional training or product development requirements&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 25 Sep 2020 00:14:56 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2020-09-25T00:14:56Z</dc:date>
    <item>
      <title>I.mxRT1020  GPIO_SD_B1_05 (Pin 26) HardFault</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/I-mxRT1020-GPIO-SD-B1-05-Pin-26-HardFault/m-p/1158141#M10233</link>
      <description>&lt;P&gt;Dear I.mxRT1020 support,&lt;/P&gt;
&lt;P&gt;It seem that whenever I tried to enable the GPIO_SD_B1_05 in using the code generated by the PInmux tool, it would generate a hard fault imediately after executing the next line after&lt;/P&gt;
&lt;P&gt;IOMUXC_SetPinConfig(&lt;BR /&gt;IOMUXC_GPIO_SD_B1_05_GPIO3_IO25, /* GPIO_SD_B1_05 PAD functional properties : */&lt;BR /&gt;0x18B0U);&lt;/P&gt;
&lt;P&gt;I am using IDE version 11.2 and SDK2.8.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;hy&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="HeMyFAE_0-1600897998075.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/126014i80B4F5E7A2A937EC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="HeMyFAE_0-1600897998075.png" alt="HeMyFAE_0-1600897998075.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="HeMyFAE_1-1600898161264.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/126016i773F467E31DAAC1A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="HeMyFAE_1-1600898161264.png" alt="HeMyFAE_1-1600898161264.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Sep 2020 22:43:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/I-mxRT1020-GPIO-SD-B1-05-Pin-26-HardFault/m-p/1158141#M10233</guid>
      <dc:creator>HeMyFAE</dc:creator>
      <dc:date>2020-09-23T22:43:52Z</dc:date>
    </item>
    <item>
      <title>Re: I.mxRT1020  GPIO_SD_B1_05 (Pin 26) HardFault</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/I-mxRT1020-GPIO-SD-B1-05-Pin-26-HardFault/m-p/1158150#M10234</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;The answer is here (same for i.MX RT 1020 and 1060 - You need to change the flash configuration to not use this pin and then it won't fail).&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT/target-crashes-writing-to-register-SW-MUX-CTL-PAD-GPIO-SD-B1-05/m-p/1137334" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-RT/target-crashes-writing-to-register-SW-MUX-CTL-PAD-GPIO-SD-B1-05/m-p/1137334GPIO_SD_B1_05&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;EM&gt;uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;BR /&gt;&lt;FONT color="#999999"&gt;Contact me by personal message or on the uTasker web site to discuss professional training or product development requirements&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#3366FF"&gt;For a complete boot loader concept for your target check out the following:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#3366FF"&gt;- i.MX RT 1060: &lt;A href="https://www.utasker.com/iMX/RT1060.html" target="_blank" rel="noopener"&gt;https://www.utasker.com/iMX/RT1060.html&lt;/A&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#3366FF"&gt;- Boot loader concept including XiP on-the-fly decryption, clone protection or AES256 protected RAM execution.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#3366FF"&gt;-- Boot Loader concept flow chart: &lt;A href="https://www.utasker.com/docs/iMX/Loader.pdf" target="_blank" rel="noopener"&gt;https://www.utasker.com/docs/iMX/Loader.pdf&lt;/A&gt; and usage reference &lt;A href="https://www.utasker.com/docs/iMX/uTaskerLoader_TestDrive.pdf" target="_blank" rel="noopener"&gt;https://www.utasker.com/docs/iMX/uTaskerLoader_TestDrive.pdf&lt;/A&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#3366FF"&gt;-- Serial Loader features: &lt;A href="https://www.utasker.com/docs/uTasker/uTaskerSerialLoader.pdf" target="_blank" rel="noopener"&gt;https://www.utasker.com/docs/uTasker/uTaskerSerialLoader.pdf&lt;/A&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#3366FF"&gt;-- Building the loader with MCUXpress: &lt;A href="https://www.utasker.com/docs/iMX/MCUXpresso.pdf" target="_blank" rel="noopener"&gt;https://www.utasker.com/docs/iMX/MCUXpresso.pdf&lt;/A&gt; (and video guide &lt;A href="https://youtu.be/p_eUGo6GypY" target="_blank" rel="noopener"&gt;https://youtu.be/p_eUGo6GypY&lt;/A&gt; ) - the guide document explains how to use with any application (eg. SDK) and to enabling its operation with On-The-Fly decryption in 5 minutes&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#3366FF"&gt;-- Building the loader with IAR: &lt;A href="https://www.utasker.com/docs/iMX/IAR.pdf" target="_blank" rel="noopener"&gt;https://www.utasker.com/docs/iMX/IAR.pdf&lt;/A&gt; (and video guide &lt;A href="https://youtu.be/XPCwVndP99s" target="_blank" rel="noopener"&gt;https://youtu.be/XPCwVndP99s&lt;/A&gt; )&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#3366FF"&gt;-- Building the loader with VisualStudio and GCC: &lt;A href="https://www.utasker.com/docs/iMX/GCC.pdf" target="_blank" rel="noopener"&gt;https://www.utasker.com/docs/iMX/GCC.pdf&lt;/A&gt; (and video guide &lt;A href="https://youtu.be/0UzLLSXABK8" target="_blank" rel="noopener"&gt;https://youtu.be/0UzLLSXABK8&lt;/A&gt; )&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Sep 2020 11:50:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/I-mxRT1020-GPIO-SD-B1-05-Pin-26-HardFault/m-p/1158150#M10234</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-09-24T11:50:51Z</dc:date>
    </item>
    <item>
      <title>Re: I.mxRT1020  GPIO_SD_B1_05 (Pin 26) HardFault</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/I-mxRT1020-GPIO-SD-B1-05-Pin-26-HardFault/m-p/1158233#M10236</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;For QSPI Flash as XIP function, to achieve highest performance it is recommended to left FLEXSPI_A_DQS（GPIO_SD_B1_05）pin floating and config-sample clock source as 01-loopback from DQS pad mode to achieve max 133MHz Flexspi_clk, and change the function of this pin will make the application code crash.&lt;BR /&gt;Hope this clear.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 24 Sep 2020 02:08:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/I-mxRT1020-GPIO-SD-B1-05-Pin-26-HardFault/m-p/1158233#M10236</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2020-09-24T02:08:57Z</dc:date>
    </item>
    <item>
      <title>Re: I.mxRT1020  GPIO_SD_B1_05 (Pin 26) HardFault</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/I-mxRT1020-GPIO-SD-B1-05-Pin-26-HardFault/m-p/1158921#M10268</link>
      <description>&lt;P&gt;thank you to both for your quick reply.&lt;/P&gt;
&lt;P&gt;I was wondering if you can let the design make a slight modification on his schematics to add a dQS signal name to the GPIO_SDS_b1_05 similar to the RT1050EVKB schematics.&lt;/P&gt;
&lt;P&gt;It would help reduce the chance to make the same mistake for the next RT1020 customer.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;hy&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2020 00:08:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/I-mxRT1020-GPIO-SD-B1-05-Pin-26-HardFault/m-p/1158921#M10268</guid>
      <dc:creator>HeMyFAE</dc:creator>
      <dc:date>2020-09-25T00:08:34Z</dc:date>
    </item>
    <item>
      <title>Re: I.mxRT1020  GPIO_SD_B1_05 (Pin 26) HardFault</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/I-mxRT1020-GPIO-SD-B1-05-Pin-26-HardFault/m-p/1158925#M10269</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;You can still use the pin but with reduced FlexSPI speed of 60MHz. If the code is not large it should be running from internal instruction RAM anyway where it achieves 500MHz with zero wait states and thus much faster than XiP mode (with less radiation and power consumption too).&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;EM&gt;uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;BR /&gt;&lt;FONT color="#999999"&gt;Contact me by personal message or on the uTasker web site to discuss professional training or product development requirements&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2020 00:14:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/I-mxRT1020-GPIO-SD-B1-05-Pin-26-HardFault/m-p/1158925#M10269</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-09-25T00:14:56Z</dc:date>
    </item>
    <item>
      <title>Re: I.mxRT1020  GPIO_SD_B1_05 (Pin 26) HardFault</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/I-mxRT1020-GPIO-SD-B1-05-Pin-26-HardFault/m-p/1159452#M10290</link>
      <description>&lt;P&gt;HI Jeremy,&lt;/P&gt;
&lt;P&gt;I spoke with Anthony Huereca and also looked closer at Reference Manual.&lt;/P&gt;
&lt;P&gt;It stated that the DQSA pin is only applicable for HyperRam/HyperFlash for dummy ready cycle.&lt;/P&gt;
&lt;P&gt;For QSPI it doesn't apply. Can you confirm with designer to see that is the case?&lt;/P&gt;
&lt;P&gt;If DQSA is not applicable for QSPI flash then we do have a conflict issue to resolve.&lt;/P&gt;
&lt;P&gt;Thx,&lt;/P&gt;
&lt;P&gt;hy&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="HeMyFAE_0-1601051402009.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/126212i9EAEA953AA3483E5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="HeMyFAE_0-1601051402009.jpeg" alt="HeMyFAE_0-1601051402009.jpeg" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2020 16:34:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/I-mxRT1020-GPIO-SD-B1-05-Pin-26-HardFault/m-p/1159452#M10290</guid>
      <dc:creator>HeMyFAE</dc:creator>
      <dc:date>2020-09-25T16:34:29Z</dc:date>
    </item>
    <item>
      <title>Re: I.mxRT1020  GPIO_SD_B1_05 (Pin 26) HardFault</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/I-mxRT1020-GPIO-SD-B1-05-Pin-26-HardFault/m-p/1159628#M10294</link>
      <description>&lt;P&gt;Thanks for your reply.&lt;BR /&gt;1) Can you confirm with the designer to see that is the case?&lt;BR /&gt;-- The DQS pin design suggestion definitely applies to QSPI flash, as I remember that AE highlighted this design tip during the RT training.&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Sun, 27 Sep 2020 02:22:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/I-mxRT1020-GPIO-SD-B1-05-Pin-26-HardFault/m-p/1159628#M10294</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2020-09-27T02:22:20Z</dc:date>
    </item>
    <item>
      <title>Re: I.mxRT1020  GPIO_SD_B1_05 (Pin 26) HardFault</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/I-mxRT1020-GPIO-SD-B1-05-Pin-26-HardFault/m-p/1160465#M10313</link>
      <description>&lt;P&gt;Also see this note from the hardware development guide&lt;/P&gt;&lt;P&gt;-Nick&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="nickwallis_0-1601363860726.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/126406iA25CC6D70746FF58/image-size/medium?v=v2&amp;amp;px=400" role="button" title="nickwallis_0-1601363860726.png" alt="nickwallis_0-1601363860726.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Sep 2020 07:17:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/I-mxRT1020-GPIO-SD-B1-05-Pin-26-HardFault/m-p/1160465#M10313</guid>
      <dc:creator>nickwallis</dc:creator>
      <dc:date>2020-09-29T07:17:55Z</dc:date>
    </item>
  </channel>
</rss>