<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: RT 1020 Firmware update using Flashloader</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT-1020-Firmware-update-using-Flashloader/m-p/1158812#M10264</link>
    <description>&lt;P&gt;Was the question about retrofitting mfgtool to Linux ever answered?&amp;nbsp; Is there source code available to do this?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Thu, 24 Sep 2020 17:30:33 GMT</pubDate>
    <dc:creator>pholden</dc:creator>
    <dc:date>2020-09-24T17:30:33Z</dc:date>
    <item>
      <title>RT 1020 Firmware update using Flashloader</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT-1020-Firmware-update-using-Flashloader/m-p/865100#M2049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a MIMRT1020-EVK board.&lt;/P&gt;&lt;P&gt;Following the AN12238 i.MX RT Flashloader Use Case (&lt;A data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fnxp%2Fapplication-notes%2FAN12238.pdf" rel="nofollow" target="_blank"&gt;&lt;SPAN style="color: #0066cc; text-decoration: underline;"&gt;&lt;/SPAN&gt;&lt;/A&gt;&lt;A href="https://www.nxp.com/docs/en/nxp/application-notes/AN12238.pdf" target="test_blank"&gt;https://www.nxp.com/docs/en/nxp/application-notes/AN12238.pdf&lt;/A&gt;&amp;nbsp;) . Though this document is written for 1050, I assume the steps would be the same for 1020.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Boot into Serial Downloader" mode. (SW8 settings , off,off,off,on).&lt;/LI&gt;&lt;LI&gt;Verified that the SDPhost tool can communicate with BootROM of MIMRT1020-evk using UART interface. (error-status command)&lt;/LI&gt;&lt;LI&gt;Successfully download the flashloader.bin located at "\Flashloader_RT1020_1.0_GA\Tools\mfgtools-rel\Profiles\MXRT102X\OS Firmware\"&amp;nbsp; (&lt;EM&gt;sdphost.exe -d -p COM25 write-file 0x20000000 ivt_flashloader.bin&lt;/EM&gt;)&lt;/LI&gt;&lt;LI&gt;Start up the flashloader image (&lt;EM&gt;sdphost.exe -d -p COM25 jump-address 0x20000400)&lt;/EM&gt;&lt;/LI&gt;&lt;LI&gt;Verify the communication with a running Flashloader (&lt;EM&gt;blhost.exe -d -p COM25 get-property 1&lt;/EM&gt;)&amp;nbsp;Failed!&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Get error- &lt;EM&gt;"Error: Initial ping failure: No response received for ping command."&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Notice that the USB did not re-enumerate to VID/PID 0x15A2/0x0073. We remain at 1FC9/130.&lt;/P&gt;&lt;P&gt;Attached is the console log.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Repeated the above with usb (-u) option same issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What am I missing here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Ashish&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jan 2019 21:14:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT-1020-Firmware-update-using-Flashloader/m-p/865100#M2049</guid>
      <dc:creator>ashishpradhan</dc:creator>
      <dc:date>2019-01-28T21:14:18Z</dc:date>
    </item>
    <item>
      <title>Re: RT 1020 Firmware update using Flashloader</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT-1020-Firmware-update-using-Flashloader/m-p/865101#M2050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tested USB-HID port, it seems the board doesn't jump to the new USB-HID(vid="15A2" pid="0073), so I don't use command, I use the mfgtool.exe in the flashloader folder, the board jump successfully, then I use&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"blhost.exe -u&amp;nbsp; get-property 1" get the correct messgae, you can try it&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jan 2019 05:57:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT-1020-Firmware-update-using-Flashloader/m-p/865101#M2050</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2019-01-31T05:57:33Z</dc:date>
    </item>
    <item>
      <title>Re: RT 1020 Firmware update using Flashloader</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT-1020-Firmware-update-using-Flashloader/m-p/865102#M2051</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; I think the option "get-property" under item 5 should be applied to the USB port.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;The flashloader uses the USB.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jan 2019 07:59:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT-1020-Firmware-update-using-Flashloader/m-p/865102#M2051</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-01-31T07:59:20Z</dc:date>
    </item>
    <item>
      <title>Re: RT 1020 Firmware update using Flashloader</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT-1020-Firmware-update-using-Flashloader/m-p/865103#M2052</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes but we cannot use mfgtool.exe in field since its a windows utility. &lt;/P&gt;&lt;P&gt;We would like to support&amp;nbsp;OTA firmware update where the firmware would be downloaded on to&amp;nbsp;master board (Android/Linux) and applied on the various sub-systems over uart.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking at the MfgTool logs and the ucl2.xml it seems the mfgtool.exe is calling sdphost and blhost to&amp;nbsp;load the ivt_flashloader and program the&amp;nbsp;flash.&amp;nbsp;We would like to update the firmware using the same either via scripts or writing our own application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is source available for the tools?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jan 2019 16:14:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT-1020-Firmware-update-using-Flashloader/m-p/865103#M2052</guid>
      <dc:creator>ashishpradhan</dc:creator>
      <dc:date>2019-01-31T16:14:59Z</dc:date>
    </item>
    <item>
      <title>Re: RT 1020 Firmware update using Flashloader</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT-1020-Firmware-update-using-Flashloader/m-p/1152272#M10064</link>
      <description>&lt;P&gt;Is there a resolution for this problem?&amp;nbsp; Do you have source code for mfgtool.exe that can be provided to retrofit it into Linux mode of operation?&lt;/P&gt;</description>
      <pubDate>Fri, 11 Sep 2020 17:34:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT-1020-Firmware-update-using-Flashloader/m-p/1152272#M10064</guid>
      <dc:creator>pholden</dc:creator>
      <dc:date>2020-09-11T17:34:54Z</dc:date>
    </item>
    <item>
      <title>Re: RT 1020 Firmware update using Flashloader</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT-1020-Firmware-update-using-Flashloader/m-p/1158812#M10264</link>
      <description>&lt;P&gt;Was the question about retrofitting mfgtool to Linux ever answered?&amp;nbsp; Is there source code available to do this?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 24 Sep 2020 17:30:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT-1020-Firmware-update-using-Flashloader/m-p/1158812#M10264</guid>
      <dc:creator>pholden</dc:creator>
      <dc:date>2020-09-24T17:30:33Z</dc:date>
    </item>
  </channel>
</rss>