<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Example of flexspi_nor_config_t for GD25LX256 in i.MX RT Crossover MCUs</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1154875#M10144</link>
    <description>&lt;P&gt;&lt;EM&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/40101"&gt;@jay_heng&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/117617"&gt;@Sabina_Bruce&lt;/a&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Finally&lt;/EM&gt; got something working. I used Jay's utility to create a binary image, then compared the first 0x200 bytes of jay's image (FDCB location) with the first 0x200 of my binary, and worked back to getting a struct that gives an identical 0x200 bytes.&lt;/P&gt;&lt;P&gt;Here's the coded struct below... I have little idea about many of the field decisions because I can't find any docs on how to set them up correctly. This code is the very definition of a pass-it-on whisper! I do sincerely wish that NXP would release some good documentation on how to configure this struct. I don't know yet if this is an optimal configuration. Some testing required to see what performance I get.&lt;/P&gt;&lt;P&gt;Good info in Chapters 9 and 27 of the Reference Manual. Jay's utility can help you configure your FDCB.&lt;/P&gt;&lt;P&gt;Table 9.9 lists the boot pins options. Table 9.14 has the full definition of the FDCB struct. Table 9.15 has the LUT sequence definition for Serial Nor.&lt;/P&gt;&lt;P&gt;In a nutshell:&lt;/P&gt;&lt;P&gt;To get McuXpresso to program the GD25LX, set BOOT_CFG2[2:0] on your board to 0b000 (3B SPI). Big thanks to Sabina for this tip: it was crucial to allow me to program the flash via McuX. I also set up my board so I can force it into USB DFU mode (to work with Jay's utility) by having the option to pull BOOT_CFG1[6] high.&lt;/P&gt;&lt;P&gt;In C/C++ Build/MCU Settings, Memory details, set your Flash memory to the correct address/size, and select &lt;STRONG&gt;MIMXRT1050_SFDP_QSPI.cfx&lt;/STRONG&gt; as your flash driver.&lt;/P&gt;&lt;P&gt;In C/C++ Build/Settings/Mcu C Compiler/Preprocessor, define the following symbols:&lt;/P&gt;&lt;P&gt;XIP_EXTERNAL_FLASH=1&lt;/P&gt;&lt;P&gt;XIP_BOOT_HEADER_ENABLE=1&lt;/P&gt;&lt;P&gt;McuX will automatically create the FDCB and fill it out to allow XIP booting.&lt;/P&gt;&lt;P&gt;If you don't need the ROM bootloader to initialize SDRAM or other peripherals, set XIP_BOOT_HEADER_DCD_ENABLE=0. If you do need SDRAM etc, then set it to 1 and you will need to provide the DCD data block also (Xpresso has a config tool for this).&lt;/P&gt;&lt;P&gt;I hope this is useful to anyone else booting off this flash device. Caveat: I've just got this working and there may be some bugs/mistakes in my code.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Thanks very much to Jay and Sabina for their help in solving this problem.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Eamonn&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;//Based on Jay Heng's McuBootUtility output configured for GD25LX:
const flexspi_nor_config_t hyperflash_config = {
    .memConfig =
        {
            .tag                = FLEXSPI_CFG_BLK_TAG,
            .version            = FLEXSPI_CFG_BLK_VERSION,
            .readSampleClksrc=kFlexSPIReadSampleClk_ExternalInputFromDqsPad,
            .csHoldTime         = 3u,
            .csSetupTime        = 3u,
            .columnAddressWidth = 0u,

			.deviceModeCfgEnable = 0,
			.deviceModeType = 0,
			.waitTimeCfgCommands = 0,
			//.deviceModeSeq = 0, //This is a flexspi_lut_seq_t sub-struct.
			.deviceModeArg = 0,
			.configCmdEnable = 0,
			//.configModeType[0..2] = 0,
			//.configCmdSeqs[3] = 0, //This an array of flexspi_lut_seq_t sub-structs.
			//.configCmdArgs0..2] = 0, //Array of uint32_t.
			.controllerMiscOption = 0x00000050, // Enable DDR mode, Safe configuration.

			.deviceType = 0x01,	//kFlexSpiDeviceType_SerialNOR
            .sflashPadType = 8, //kSerialFlash_8Pads,

            .serialClkFreq = 8, //kFlexSpiSerialClk_166MHz,

			.lutCustomSeqEnable = 0, //LUT customization disabled.

            .sflashA1Size  = 0x2000000, //32u * 1024u * 1024u,
			.sflashA2Size = 0,
			.sflashB1Size = 0,
			.sflashB2Size = 0,

			.csPadSettingOverride = 0,
			.sclkPadSettingOverride = 0,
			.dataPadSettingOverride = 0,
			.dqsPadSettingOverride = 0,
			.timeoutInMs = 0,
			.commandInterval = 0,

            .dataValidTime = {15u, 0u},

			.busyOffset = 0,
			.busyBitPolarity = 0,
            .lookupTable =
                {
                    // Read LUTs as per binary from Jay Heng's MCUBootUtility configured for GD25LX...
					FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xFD,    RADDR_DDR, FLEXSPI_8PAD, 0x20),
					FLEXSPI_LUT_SEQ(DUMMY_DDR, FLEXSPI_8PAD, 0x06,  READ_DDR, FLEXSPI_8PAD, 0x04),
					0,0,

					FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x05,    READ_SDR, FLEXSPI_1PAD, 0x04),
					0,0,0,

					0,0,0,0,

					FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x06,    STOP, FLEXSPI_1PAD, 0x0),
					0,0,0,

					0,0,0,0,

					FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x21,    RADDR_SDR, FLEXSPI_1PAD, 0x20),
					0,0,0,

					0,0,0,0,

					0,0,0,0,

					FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xDC,    RADDR_SDR, FLEXSPI_1PAD, 0x20),
					0,0,0,

					FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x8E,    RADDR_SDR, FLEXSPI_8PAD, 0x20),
					FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_8PAD, 0x80,  STOP, FLEXSPI_1PAD, 0x0),
					0,0,

					0,0,0,0,

					FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x60,    STOP, FLEXSPI_1PAD, 0x0),

                },
        },
	    .pageSize           = 0x100,
	    .sectorSize         = 0x1000,
		.ipcmdSerialClkFreq = 1,
	    .isUniformBlockSize = 0,
		.serialNorType = 0,
		.needExitNoCmdMode = 0,
		.halfClkForNonReadCmd = 1,
		.needRestoreNoCmdMode = 0,

	    .blockSize          = 64u * 1024u,
};&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 17 Sep 2020 14:42:43 GMT</pubDate>
    <dc:creator>eamonnheffernan</dc:creator>
    <dc:date>2020-09-17T14:42:43Z</dc:date>
    <item>
      <title>Example of flexspi_nor_config_t for GD25LX256</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1072979#M8883</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm looking for an example of &lt;SPAN style="color: #333399;"&gt;flexspi_nor_config_t&lt;/SPAN&gt;&amp;nbsp; found in &lt;SPAN style="color: #333399;"&gt;xip/evkbimxrt1050_flexspi_nor_config.c&lt;/SPAN&gt; for GD25LX256 octal flash.&lt;/P&gt;&lt;P&gt;What other changes do I need to make in McuXpresso IDE/Config?&lt;/P&gt;&lt;P&gt;1. flexspi_nor_config_t&lt;/P&gt;&lt;P&gt;2. Device Configuration Data [DCD].&lt;/P&gt;&lt;P&gt;3. Flash driver.&lt;/P&gt;&lt;P&gt;4. ???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone successfully booted from this device?&lt;/P&gt;&lt;P&gt;I'd appreciate any advice and config examples.&lt;/P&gt;&lt;P&gt;Thanks - Eamonn&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2020 12:54:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1072979#M8883</guid>
      <dc:creator>eamonnheffernan</dc:creator>
      <dc:date>2020-08-07T12:54:34Z</dc:date>
    </item>
    <item>
      <title>Re: Example of flexspi_nor_config_t for GD25LX256</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1072980#M8884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;RT can boot from GD25LX256, you can use my tool MCUBootUtility to download app into this flash, my tool can generate FDCB automatically, the you can refer to FDCB for flexspi_nor_config_t&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/JayHeng/NXP-MCUBootUtility" title="https://github.com/JayHeng/NXP-MCUBootUtility"&gt;GitHub - JayHeng/NXP-MCUBootUtility: A one-stop boot utility tool based on Python2.7+wxPython4.0, it can help you get st…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2020 08:26:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1072980#M8884</guid>
      <dc:creator>jay_heng</dc:creator>
      <dc:date>2020-08-10T08:26:22Z</dc:date>
    </item>
    <item>
      <title>Re: Example of flexspi_nor_config_t for GD25LX256</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1072981#M8885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;Hope you are doing well.&lt;/P&gt;&lt;P&gt;I'd like to recommend the following application note. It describes how to enable octal spi flash.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12107.pdf" title="https://www.nxp.com/docs/en/application-note/AN12107.pdf"&gt;How to Enable Boot from Octal SPI Flash and SD Card&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In addition I'd recommend to review the details of the datasheet of the flash that you are using. The&amp;nbsp;MIMXRT1050_SFDP_HYPERFLASH.cfx is a generic driver that attempts to recognize what type of flash it is connected to.&amp;nbsp;&amp;nbsp;Generally, flash devices typically contain a data block describing their properties including device size, low level structure and programming details etc. These data blocks and their use are collectively known as Serial Flash Discovery Protocol or SFDP. The standard for these blocks are described by JEDEC JESD216 standard(s).&lt;/P&gt;&lt;P&gt;If this is possible then it should be recognized with this driver.&amp;nbsp; Flashdrivers cannot detect whether QSPI or Hyperflash is fitted on a board, therefore it is the responsibility of the user to ensure the correct driver is used.&lt;/P&gt;&lt;P&gt;For more details, section 15.2.4 of the MCUXpresso IDE User Guide:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/user-guide/MCUXpresso_IDE_User_Guide.pdf" title="https://www.nxp.com/docs/en/user-guide/MCUXpresso_IDE_User_Guide.pdf"&gt;https://www.nxp.com/docs/en/user-guide/MCUXpresso_IDE_User_Guide.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2020 05:49:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1072981#M8885</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2020-08-11T05:49:45Z</dc:date>
    </item>
    <item>
      <title>Re: Example of flexspi_nor_config_t for GD25LX256</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1072982#M8886</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Jay and Sabina.&lt;/P&gt;&lt;P&gt;Jay: impressive tool. I'll download it and try it out. I know it's only&amp;nbsp; tested on Windows, but do you know if it works on Ubuntu? Meanwhile, I'll use the code to help me build a DCD block.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sabina: I assume you mean &lt;STRONG&gt;15.2.4&lt;/STRONG&gt; of the IDE UG? I've read both AN12107 and the RM carefully and I've based my design on these. I'm hoping that the generic driver will be able to talk to the GD25LX256 as 15.2.4 suggests. I'll expect I'll configure the BOOT_CFG2 pins to 101b, Micron Octal DDR, command 0xFD OPI mode, which seems to be the closest match to the GD25LX256. MIMXRT1050_SFDP_HYPERFLASH.cfx for the IDE flash driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm just waiting on boards to arrive and I'll pick this up again when they do.&lt;/P&gt;&lt;P&gt;Thank you both very much for your help. Much appreciated.&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Eamonn&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2020 18:05:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1072982#M8886</guid>
      <dc:creator>eamonnheffernan</dc:creator>
      <dc:date>2020-08-13T18:05:01Z</dc:date>
    </item>
    <item>
      <title>Re: Example of flexspi_nor_config_t for GD25LX256</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1072983#M8887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, thank you. I've corrected this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Aug 2020 05:05:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1072983#M8887</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2020-08-15T05:05:58Z</dc:date>
    </item>
    <item>
      <title>Re: Example of flexspi_nor_config_t for GD25LX256</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1135178#M9944</link>
      <description>&lt;P&gt;Ok, so I've got my boards and all seems well. I can load code and debug a RAM application.&lt;/P&gt;&lt;P&gt;Now, I'm trying to set up McuXpresso 11.2.0 to load code into the GD25LX256.&lt;/P&gt;&lt;P&gt;To achieve this, I use the following configurion:&lt;/P&gt;&lt;P&gt;BOOT_MODE[1:0] = 0b10 (internal boot with GPIO override)&lt;/P&gt;&lt;P&gt;BOOT_CFG1[7:0] = 0b00000000&lt;/P&gt;&lt;P&gt;BOOT_CFG2[2:0] = 0b101 (Micron Octal DDR, command 0xFD, OPI mode)&amp;nbsp; (This seems most similar to GD25, is this correct choice?)&lt;/P&gt;&lt;P&gt;In the Memory details section of Mcu Settings, I have added Flash at 0x60000000, size 0x2000000, and chosen MIMXRT1050_SFDP_HYPERFLASH. Correct?&lt;/P&gt;&lt;P&gt;When I debug, I get this error message:&lt;/P&gt;&lt;P&gt;MCUXpresso IDE RedlinkMulti Driver v11.1 (Jul 7 2020 10:53:47 - crt_emu_cm_redlink build 5)&lt;BR /&gt;Found chip XML file in /home/eamonn/Documents/MCUXpresso_11.2.0_4120/workspace/pink_3/Debug/MIMXRT1051xxxxB.xml&lt;BR /&gt;( 5) Remote configuration complete&lt;BR /&gt;Reconnected to existing LinkServer process.&lt;BR /&gt;============= SCRIPT: RT1050_connect.scp =============&lt;BR /&gt;RT1050 Connect Script&lt;BR /&gt;DpID = 0BD11477&lt;BR /&gt;APID = 0x04770041&lt;BR /&gt;Disabling MPU&lt;BR /&gt;Configure FlexRAM for 256KB OC RAM, 128KB I-TCM, 128KB D-TCM&lt;BR /&gt;Finished&lt;BR /&gt;============= END SCRIPT =============================&lt;BR /&gt;Probe Firmware: LPC-LINK2 CMSIS-DAP V5.361 (NXP Semiconductors)&lt;BR /&gt;Serial Number: IXFUMYIS&lt;BR /&gt;VID:PID: 1FC9:0090&lt;BR /&gt;USB Path: /dev/hidraw2&lt;BR /&gt;Using memory from core 0 after searching for a good core&lt;BR /&gt;debug interface type = Cortex-M7 (DAP DP ID 0BD11477) over SWD TAP 0&lt;BR /&gt;processor type = Cortex-M7 (CPU ID 00000C27) on DAP AP 0&lt;BR /&gt;number of h/w breakpoints = 8&lt;BR /&gt;number of flash patches = 0&lt;BR /&gt;number of h/w watchpoints = 4&lt;BR /&gt;Probe(0): Connected&amp;amp;Reset. DpID: 0BD11477. CpuID: 00000C27. Info: &amp;lt;None&amp;gt;&lt;BR /&gt;Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;BR /&gt;Content of CoreSight Debug ROM(s):&lt;BR /&gt;RBASE E00FD000: CID B105100D PID 000008E88C ROM (type 0x1)&lt;BR /&gt;ROM 1 E00FE000: CID B105100D PID 04000BB4C8 ROM (type 0x1)&lt;BR /&gt;ROM 2 E00FF000: CID B105100D PID 04000BB4C7 ROM (type 0x1)&lt;BR /&gt;ROM 3 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)&lt;BR /&gt;ROM 3 E0001000: CID B105E00D PID 04000BB002 Gen DWT (type 0x0)&lt;BR /&gt;ROM 3 E0002000: CID B105E00D PID 04000BB00E Gen (type 0x0)&lt;BR /&gt;ROM 3 E0000000: CID B105E00D PID 04000BB001 Gen ITM (type 0x0)&lt;BR /&gt;ROM 2 E0041000: CID B105900D PID 04001BB975 CSt ARM ETMv4.0 type 0x13 Trace Source - Core&lt;BR /&gt;ROM 2 E0042000: CID B105900D PID 04004BB906 CSt type 0x14 Debug Control - Trigger, e.g. ECT&lt;BR /&gt;ROM 1 E0040000: CID B105900D PID 04000BB9A9 CSt type 0x11 Trace Sink - TPIU&lt;BR /&gt;ROM 1 E0043000: CID B105F00D PID 04001BB101 Sys (type 0x0)&lt;BR /&gt;NXP: MIMXRT1051xxxxB&lt;BR /&gt;DAP stride is 1024 bytes (256 words)&lt;BR /&gt;Inspected v.2 External Flash Device on SPI using SFDP JEDEC ID MIMXRT1050_SFDP_HYPERFLASH.cfx&lt;BR /&gt;Image 'iMXRT1050_SFDP_HYPERFLASH Jul 7 2020 10:54:44'&lt;BR /&gt;Opening flash driver MIMXRT1050_SFDP_HYPERFLASH.cfx&lt;BR /&gt;Sending VECTRESET to run flash driver&lt;BR /&gt;Driver V.2 dynamic startup failed - driver Init provided no flash parameters&lt;BR /&gt;Flash Driver V.2 startup failed - rc Ef(55): Dynamic flash driver startup failed to provide flash parameters.&lt;BR /&gt;Terminate (0x0, 0x0, 0x0) status 0x40 - driver reports init failure - EXTSPIJ driver rc 7000 (0x1B58)&lt;BR /&gt;chip initialization failed - Ef(55): Dynamic flash driver startup failed to provide flash parameters.&lt;BR /&gt;failed to initialize flash driver MIMXRT1050_SFDP_HYPERFLASH.cfx&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Am I missing something?&lt;/P&gt;&lt;P&gt;Thanks - Eamonn&lt;/P&gt;</description>
      <pubDate>Thu, 03 Sep 2020 10:58:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1135178#M9944</guid>
      <dc:creator>eamonnheffernan</dc:creator>
      <dc:date>2020-09-03T10:58:58Z</dc:date>
    </item>
    <item>
      <title>Re: Example of flexspi_nor_config_t for GD25LX256</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1149787#M9999</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/40101"&gt;@jay_heng&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/117617"&gt;@Sabina_Bruce&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi Jay/Sabina. Please let me know if you have any comments on my setup and the error message I'm getting.&lt;/P&gt;&lt;P&gt;Thanks - Eamonn&lt;/P&gt;</description>
      <pubDate>Mon, 07 Sep 2020 15:31:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1149787#M9999</guid>
      <dc:creator>eamonnheffernan</dc:creator>
      <dc:date>2020-09-07T15:31:09Z</dc:date>
    </item>
    <item>
      <title>Re: Example of flexspi_nor_config_t for GD25LX256</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1150511#M10021</link>
      <description>&lt;P&gt;Hope you are doing well. It looks like its not able to read the parameters correctly. Therefore I believe that choosing the the CFG_Boot2[2:0] to 101 is not correct. The option is specific to the brand Micron which in this case is not a match even though the command is listed in the datasheet of the device you are using.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please try with a generic option that supports 3B as the default. Looking at the datasheet it looks like the address status bit of your device is in 3-byte address mode by default.&lt;/P&gt;
&lt;P&gt;Let me know if this results differently for you.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Sabina&lt;/P&gt;</description>
      <pubDate>Tue, 08 Sep 2020 17:43:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1150511#M10021</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2020-09-08T17:43:06Z</dc:date>
    </item>
    <item>
      <title>Re: Example of flexspi_nor_config_t for GD25LX256</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1151518#M10044</link>
      <description>&lt;P&gt;Hi Sabina, this is very helpful.&lt;/P&gt;&lt;P&gt;I switched to CFG_Boot2[2:0] to 0b000, tested, failed.&lt;/P&gt;&lt;P&gt;Next I changed the Flash driver in MCU Settings from MIMXRT1050_SFDP_HYPERFLASH.cfx to MIMXRT1050_SFDP_QSPI.cfx.&lt;/P&gt;&lt;P&gt;Bingo! That combination is reporting success in programming the flash. (See debugger messages below.)&lt;/P&gt;&lt;P&gt;I get a target crash because I haven't correctly configured the XIP FDCB (&lt;SPAN&gt;flexspi_nor_config_t&lt;/SPAN&gt;) in the target code yet. That's my next challenge.&lt;/P&gt;&lt;P&gt;I'll try Jay's MCUBootUtility to generate the FDCB. If you have an example of this oven-ready, I'll happily take a short cut!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you so much for your help.&lt;/P&gt;&lt;P&gt;Best - Eamonn&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;MCUXpresso IDE RedlinkMulti Driver v11.1 (Jul 7 2020 10:53:47 - crt_emu_cm_redlink build 5)&lt;BR /&gt;Found chip XML file in /home/eamonn/Documents/MCUXpresso_11.2.0_4120/workspace/pink_2/Debug/MIMXRT1051xxxxB.xml&lt;BR /&gt;Reconnected to existing LinkServer process.&lt;BR /&gt;============= SCRIPT: RT1050_connect.scp =============&lt;BR /&gt;RT1050 Connect Script&lt;BR /&gt;DpID = 0BD11477&lt;BR /&gt;APID = 0x04770041&lt;BR /&gt;Disabling MPU&lt;BR /&gt;Configure FlexRAM for 256KB OC RAM, 128KB I-TCM, 128KB D-TCM&lt;BR /&gt;Finished&lt;BR /&gt;============= END SCRIPT =============================&lt;BR /&gt;Probe Firmware: LPC-LINK2 CMSIS-DAP V5.361 (NXP Semiconductors)&lt;BR /&gt;Serial Number: IXFUMYIS&lt;BR /&gt;VID:PID: 1FC9:0090&lt;BR /&gt;USB Path: /dev/hidraw3&lt;BR /&gt;Using memory from core 0 after searching for a good core&lt;BR /&gt;debug interface type = Cortex-M7 (DAP DP ID 0BD11477) over SWD TAP 0&lt;BR /&gt;processor type = Cortex-M7 (CPU ID 00000C27) on DAP AP 0&lt;BR /&gt;number of h/w breakpoints = 8&lt;BR /&gt;number of flash patches = 0&lt;BR /&gt;number of h/w watchpoints = 4&lt;BR /&gt;Probe(0): Connected&amp;amp;Reset. DpID: 0BD11477. CpuID: 00000C27. Info: &amp;lt;None&amp;gt;&lt;BR /&gt;Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;BR /&gt;Content of CoreSight Debug ROM(s):&lt;BR /&gt;RBASE E00FD000: CID B105100D PID 000008E88C ROM (type 0x1)&lt;BR /&gt;ROM 1 E00FE000: CID B105100D PID 04000BB4C8 ROM (type 0x1)&lt;BR /&gt;ROM 2 E00FF000: CID B105100D PID 04000BB4C7 ROM (type 0x1)&lt;BR /&gt;ROM 3 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)&lt;BR /&gt;ROM 3 E0001000: CID B105E00D PID 04000BB002 Gen DWT (type 0x0)&lt;BR /&gt;ROM 3 E0002000: CID B105E00D PID 04000BB00E Gen (type 0x0)&lt;BR /&gt;ROM 3 E0000000: CID B105E00D PID 04000BB001 Gen ITM (type 0x0)&lt;BR /&gt;ROM 2 E0041000: CID B105900D PID 04001BB975 CSt ARM ETMv4.0 type 0x13 Trace Source - Core&lt;BR /&gt;ROM 2 E0042000: CID B105900D PID 04004BB906 CSt type 0x14 Debug Control - Trigger, e.g. ECT&lt;BR /&gt;ROM 1 E0040000: CID B105900D PID 04000BB9A9 CSt type 0x11 Trace Sink - TPIU&lt;BR /&gt;ROM 1 E0043000: CID B105F00D PID 04001BB101 Sys (type 0x0)&lt;BR /&gt;NXP: MIMXRT1051xxxxB&lt;BR /&gt;DAP stride is 1024 bytes (256 words)&lt;BR /&gt;Inspected v.2 External Flash Device on SPI using SFDP JEDEC ID MIMXRT1050_SFDP_QSPI.cfx&lt;BR /&gt;Image 'iMXRT1050_SFDP_QSPI Jul 7 2020 10:54:37'&lt;BR /&gt;Opening flash driver MIMXRT1050_SFDP_QSPI.cfx&lt;BR /&gt;Sending VECTRESET to run flash driver&lt;BR /&gt;Flash variant 'JEDEC_SFDP_Device' detected (32MB = 512*64K at 0x60000000)&lt;BR /&gt;Closing flash driver MIMXRT1050_SFDP_QSPI.cfx&lt;BR /&gt;Connected: was_reset=false. was_stopped=true&lt;BR /&gt;Awaiting telnet connection to port 3330 ...&lt;BR /&gt;GDB nonstop mode enabled&lt;BR /&gt;Opening flash driver MIMXRT1050_SFDP_QSPI.cfx (already resident)&lt;BR /&gt;Sending VECTRESET to run flash driver&lt;BR /&gt;Flash variant 'JEDEC_SFDP_Device' detected (32MB = 512*64K at 0x60000000)&lt;BR /&gt;Writing 26152 bytes to address 0x60002000 in Flash&lt;BR /&gt;Sectors written: 0, unchanged: 1, total: 1&lt;BR /&gt;Erased/Wrote sector 0-0 with 26152 bytes in 50msec&lt;BR /&gt;Closing flash driver MIMXRT1050_SFDP_QSPI.cfx&lt;BR /&gt;Flash Write Done&lt;BR /&gt;Flash Program Summary: 26152 bytes in 0.05 seconds (510.78 KB/sec)&lt;BR /&gt;Starting execution using system reset and halt target&lt;/P&gt;</description>
      <pubDate>Thu, 10 Sep 2020 10:21:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1151518#M10044</guid>
      <dc:creator>eamonnheffernan</dc:creator>
      <dc:date>2020-09-10T10:21:35Z</dc:date>
    </item>
    <item>
      <title>Re: Example of flexspi_nor_config_t for GD25LX256</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1153024#M10098</link>
      <description>&lt;P&gt;Excellent! I am glad that you were able to resolve this.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Sabina&lt;/P&gt;</description>
      <pubDate>Mon, 14 Sep 2020 18:52:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1153024#M10098</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2020-09-14T18:52:51Z</dc:date>
    </item>
    <item>
      <title>Re: Example of flexspi_nor_config_t for GD25LX256</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1153369#M10108</link>
      <description>&lt;P&gt;Hi Sabina,&lt;/P&gt;&lt;P&gt;I succeed in getting the ROM bootloader to boot from the GD25LX by configuring flexspi_nor_config_t struct (listing below) as a 1-pad, 3-byte-address QSPI. This works and boots reliably.&lt;/P&gt;&lt;P&gt;Next task is to get the bootloader to switch up the GD25LX into 8-pad, 4-byte address mode.&lt;/P&gt;&lt;P&gt;I've been working through examples in the RM, AN12107, AN12108, AN12183, but their main focus is Hyperflash. I've studied the code documentation in xip/xxxx_flexspi_nor_config.c/h but the comments are terse one-liners. Is there any documentation out there that tells me how to build this struct?&lt;/P&gt;&lt;P&gt;Thanks again for all your help - Eamonn&lt;/P&gt;&lt;LI-CODE lang="c"&gt;const flexspi_nor_config_t qspiflash_config = {
    .memConfig =
        {
            .tag                = FLEXSPI_CFG_BLK_TAG,
            .version            = FLEXSPI_CFG_BLK_VERSION,
            .readSampleClksrc=kFlexSPIReadSampleClk_ExternalInputFromDqsPad,
            .csHoldTime         = 3u,
            .csSetupTime        = 3u,
            .columnAddressWidth = 0u,
			.configCmdEnable    = 0u,
			.controllerMiscOption = 0u,
			.deviceType = kFlexSpiDeviceType_SerialNOR,
            .sflashPadType = kSerialFlash_1Pad,		//kSerialFlash_8Pads
            .serialClkFreq = kFlexSpiSerialClk_100MHz, //kFlexSpiSerialClk_30MHz, 	//kFlexSpiSerialClk_133MHz,
			.lutCustomSeqEnable = 0u,
            .sflashA1Size  = 32u * 1024u * 1024u,
            .dataValidTime = {16u, 16u},
			.lookupTable =
	                {
	                    // Read LUTs
	                    FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x03, RADDR_SDR, FLEXSPI_1PAD, 0x18),
	                    FLEXSPI_LUT_SEQ(READ_SDR, FLEXSPI_1PAD, 0x04, STOP, FLEXSPI_1PAD, 0x0),
	                },
        },
    .pageSize           = 256u,
    .sectorSize         = 4u * 1024u,
    .blockSize          = 64u * 1024u,
    .isUniformBlockSize = true,
};&lt;/LI-CODE&gt;</description>
      <pubDate>Tue, 15 Sep 2020 09:10:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1153369#M10108</guid>
      <dc:creator>eamonnheffernan</dc:creator>
      <dc:date>2020-09-15T09:10:44Z</dc:date>
    </item>
    <item>
      <title>Re: Example of flexspi_nor_config_t for GD25LX256</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1154781#M10141</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/40101"&gt;@jay_heng&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/117617"&gt;@Sabina_Bruce&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi Jay and Sabina,&lt;/P&gt;&lt;P&gt;I hooked up my board to Jay's MCUBootUtility, and flashed it specifying a GD25LX configuration. Flashing seems to go ok (no error messages), but the board is not booting from it.&lt;/P&gt;&lt;P&gt;I've taken the image file and decoded the FDCB back into an initialised struct, and below is what I get:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;const flexspi_nor_config_t hyperflash_config = {
    .memConfig =
        {
            .tag                = FLEXSPI_CFG_BLK_TAG,
            .version            = FLEXSPI_CFG_BLK_VERSION,
            .readSampleClksrc=kFlexSPIReadSampleClk_ExternalInputFromDqsPad,
            .csHoldTime         = 3u,
            .csSetupTime        = 3u,
            .columnAddressWidth = 0u,
			
			.deviceModeCfgEnable = 0,
			.deviceModeType = 0,
			.waitTimeCfgCommands = 0,
			//.deviceModeSeq = 0, //This is a flexspi_lut_seq_t sub-struct.
			.deviceModeArg = 0,
			.configCmdEnable = 0,
			//.configModeType[0..2] = 0,
			//.configCmdSeqs[3] = 0, //This an array of flexspi_lut_seq_t sub-structs.
			//.configCmdArgs0..2] = 0, //Array of uint32_t.
			.controllerMiscOption = 0x00000050, // Enable DDR mode, Safe configuration.
			
			.deviceType = 0x01,	//kFlexSpiDeviceType_SerialNOR
            .sflashPadType = 8, //kSerialFlash_8Pads,
			
            .serialClkFreq = 8, kFlexSpiSerialClk_133MHz,
			
			.lutCustomSeqEnable = 0, //LUT customization disabled.
			
            .sflashA1Size  = 0x2000000, //32u * 1024u * 1024u,
			.sflashA2Size = 0,
			.sflashB1Size = 0,
			.sflashB2Size = 0,
			
			.csPadSettingOverride = 0,
			.sclkPadSettingOverride = 0,
			.dataPadSettingOverride = 0,
			.dqsPadSettingOverride = 0,
			.timeoutInMs = 0,
			.commandInterval = 0,
			
            .dataValidTime = {15u, 0u},
			
			.busyoffset = 0,
			.busyBitPolarity = 0,
            .lookupTable =
                {
                    // Read LUTs as per binary...
                },
        },
	    .pageSize           = 0x100,
	    .sectorSize         = 0x100,
		.ipcmdSerialClkFreq = 1,
	    .isUniformBlockSize = 1,
		.serialNorType = 0,
		.needExitNoCmdMode = 0,
		.halfClkForNonReadCmd = 1,
		.needRestoreNoCmdMode = 0,
		
	    .blockSize          = 64u * 1024u,
};&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;This is the FDCB:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2020-09-17 12-56-26.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/125428iB8612A1AF2E02DA6/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2020-09-17 12-56-26.png" alt="Screenshot from 2020-09-17 12-56-26.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot from 2020-09-17 12-56-26.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Questions for Jay:&lt;/P&gt;&lt;P&gt;1. Where are you getting the information to fill out the flexspi_nor_config struct in your utility tool? I've looked through all the docs I can find, and I can't seem to find any instructions on how to properly fill out this struct. Some of the settings I find puzzling (e.g. sector size).&lt;/P&gt;&lt;P&gt;2. It seems GD25LX powers up in 3B address mode, and would need to be switched up to 4B mode. I assume deviceMode fields or configMode fields could be used to do the configure. Any idea how to do this?&lt;/P&gt;&lt;P&gt;3. Is Octal DTR SPI or DTR OPI better for performance? How would one set up the struct to ask for DTR OPI mode if that is better?&lt;/P&gt;&lt;P&gt;NXP has qualified the GD25LX as a viable bootable flash device. There must be a project somewhere in the vault that was used to test this device. Could this be published to provide an example for using the GD25LX?&lt;/P&gt;&lt;P&gt;Thanks again for your attention and kind help.&lt;/P&gt;&lt;P&gt;Best regards - Eamonn&lt;/P&gt;</description>
      <pubDate>Thu, 17 Sep 2020 12:11:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1154781#M10141</guid>
      <dc:creator>eamonnheffernan</dc:creator>
      <dc:date>2020-09-17T12:11:01Z</dc:date>
    </item>
    <item>
      <title>Re: Example of flexspi_nor_config_t for GD25LX256</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1154791#M10142</link>
      <description>&lt;P&gt;Edit: the initializer line .serialClkFreq = 8, kFlexSpiSerialClk_166MHz, should read //kFlexSpiSerialClk_166MHz.&lt;/P&gt;</description>
      <pubDate>Thu, 17 Sep 2020 12:33:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1154791#M10142</guid>
      <dc:creator>eamonnheffernan</dc:creator>
      <dc:date>2020-09-17T12:33:40Z</dc:date>
    </item>
    <item>
      <title>Re: Example of flexspi_nor_config_t for GD25LX256</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1154875#M10144</link>
      <description>&lt;P&gt;&lt;EM&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/40101"&gt;@jay_heng&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/117617"&gt;@Sabina_Bruce&lt;/a&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Finally&lt;/EM&gt; got something working. I used Jay's utility to create a binary image, then compared the first 0x200 bytes of jay's image (FDCB location) with the first 0x200 of my binary, and worked back to getting a struct that gives an identical 0x200 bytes.&lt;/P&gt;&lt;P&gt;Here's the coded struct below... I have little idea about many of the field decisions because I can't find any docs on how to set them up correctly. This code is the very definition of a pass-it-on whisper! I do sincerely wish that NXP would release some good documentation on how to configure this struct. I don't know yet if this is an optimal configuration. Some testing required to see what performance I get.&lt;/P&gt;&lt;P&gt;Good info in Chapters 9 and 27 of the Reference Manual. Jay's utility can help you configure your FDCB.&lt;/P&gt;&lt;P&gt;Table 9.9 lists the boot pins options. Table 9.14 has the full definition of the FDCB struct. Table 9.15 has the LUT sequence definition for Serial Nor.&lt;/P&gt;&lt;P&gt;In a nutshell:&lt;/P&gt;&lt;P&gt;To get McuXpresso to program the GD25LX, set BOOT_CFG2[2:0] on your board to 0b000 (3B SPI). Big thanks to Sabina for this tip: it was crucial to allow me to program the flash via McuX. I also set up my board so I can force it into USB DFU mode (to work with Jay's utility) by having the option to pull BOOT_CFG1[6] high.&lt;/P&gt;&lt;P&gt;In C/C++ Build/MCU Settings, Memory details, set your Flash memory to the correct address/size, and select &lt;STRONG&gt;MIMXRT1050_SFDP_QSPI.cfx&lt;/STRONG&gt; as your flash driver.&lt;/P&gt;&lt;P&gt;In C/C++ Build/Settings/Mcu C Compiler/Preprocessor, define the following symbols:&lt;/P&gt;&lt;P&gt;XIP_EXTERNAL_FLASH=1&lt;/P&gt;&lt;P&gt;XIP_BOOT_HEADER_ENABLE=1&lt;/P&gt;&lt;P&gt;McuX will automatically create the FDCB and fill it out to allow XIP booting.&lt;/P&gt;&lt;P&gt;If you don't need the ROM bootloader to initialize SDRAM or other peripherals, set XIP_BOOT_HEADER_DCD_ENABLE=0. If you do need SDRAM etc, then set it to 1 and you will need to provide the DCD data block also (Xpresso has a config tool for this).&lt;/P&gt;&lt;P&gt;I hope this is useful to anyone else booting off this flash device. Caveat: I've just got this working and there may be some bugs/mistakes in my code.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Thanks very much to Jay and Sabina for their help in solving this problem.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Eamonn&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;//Based on Jay Heng's McuBootUtility output configured for GD25LX:
const flexspi_nor_config_t hyperflash_config = {
    .memConfig =
        {
            .tag                = FLEXSPI_CFG_BLK_TAG,
            .version            = FLEXSPI_CFG_BLK_VERSION,
            .readSampleClksrc=kFlexSPIReadSampleClk_ExternalInputFromDqsPad,
            .csHoldTime         = 3u,
            .csSetupTime        = 3u,
            .columnAddressWidth = 0u,

			.deviceModeCfgEnable = 0,
			.deviceModeType = 0,
			.waitTimeCfgCommands = 0,
			//.deviceModeSeq = 0, //This is a flexspi_lut_seq_t sub-struct.
			.deviceModeArg = 0,
			.configCmdEnable = 0,
			//.configModeType[0..2] = 0,
			//.configCmdSeqs[3] = 0, //This an array of flexspi_lut_seq_t sub-structs.
			//.configCmdArgs0..2] = 0, //Array of uint32_t.
			.controllerMiscOption = 0x00000050, // Enable DDR mode, Safe configuration.

			.deviceType = 0x01,	//kFlexSpiDeviceType_SerialNOR
            .sflashPadType = 8, //kSerialFlash_8Pads,

            .serialClkFreq = 8, //kFlexSpiSerialClk_166MHz,

			.lutCustomSeqEnable = 0, //LUT customization disabled.

            .sflashA1Size  = 0x2000000, //32u * 1024u * 1024u,
			.sflashA2Size = 0,
			.sflashB1Size = 0,
			.sflashB2Size = 0,

			.csPadSettingOverride = 0,
			.sclkPadSettingOverride = 0,
			.dataPadSettingOverride = 0,
			.dqsPadSettingOverride = 0,
			.timeoutInMs = 0,
			.commandInterval = 0,

            .dataValidTime = {15u, 0u},

			.busyOffset = 0,
			.busyBitPolarity = 0,
            .lookupTable =
                {
                    // Read LUTs as per binary from Jay Heng's MCUBootUtility configured for GD25LX...
					FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xFD,    RADDR_DDR, FLEXSPI_8PAD, 0x20),
					FLEXSPI_LUT_SEQ(DUMMY_DDR, FLEXSPI_8PAD, 0x06,  READ_DDR, FLEXSPI_8PAD, 0x04),
					0,0,

					FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x05,    READ_SDR, FLEXSPI_1PAD, 0x04),
					0,0,0,

					0,0,0,0,

					FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x06,    STOP, FLEXSPI_1PAD, 0x0),
					0,0,0,

					0,0,0,0,

					FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x21,    RADDR_SDR, FLEXSPI_1PAD, 0x20),
					0,0,0,

					0,0,0,0,

					0,0,0,0,

					FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xDC,    RADDR_SDR, FLEXSPI_1PAD, 0x20),
					0,0,0,

					FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x8E,    RADDR_SDR, FLEXSPI_8PAD, 0x20),
					FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_8PAD, 0x80,  STOP, FLEXSPI_1PAD, 0x0),
					0,0,

					0,0,0,0,

					FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x60,    STOP, FLEXSPI_1PAD, 0x0),

                },
        },
	    .pageSize           = 0x100,
	    .sectorSize         = 0x1000,
		.ipcmdSerialClkFreq = 1,
	    .isUniformBlockSize = 0,
		.serialNorType = 0,
		.needExitNoCmdMode = 0,
		.halfClkForNonReadCmd = 1,
		.needRestoreNoCmdMode = 0,

	    .blockSize          = 64u * 1024u,
};&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Sep 2020 14:42:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Example-of-flexspi-nor-config-t-for-GD25LX256/m-p/1154875#M10144</guid>
      <dc:creator>eamonnheffernan</dc:creator>
      <dc:date>2020-09-17T14:42:43Z</dc:date>
    </item>
  </channel>
</rss>