<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックGPIO array ; RT106X</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/GPIO-array-RT106X/m-p/1150986#M10034</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to change 8 GPIO signals at the same time (as close to a single clock) based on the data revived from UART. Or in other words, I want to treat 8 GPIO signals (or any number for that matter) as an array.&lt;/P&gt;&lt;P&gt;Is this possible? If so, How?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;TIA,&lt;/P&gt;</description>
    <pubDate>Wed, 09 Sep 2020 09:13:38 GMT</pubDate>
    <dc:creator>bezalel</dc:creator>
    <dc:date>2020-09-09T09:13:38Z</dc:date>
    <item>
      <title>GPIO array ; RT106X</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/GPIO-array-RT106X/m-p/1150986#M10034</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to change 8 GPIO signals at the same time (as close to a single clock) based on the data revived from UART. Or in other words, I want to treat 8 GPIO signals (or any number for that matter) as an array.&lt;/P&gt;&lt;P&gt;Is this possible? If so, How?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;TIA,&lt;/P&gt;</description>
      <pubDate>Wed, 09 Sep 2020 09:13:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/GPIO-array-RT106X/m-p/1150986#M10034</guid>
      <dc:creator>bezalel</dc:creator>
      <dc:date>2020-09-09T09:13:38Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO array ; RT106X</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/GPIO-array-RT106X/m-p/1151131#M10037</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;If your 8 (or more) pins are connected to the same GPIO port (eg. GPIO1 or GPIO2) any write to that port will result in all of the outputs being updated at the same time.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;EM&gt;[uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Sep 2020 22:09:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/GPIO-array-RT106X/m-p/1151131#M10037</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-09-09T22:09:48Z</dc:date>
    </item>
  </channel>
</rss>