<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 iMXRT1010 SWD interface disabled</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMXRT1010-SWD-interface-disabled/m-p/1150427#M10020</link>
    <description>&lt;P&gt;We built a new hardware based on iMXRT1011 and spent several hours with SWD interface bring up. MCU refused re-programming requests over SWD interface. Then we found 10K pull_down resistor on JTAG_MOD (GPIO_AD_11) in RT1010 reference board schematics that enables SWD interface. Funny thing is that I could not find anything mentioned IMXRT1010RM datasheet.&lt;BR /&gt;Fuse DAP_SJC_SWD_SEL&amp;nbsp; is set to 0 so I would expect that SWD is enabled by default, but it's somehow overridden by GPIO_AD_11 and JTAG is selected when&amp;nbsp;GPIO_AD_11 is floating.&lt;/P&gt;</description>
    <pubDate>Tue, 08 Sep 2020 14:29:16 GMT</pubDate>
    <dc:creator>ladislav_piroha</dc:creator>
    <dc:date>2020-09-08T14:29:16Z</dc:date>
    <item>
      <title>iMXRT1010 SWD interface disabled</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMXRT1010-SWD-interface-disabled/m-p/1150427#M10020</link>
      <description>&lt;P&gt;We built a new hardware based on iMXRT1011 and spent several hours with SWD interface bring up. MCU refused re-programming requests over SWD interface. Then we found 10K pull_down resistor on JTAG_MOD (GPIO_AD_11) in RT1010 reference board schematics that enables SWD interface. Funny thing is that I could not find anything mentioned IMXRT1010RM datasheet.&lt;BR /&gt;Fuse DAP_SJC_SWD_SEL&amp;nbsp; is set to 0 so I would expect that SWD is enabled by default, but it's somehow overridden by GPIO_AD_11 and JTAG is selected when&amp;nbsp;GPIO_AD_11 is floating.&lt;/P&gt;</description>
      <pubDate>Tue, 08 Sep 2020 14:29:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMXRT1010-SWD-interface-disabled/m-p/1150427#M10020</guid>
      <dc:creator>ladislav_piroha</dc:creator>
      <dc:date>2020-09-08T14:29:16Z</dc:date>
    </item>
    <item>
      <title>Re: iMXRT1010 SWD interface disabled</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMXRT1010-SWD-interface-disabled/m-p/1151116#M10035</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your feedback, I will pass it to the documentation team.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also, when creating your own board besides using as reference the reference manual and the datasheet, I highly recommend you to use also the Hardware Development Guide for the RT1010.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/MIMXRT1010HDUG.pdf" target="_blank" rel="noopener"&gt;https://www.nxp.com/docs/en/user-guide/MIMXRT1010HDUG.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;/P&gt;
&lt;P&gt;Victor&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note:&lt;/P&gt;
&lt;P&gt;- If this post answers your question, please click the "Mark Correct"button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;/P&gt;
&lt;P&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Sep 2020 20:51:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMXRT1010-SWD-interface-disabled/m-p/1151116#M10035</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2020-09-09T20:51:08Z</dc:date>
    </item>
  </channel>
</rss>