<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 What is the performance difference between internal SRAM and external SDRAM in RT1050?</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/What-is-the-performance-difference-between-internal-SRAM-and/m-p/804151#M1001</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to transfer data using FlexIO2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FlexIO2 and memory are connected&amp;nbsp;by eDMA and FlexIO2 transfer data&amp;nbsp;at 15Mbps using 16&amp;nbsp;data line and&amp;nbsp;1 clock line&amp;nbsp;&lt;/P&gt;&lt;P&gt;I set SEMC clock to 150MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I transfer 384Kbyte with&amp;nbsp;internal SRAM, it takes about 14ms&lt;/P&gt;&lt;P&gt;But when I transfer 384Kbyte with external SDRAM, it takes about 36ms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it the correct performance difference between internal SRAM and external SDRAM&amp;nbsp;?&lt;/P&gt;&lt;P&gt;Is there any way to improve performace with external SDRAM?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Nov 2018 16:16:45 GMT</pubDate>
    <dc:creator>yongjin2712_cho</dc:creator>
    <dc:date>2018-11-27T16:16:45Z</dc:date>
    <item>
      <title>What is the performance difference between internal SRAM and external SDRAM in RT1050?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/What-is-the-performance-difference-between-internal-SRAM-and/m-p/804151#M1001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to transfer data using FlexIO2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FlexIO2 and memory are connected&amp;nbsp;by eDMA and FlexIO2 transfer data&amp;nbsp;at 15Mbps using 16&amp;nbsp;data line and&amp;nbsp;1 clock line&amp;nbsp;&lt;/P&gt;&lt;P&gt;I set SEMC clock to 150MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I transfer 384Kbyte with&amp;nbsp;internal SRAM, it takes about 14ms&lt;/P&gt;&lt;P&gt;But when I transfer 384Kbyte with external SDRAM, it takes about 36ms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it the correct performance difference between internal SRAM and external SDRAM&amp;nbsp;?&lt;/P&gt;&lt;P&gt;Is there any way to improve performace with external SDRAM?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Nov 2018 16:16:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/What-is-the-performance-difference-between-internal-SRAM-and/m-p/804151#M1001</guid>
      <dc:creator>yongjin2712_cho</dc:creator>
      <dc:date>2018-11-27T16:16:45Z</dc:date>
    </item>
    <item>
      <title>Re: What is the performance difference between internal SRAM and external SDRAM in RT1050?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/What-is-the-performance-difference-between-internal-SRAM-and/m-p/804152#M1002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="320640" data-username="yongjin2712.choi@samsung.com" href="https://community.nxp.com/people/yongjin2712.choi@samsung.com"&gt;YongJin Choi&lt;/A&gt;, &lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1）Is it the correct performance difference between internal SRAM and external SDRAM?&lt;BR /&gt;-- The difference between the SRAM and SDRAM's performance is normal.&lt;BR /&gt;2) Is there any way to improve performance with external SDRAM?&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;SDRAM write performance is good under of DCACHE disable, however, SDRAM read performance increase by 5 times after enabling DCACHE.&lt;/LI&gt;&lt;LI&gt;Better performance on SDRAM write than read, as write operation is pipelined.&lt;/LI&gt;&lt;LI&gt;To balance read and write performance, as well as practices application, recommend to enable CACHE in most case.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Nov 2018 09:17:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/What-is-the-performance-difference-between-internal-SRAM-and/m-p/804152#M1002</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2018-11-28T09:17:08Z</dc:date>
    </item>
  </channel>
</rss>