<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Solutions中的主题 Flutter on IMX93</title>
    <link>https://community.nxp.com/t5/i-MX-Solutions/Flutter-on-IMX93/m-p/2380305#M735</link>
    <description>&lt;P&gt;Hello&lt;BR /&gt;I have an IMX93 board and I'm trying to run a flutter program on it. I'm having a loto of trouble with CPU usage (around 20% for a static screen with a clock that refresh every second, and over 90% for a full page scroll with images). Most of it depends from raster (around 180ms each second in the static screen). I am trying to enable PxP but either I am not able to either flutter can not use it to rasterize.&lt;/P&gt;&lt;P&gt;I saw that flutter uses OpenGl ES, Vulkan and metal as API, so I'm not sure if it is possible to use pxp to help CPU.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Thu, 11 Jun 2026 15:56:33 GMT</pubDate>
    <dc:creator>FedeLucchini</dc:creator>
    <dc:date>2026-06-11T15:56:33Z</dc:date>
    <item>
      <title>Flutter on IMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Solutions/Flutter-on-IMX93/m-p/2380305#M735</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;I have an IMX93 board and I'm trying to run a flutter program on it. I'm having a loto of trouble with CPU usage (around 20% for a static screen with a clock that refresh every second, and over 90% for a full page scroll with images). Most of it depends from raster (around 180ms each second in the static screen). I am trying to enable PxP but either I am not able to either flutter can not use it to rasterize.&lt;/P&gt;&lt;P&gt;I saw that flutter uses OpenGl ES, Vulkan and metal as API, so I'm not sure if it is possible to use pxp to help CPU.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jun 2026 15:56:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Solutions/Flutter-on-IMX93/m-p/2380305#M735</guid>
      <dc:creator>FedeLucchini</dc:creator>
      <dc:date>2026-06-11T15:56:33Z</dc:date>
    </item>
  </channel>
</rss>