<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic M.2 Custom AI Hat board in i.MX Solutions</title>
    <link>https://community.nxp.com/t5/i-MX-Solutions/M-2-Custom-AI-Hat-board/m-p/2370933#M729</link>
    <description>&lt;P&gt;Good morning All, Hope you are doing well.&lt;/P&gt;&lt;P&gt;i have an idea and i want to know if it is applicable or if i will face problems, And i need your recommendations.&lt;/P&gt;&lt;P&gt;currently i am buying NXP I.MX8QM MEK board, and my project idea is to use local LLM on the board, For that i will need AI accelerator.&lt;/P&gt;&lt;P&gt;my current setup is using RPI5 and AI Hat +2 and i want to level up the project so i will use NXP i.mx8QM board, And i want to use the AI Hat +2 with the NXP board&lt;/P&gt;&lt;P&gt;the AI Hat +2 is Hailo-10 H AI acceleration module and it is interfaced with pcie fpc 16 way connector as follows its signal is standard PCIe signals&lt;/P&gt;&lt;P&gt;The following Image shows it.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Mustafa07_1-1779749448515.png" style="width: 356px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/386738iF41265E0897071C6/image-dimensions/356x356?v=v2" width="356" height="356" role="button" title="Mustafa07_1-1779749448515.png" alt="Mustafa07_1-1779749448515.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So i want to use it with the NXP board and i thought to create a custom M.2 Card that just routes the PCIe signals from the Hat to the M.2 like the following image.&lt;/P&gt;&lt;P&gt;this is just a simple example of the board as a explanation.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Mustafa07_0-1779749224507.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/386737iB594AD8AC1659E36/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Mustafa07_0-1779749224507.png" alt="Mustafa07_0-1779749224507.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;so my question, Is what i am thinking of is applicable or there is something i didn't take care of it?&lt;BR /&gt;also if this is applicable do i need a special driver or the linux driver of the hat is enough?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;your answer will help me a lot and thank you in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 25 May 2026 23:01:20 GMT</pubDate>
    <dc:creator>Mustafa07</dc:creator>
    <dc:date>2026-05-25T23:01:20Z</dc:date>
    <item>
      <title>M.2 Custom AI Hat board</title>
      <link>https://community.nxp.com/t5/i-MX-Solutions/M-2-Custom-AI-Hat-board/m-p/2370933#M729</link>
      <description>&lt;P&gt;Good morning All, Hope you are doing well.&lt;/P&gt;&lt;P&gt;i have an idea and i want to know if it is applicable or if i will face problems, And i need your recommendations.&lt;/P&gt;&lt;P&gt;currently i am buying NXP I.MX8QM MEK board, and my project idea is to use local LLM on the board, For that i will need AI accelerator.&lt;/P&gt;&lt;P&gt;my current setup is using RPI5 and AI Hat +2 and i want to level up the project so i will use NXP i.mx8QM board, And i want to use the AI Hat +2 with the NXP board&lt;/P&gt;&lt;P&gt;the AI Hat +2 is Hailo-10 H AI acceleration module and it is interfaced with pcie fpc 16 way connector as follows its signal is standard PCIe signals&lt;/P&gt;&lt;P&gt;The following Image shows it.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Mustafa07_1-1779749448515.png" style="width: 356px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/386738iF41265E0897071C6/image-dimensions/356x356?v=v2" width="356" height="356" role="button" title="Mustafa07_1-1779749448515.png" alt="Mustafa07_1-1779749448515.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So i want to use it with the NXP board and i thought to create a custom M.2 Card that just routes the PCIe signals from the Hat to the M.2 like the following image.&lt;/P&gt;&lt;P&gt;this is just a simple example of the board as a explanation.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Mustafa07_0-1779749224507.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/386737iB594AD8AC1659E36/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Mustafa07_0-1779749224507.png" alt="Mustafa07_0-1779749224507.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;so my question, Is what i am thinking of is applicable or there is something i didn't take care of it?&lt;BR /&gt;also if this is applicable do i need a special driver or the linux driver of the hat is enough?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;your answer will help me a lot and thank you in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 25 May 2026 23:01:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Solutions/M-2-Custom-AI-Hat-board/m-p/2370933#M729</guid>
      <dc:creator>Mustafa07</dc:creator>
      <dc:date>2026-05-25T23:01:20Z</dc:date>
    </item>
  </channel>
</rss>