<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic GPS support on IMX6Q Sabre board in i.MX Solutions</title>
    <link>https://community.nxp.com/t5/i-MX-Solutions/GPS-support-on-IMX6Q-Sabre-board/m-p/2344676#M714</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I would like to know if it is possible to use GPS on the IMX6Q Sabre board.&lt;/P&gt;&lt;P&gt;If yes, could you please explain how it can be implemented?&lt;BR /&gt;Also, do we need to add an external GPS module, or is there built-in support?&lt;/P&gt;&lt;P&gt;Thank you in advance for your help.&lt;/P&gt;</description>
    <pubDate>Thu, 02 Apr 2026 13:38:40 GMT</pubDate>
    <dc:creator>Mortada</dc:creator>
    <dc:date>2026-04-02T13:38:40Z</dc:date>
    <item>
      <title>GPS support on IMX6Q Sabre board</title>
      <link>https://community.nxp.com/t5/i-MX-Solutions/GPS-support-on-IMX6Q-Sabre-board/m-p/2344676#M714</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I would like to know if it is possible to use GPS on the IMX6Q Sabre board.&lt;/P&gt;&lt;P&gt;If yes, could you please explain how it can be implemented?&lt;BR /&gt;Also, do we need to add an external GPS module, or is there built-in support?&lt;/P&gt;&lt;P&gt;Thank you in advance for your help.&lt;/P&gt;</description>
      <pubDate>Thu, 02 Apr 2026 13:38:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Solutions/GPS-support-on-IMX6Q-Sabre-board/m-p/2344676#M714</guid>
      <dc:creator>Mortada</dc:creator>
      <dc:date>2026-04-02T13:38:40Z</dc:date>
    </item>
  </channel>
</rss>