<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX SolutionsのトピックiMX8MPLUS - ANDROID BSP</title>
    <link>https://community.nxp.com/t5/i-MX-Solutions/iMX8MPLUS-ANDROID-BSP/m-p/2180342#M660</link>
    <description>&lt;P&gt;&lt;STRONG&gt;Hello,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am new to the i.MX platform and Android BSP.&lt;BR /&gt;I am using i.MX8M Plus with the NXP Android BSP, and I am developing a display system (digital cluster) that communicates with the CAN bus.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I want to confirm if my understanding of the process is correct:-&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;-&amp;gt; I download and flash the Android BSP image from NXP (which includes the Linux kernel and CAN drivers).&lt;/P&gt;&lt;P&gt;-&amp;gt;The BSP already supports SocketCAN, so I don’t need to modify the CAN HAL or kernel code.&lt;/P&gt;&lt;P&gt;-&amp;gt;From Android Studio, I can build an app that:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; -Opens the SocketCAN interface (e.g.,can0 using C/C++ via NDK/JNI&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; -Receives CAN frames from the bus&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; -Decodes them and updates UI variables (like speed, RPM, etc.) in the Android app&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;(Java/Kotlin layer)&lt;/P&gt;&lt;P&gt;-&amp;gt;In the future, I plan to add camera and navigation features, which I also plan to implement in the same Android Studio app.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Could you please confirm:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;-&amp;gt; Is this overall approach correct for using CAN communication in an Android BSP environment?&lt;/P&gt;&lt;P&gt;-&amp;gt; Is it the right way to open and read SocketCAN data from an app using Android Studio (through JNI)?&lt;/P&gt;&lt;P&gt;-&amp;gt; For camera and navigation integration, is it also fine to develop them directly in Android Studio (application layer)?&lt;/P&gt;&lt;P&gt;-&amp;gt;If this process is not correct, could you please explain the proper method or architecture I should follow?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am very new to this platform, so I would really appreciate a clear explanation or references to official documentation that describes the correct flow for Android BSP development with CAN.&lt;/P&gt;</description>
    <pubDate>Mon, 06 Oct 2025 04:44:05 GMT</pubDate>
    <dc:creator>parvathitp</dc:creator>
    <dc:date>2025-10-06T04:44:05Z</dc:date>
    <item>
      <title>iMX8MPLUS - ANDROID BSP</title>
      <link>https://community.nxp.com/t5/i-MX-Solutions/iMX8MPLUS-ANDROID-BSP/m-p/2180342#M660</link>
      <description>&lt;P&gt;&lt;STRONG&gt;Hello,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am new to the i.MX platform and Android BSP.&lt;BR /&gt;I am using i.MX8M Plus with the NXP Android BSP, and I am developing a display system (digital cluster) that communicates with the CAN bus.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I want to confirm if my understanding of the process is correct:-&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;-&amp;gt; I download and flash the Android BSP image from NXP (which includes the Linux kernel and CAN drivers).&lt;/P&gt;&lt;P&gt;-&amp;gt;The BSP already supports SocketCAN, so I don’t need to modify the CAN HAL or kernel code.&lt;/P&gt;&lt;P&gt;-&amp;gt;From Android Studio, I can build an app that:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; -Opens the SocketCAN interface (e.g.,can0 using C/C++ via NDK/JNI&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; -Receives CAN frames from the bus&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; -Decodes them and updates UI variables (like speed, RPM, etc.) in the Android app&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;(Java/Kotlin layer)&lt;/P&gt;&lt;P&gt;-&amp;gt;In the future, I plan to add camera and navigation features, which I also plan to implement in the same Android Studio app.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Could you please confirm:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;-&amp;gt; Is this overall approach correct for using CAN communication in an Android BSP environment?&lt;/P&gt;&lt;P&gt;-&amp;gt; Is it the right way to open and read SocketCAN data from an app using Android Studio (through JNI)?&lt;/P&gt;&lt;P&gt;-&amp;gt; For camera and navigation integration, is it also fine to develop them directly in Android Studio (application layer)?&lt;/P&gt;&lt;P&gt;-&amp;gt;If this process is not correct, could you please explain the proper method or architecture I should follow?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am very new to this platform, so I would really appreciate a clear explanation or references to official documentation that describes the correct flow for Android BSP development with CAN.&lt;/P&gt;</description>
      <pubDate>Mon, 06 Oct 2025 04:44:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Solutions/iMX8MPLUS-ANDROID-BSP/m-p/2180342#M660</guid>
      <dc:creator>parvathitp</dc:creator>
      <dc:date>2025-10-06T04:44:05Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MPLUS - ANDROID BSP</title>
      <link>https://community.nxp.com/t5/i-MX-Solutions/iMX8MPLUS-ANDROID-BSP/m-p/2180930#M661</link>
      <description>&lt;P&gt;Could you please reply soon? It would be very helpful for me&lt;/P&gt;</description>
      <pubDate>Tue, 07 Oct 2025 04:25:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Solutions/iMX8MPLUS-ANDROID-BSP/m-p/2180930#M661</guid>
      <dc:creator>parvathitp</dc:creator>
      <dc:date>2025-10-07T04:25:15Z</dc:date>
    </item>
  </channel>
</rss>