<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Config Tools for i.MX custom Vid:Pid in i.MX Solutions</title>
    <link>https://community.nxp.com/t5/i-MX-Solutions/Config-Tools-for-i-MX-custom-Vid-Pid/m-p/2093697#M614</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;If you are using Config tools for i.MX 25.03, you can edit the following file to use custom pid/vid&lt;/P&gt;
&lt;P&gt;"C:\nxp\i.MX_CFG_25.06_EAR2\bin\python3\spsdk\data\devices\mimx9596\database.yaml"&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Adrian&lt;/P&gt;</description>
    <pubDate>Thu, 08 May 2025 13:56:21 GMT</pubDate>
    <dc:creator>addiyi</dc:creator>
    <dc:date>2025-05-08T13:56:21Z</dc:date>
    <item>
      <title>Config Tools for i.MX custom Vid:Pid</title>
      <link>https://community.nxp.com/t5/i-MX-Solutions/Config-Tools-for-i-MX-custom-Vid-Pid/m-p/2093689#M613</link>
      <description>&lt;P&gt;Hi!&lt;BR /&gt;When trying to run the DDR stress test on a device which has been fused with a custom Vid:Pid the tests fail. Performing the test on a device which has the default Vid:Pid fuses, the test succeeds. I believe that the issue is related to the sdps_comm load binary image mechanism.&lt;/P&gt;</description>
      <pubDate>Thu, 08 May 2025 13:29:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Solutions/Config-Tools-for-i-MX-custom-Vid-Pid/m-p/2093689#M613</guid>
      <dc:creator>eaemlogic</dc:creator>
      <dc:date>2025-05-08T13:29:19Z</dc:date>
    </item>
    <item>
      <title>Re: Config Tools for i.MX custom Vid:Pid</title>
      <link>https://community.nxp.com/t5/i-MX-Solutions/Config-Tools-for-i-MX-custom-Vid-Pid/m-p/2093697#M614</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;If you are using Config tools for i.MX 25.03, you can edit the following file to use custom pid/vid&lt;/P&gt;
&lt;P&gt;"C:\nxp\i.MX_CFG_25.06_EAR2\bin\python3\spsdk\data\devices\mimx9596\database.yaml"&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Adrian&lt;/P&gt;</description>
      <pubDate>Thu, 08 May 2025 13:56:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Solutions/Config-Tools-for-i-MX-custom-Vid-Pid/m-p/2093697#M614</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2025-05-08T13:56:21Z</dc:date>
    </item>
    <item>
      <title>Re: Config Tools for i.MX custom Vid:Pid</title>
      <link>https://community.nxp.com/t5/i-MX-Solutions/Config-Tools-for-i-MX-custom-Vid-Pid/m-p/2094616#M615</link>
      <description>&lt;P&gt;That did unfortunately not do it, I see that there are some libuuu dependencies to this python back-end, maybe that has to be updated also?&lt;/P&gt;</description>
      <pubDate>Fri, 09 May 2025 12:28:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Solutions/Config-Tools-for-i-MX-custom-Vid-Pid/m-p/2094616#M615</guid>
      <dc:creator>eaemlogic</dc:creator>
      <dc:date>2025-05-09T12:28:04Z</dc:date>
    </item>
  </channel>
</rss>