<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX SolutionsのトピックUSB Camera Interface with iMX6 SABRE</title>
    <link>https://community.nxp.com/t5/i-MX-Solutions/USB-Camera-Interface-with-iMX6-SABRE/m-p/1169292#M6</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using iMX6 SABRELITE for my application development. I need to interface usb camera to the board. In a simple way, i need to test it using vlc installed on board. I can see the camera module detected as 'video4' in '/dev/video*'. Once i run the vlc, it shows....&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;[006ddb58] main libvlc: Running vlc with the default interface. Use 'cvlc' to use vlc without interface.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[0073f9f8] main playlist: playlist is empty&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;and nothing happens.&lt;/P&gt;&lt;P&gt;Please suggest!&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Mon, 19 Oct 2020 03:48:52 GMT</pubDate>
    <dc:creator>i_ashok_s</dc:creator>
    <dc:date>2020-10-19T03:48:52Z</dc:date>
    <item>
      <title>USB Camera Interface with iMX6 SABRE</title>
      <link>https://community.nxp.com/t5/i-MX-Solutions/USB-Camera-Interface-with-iMX6-SABRE/m-p/1169292#M6</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using iMX6 SABRELITE for my application development. I need to interface usb camera to the board. In a simple way, i need to test it using vlc installed on board. I can see the camera module detected as 'video4' in '/dev/video*'. Once i run the vlc, it shows....&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;[006ddb58] main libvlc: Running vlc with the default interface. Use 'cvlc' to use vlc without interface.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;[0073f9f8] main playlist: playlist is empty&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;and nothing happens.&lt;/P&gt;&lt;P&gt;Please suggest!&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Mon, 19 Oct 2020 03:48:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Solutions/USB-Camera-Interface-with-iMX6-SABRE/m-p/1169292#M6</guid>
      <dc:creator>i_ashok_s</dc:creator>
      <dc:date>2020-10-19T03:48:52Z</dc:date>
    </item>
    <item>
      <title>Re: USB Camera Interface with iMX6 SABRE</title>
      <link>https://community.nxp.com/t5/i-MX-Solutions/USB-Camera-Interface-with-iMX6-SABRE/m-p/1195968#M27</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The log remind you "&lt;EM&gt;&lt;STRONG&gt;Use 'cvlc' to use vlc without interface&lt;/STRONG&gt;&lt;/EM&gt;"&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; it means you should use cvlc command, not vlc.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;
&lt;P&gt;B.R,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;</description>
      <pubDate>Wed, 09 Dec 2020 04:28:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Solutions/USB-Camera-Interface-with-iMX6-SABRE/m-p/1195968#M27</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2020-12-09T04:28:42Z</dc:date>
    </item>
  </channel>
</rss>