<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Solutionsのトピック[IMX8MN] Android13 ADB Not Responding When Using USB Hub with NXP Development Board</title>
    <link>https://community.nxp.com/t5/i-MX-Solutions/IMX8MN-Android13-ADB-Not-Responding-When-Using-USB-Hub-with-NXP/m-p/2004898#M546</link>
    <description>&lt;P&gt;I am currently working with an NXP development board (evk 8mn) running Android 13 BSP, and I am experiencing an issue where ADB does not work when the Android device is connected through a USB Hub. When I connect my Android device directly to the USB port, ADB works perfectly, and I can see the device listed via &lt;FONT face="andale mono,times" color="#800000"&gt;adb devices&lt;/FONT&gt;. However, when I connect the Android device through a USB Hub, while other USB devices such as a mouse or a USB flash drive are recognized, ADB does not respond, and the Android device is not listed in ADB.&lt;/P&gt;&lt;P&gt;Additionally, I have tried several USB Hubs, including powered ones, but the problem persists.&lt;/P&gt;&lt;P&gt;Has anyone experienced similar issues, or does anyone have suggestions on how to debug or resolve this ADB connectivity issue when using a USB Hub? Any help or guidance would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
    <pubDate>Mon, 02 Dec 2024 07:33:51 GMT</pubDate>
    <dc:creator>phoebe0511</dc:creator>
    <dc:date>2024-12-02T07:33:51Z</dc:date>
    <item>
      <title>[IMX8MN] Android13 ADB Not Responding When Using USB Hub with NXP Development Board</title>
      <link>https://community.nxp.com/t5/i-MX-Solutions/IMX8MN-Android13-ADB-Not-Responding-When-Using-USB-Hub-with-NXP/m-p/2004898#M546</link>
      <description>&lt;P&gt;I am currently working with an NXP development board (evk 8mn) running Android 13 BSP, and I am experiencing an issue where ADB does not work when the Android device is connected through a USB Hub. When I connect my Android device directly to the USB port, ADB works perfectly, and I can see the device listed via &lt;FONT face="andale mono,times" color="#800000"&gt;adb devices&lt;/FONT&gt;. However, when I connect the Android device through a USB Hub, while other USB devices such as a mouse or a USB flash drive are recognized, ADB does not respond, and the Android device is not listed in ADB.&lt;/P&gt;&lt;P&gt;Additionally, I have tried several USB Hubs, including powered ones, but the problem persists.&lt;/P&gt;&lt;P&gt;Has anyone experienced similar issues, or does anyone have suggestions on how to debug or resolve this ADB connectivity issue when using a USB Hub? Any help or guidance would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
      <pubDate>Mon, 02 Dec 2024 07:33:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Solutions/IMX8MN-Android13-ADB-Not-Responding-When-Using-USB-Hub-with-NXP/m-p/2004898#M546</guid>
      <dc:creator>phoebe0511</dc:creator>
      <dc:date>2024-12-02T07:33:51Z</dc:date>
    </item>
  </channel>
</rss>