<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Solutionsのトピックimx kernel fails to load</title>
    <link>https://community.nxp.com/t5/i-MX-Solutions/imx-kernel-fails-to-load/m-p/1754854#M379</link>
    <description>&lt;P&gt;mmc0(part 0) is current device&lt;BR /&gt;Scanning mmc 0:1...&lt;BR /&gt;Failed to load '/'&lt;BR /&gt;MMC: no card present&lt;BR /&gt;optee optee: OP-TEE api uid mismatch&lt;BR /&gt;Unable to open OP-TEE session (err=-19)&lt;BR /&gt;mm_communicate failed!&lt;BR /&gt;Error: Cannot initialize UEFI sub-system, r = 3&lt;BR /&gt;Running BSP bootcmd ...&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0(part 0) is current device&lt;BR /&gt;Failed to load 'boot.scr'&lt;BR /&gt;32262656 bytes read in 192 ms (160.2 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;61388 bytes read in 15 ms (3.9 MiB/s)&lt;BR /&gt;792 bytes read in 4 ms (193.4 KiB/s)&lt;BR /&gt;Working FDT set to 43000000&lt;BR /&gt;## Flattened Device Tree blob at 43000000&lt;BR /&gt;Booting using the fdt blob at 0x43000000&lt;BR /&gt;Working FDT set to 43000000&lt;BR /&gt;clk usb1_phy_root_clk already disabled&lt;BR /&gt;clk usb2_phy_root_clk already disabled&lt;BR /&gt;Using Device Tree in place at 0000000043000000, end 0000000043012fff&lt;BR /&gt;Working FDT set to 43000000&lt;/P&gt;</description>
    <pubDate>Thu, 30 Nov 2023 06:21:41 GMT</pubDate>
    <dc:creator>solve_this</dc:creator>
    <dc:date>2023-11-30T06:21:41Z</dc:date>
    <item>
      <title>imx kernel fails to load</title>
      <link>https://community.nxp.com/t5/i-MX-Solutions/imx-kernel-fails-to-load/m-p/1754854#M379</link>
      <description>&lt;P&gt;mmc0(part 0) is current device&lt;BR /&gt;Scanning mmc 0:1...&lt;BR /&gt;Failed to load '/'&lt;BR /&gt;MMC: no card present&lt;BR /&gt;optee optee: OP-TEE api uid mismatch&lt;BR /&gt;Unable to open OP-TEE session (err=-19)&lt;BR /&gt;mm_communicate failed!&lt;BR /&gt;Error: Cannot initialize UEFI sub-system, r = 3&lt;BR /&gt;Running BSP bootcmd ...&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0(part 0) is current device&lt;BR /&gt;Failed to load 'boot.scr'&lt;BR /&gt;32262656 bytes read in 192 ms (160.2 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;61388 bytes read in 15 ms (3.9 MiB/s)&lt;BR /&gt;792 bytes read in 4 ms (193.4 KiB/s)&lt;BR /&gt;Working FDT set to 43000000&lt;BR /&gt;## Flattened Device Tree blob at 43000000&lt;BR /&gt;Booting using the fdt blob at 0x43000000&lt;BR /&gt;Working FDT set to 43000000&lt;BR /&gt;clk usb1_phy_root_clk already disabled&lt;BR /&gt;clk usb2_phy_root_clk already disabled&lt;BR /&gt;Using Device Tree in place at 0000000043000000, end 0000000043012fff&lt;BR /&gt;Working FDT set to 43000000&lt;/P&gt;</description>
      <pubDate>Thu, 30 Nov 2023 06:21:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Solutions/imx-kernel-fails-to-load/m-p/1754854#M379</guid>
      <dc:creator>solve_this</dc:creator>
      <dc:date>2023-11-30T06:21:41Z</dc:date>
    </item>
  </channel>
</rss>