<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Solutions中的主题 Netx TCP multipart not working in http server</title>
    <link>https://community.nxp.com/t5/i-MX-Solutions/Netx-TCP-multipart-not-working-in-http-server/m-p/1301917#M160</link>
    <description>&lt;P&gt;I am using Azure http server using netx library on IMX1064 processor. The Client is posting large data which is spit into multiple TCP packets using HTTP PUT. I have a custom handler on the server side.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When the multipart data is received, I get only the first PUT packet on the server but the additional packets with multipart boundary do not&amp;nbsp; show up in the netx http server.&lt;/P&gt;&lt;P&gt;I can see the packets are coming when I sniff the traffic using wireshark.&lt;/P&gt;</description>
    <pubDate>Fri, 02 Jul 2021 16:01:06 GMT</pubDate>
    <dc:creator>MAUZ</dc:creator>
    <dc:date>2021-07-02T16:01:06Z</dc:date>
    <item>
      <title>Netx TCP multipart not working in http server</title>
      <link>https://community.nxp.com/t5/i-MX-Solutions/Netx-TCP-multipart-not-working-in-http-server/m-p/1301917#M160</link>
      <description>&lt;P&gt;I am using Azure http server using netx library on IMX1064 processor. The Client is posting large data which is spit into multiple TCP packets using HTTP PUT. I have a custom handler on the server side.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When the multipart data is received, I get only the first PUT packet on the server but the additional packets with multipart boundary do not&amp;nbsp; show up in the netx http server.&lt;/P&gt;&lt;P&gt;I can see the packets are coming when I sniff the traffic using wireshark.&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jul 2021 16:01:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Solutions/Netx-TCP-multipart-not-working-in-http-server/m-p/1301917#M160</guid>
      <dc:creator>MAUZ</dc:creator>
      <dc:date>2021-07-02T16:01:06Z</dc:date>
    </item>
  </channel>
</rss>