<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Question about DCD setting in imximage.cfg in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-about-DCD-setting-in-imximage-cfg/m-p/653111#M99975</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;I want to clarify DDR initialization for i.MX7D so I'm checking the following file.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx7dsabresd/imximage.cfg?h=imx_v2016.03_4.1.15_2.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx7dsabresd/imximage.cfg?h=imx_v2016.03_4.1.15_2.0.0_ga"&gt;uboot-imx.git - Freescale i.MX u-boot Tree&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;There are two registers which is not described in reference manual as below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Clear then set bit30 to ensure exit from DDR retention */&lt;BR /&gt;DATA 4 0x30360388 0x40000000&lt;BR /&gt;DATA 4 0x30360384 0x40000000&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Q1&lt;BR /&gt;What function of those registers ?&lt;BR /&gt;According to the section 2.1.5 AIPS Memory Map, it supposed to be CCM Analog register.&lt;BR /&gt;However, there are no description in RM so please tell me the function of the register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q2&lt;BR /&gt;Why do you set 0x40000000 to 0x30360388 and 0x30360384 ?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Q3&lt;BR /&gt;I also checked following thread.&lt;BR /&gt;Do I need to post this question to SR ?&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/870552"&gt;https://community.nxp.com/message/870552&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ko-hey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Feb 2017 04:33:56 GMT</pubDate>
    <dc:creator>ko-hey</dc:creator>
    <dc:date>2017-02-21T04:33:56Z</dc:date>
    <item>
      <title>Question about DCD setting in imximage.cfg</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-about-DCD-setting-in-imximage-cfg/m-p/653111#M99975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;I want to clarify DDR initialization for i.MX7D so I'm checking the following file.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx7dsabresd/imximage.cfg?h=imx_v2016.03_4.1.15_2.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx7dsabresd/imximage.cfg?h=imx_v2016.03_4.1.15_2.0.0_ga"&gt;uboot-imx.git - Freescale i.MX u-boot Tree&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;There are two registers which is not described in reference manual as below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Clear then set bit30 to ensure exit from DDR retention */&lt;BR /&gt;DATA 4 0x30360388 0x40000000&lt;BR /&gt;DATA 4 0x30360384 0x40000000&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Q1&lt;BR /&gt;What function of those registers ?&lt;BR /&gt;According to the section 2.1.5 AIPS Memory Map, it supposed to be CCM Analog register.&lt;BR /&gt;However, there are no description in RM so please tell me the function of the register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q2&lt;BR /&gt;Why do you set 0x40000000 to 0x30360388 and 0x30360384 ?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Q3&lt;BR /&gt;I also checked following thread.&lt;BR /&gt;Do I need to post this question to SR ?&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/870552"&gt;https://community.nxp.com/message/870552&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ko-hey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Feb 2017 04:33:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-about-DCD-setting-in-imximage-cfg/m-p/653111#M99975</guid>
      <dc:creator>ko-hey</dc:creator>
      <dc:date>2017-02-21T04:33:56Z</dc:date>
    </item>
    <item>
      <title>Re: Question about DCD setting in imximage.cfg</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-about-DCD-setting-in-imximage-cfg/m-p/653112#M99976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I sent You some information directly via e-mail.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Feb 2017 08:13:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-about-DCD-setting-in-imximage-cfg/m-p/653112#M99976</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-02-21T08:13:02Z</dc:date>
    </item>
  </channel>
</rss>