<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックgstreamer play failed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/gstreamer-play-failed/m-p/652764#M99918</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; I used imx6q which linux kernel version is 3.14.52.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; I use gstreamer to play media .&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; but always failed .The debug message is blew&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(gst-plugin-scanner:578): GLib-GObject-WARNING **: cannot register existing type 'GstImxCompositorPad'&lt;/P&gt;&lt;P&gt;(gst-plugin-scanner:578): GLib-CRITICAL **: g_once_init_leave: assertion 'result != 0' failed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to fixed it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Nov 2016 09:38:19 GMT</pubDate>
    <dc:creator>senli</dc:creator>
    <dc:date>2016-11-11T09:38:19Z</dc:date>
    <item>
      <title>gstreamer play failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/gstreamer-play-failed/m-p/652764#M99918</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; I used imx6q which linux kernel version is 3.14.52.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; I use gstreamer to play media .&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; but always failed .The debug message is blew&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(gst-plugin-scanner:578): GLib-GObject-WARNING **: cannot register existing type 'GstImxCompositorPad'&lt;/P&gt;&lt;P&gt;(gst-plugin-scanner:578): GLib-CRITICAL **: g_once_init_leave: assertion 'result != 0' failed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to fixed it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Nov 2016 09:38:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/gstreamer-play-failed/m-p/652764#M99918</guid>
      <dc:creator>senli</dc:creator>
      <dc:date>2016-11-11T09:38:19Z</dc:date>
    </item>
    <item>
      <title>Re: gstreamer play failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/gstreamer-play-failed/m-p/652765#M99919</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sen Li, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a similar issue explained on the following external forum:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.toradex.com/community/questions/1244/couldnt-make-gsreamer-works-on-core-image-minimal.html" title="https://www.toradex.com/community/questions/1244/couldnt-make-gsreamer-works-on-core-image-minimal.html"&gt;Couldn't make gsreamer works on core image minimal with qt5 eglfs - Toradex Community&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The solution listed there is removing a plugin that apparently has an X11 dependency by adding the following line to local.conf.&lt;/P&gt;&lt;P&gt;PACKAGECONFIG_remove_pn-gstreamer1.0-plugins-good = " gdk-pixbuf "&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe this will help!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Nov 2016 17:06:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/gstreamer-play-failed/m-p/652765#M99919</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-11-11T17:06:25Z</dc:date>
    </item>
  </channel>
</rss>