<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.mx solox boot from QSPI1B in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx-solox-boot-from-QSPI1B/m-p/652762#M99916</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey&lt;/P&gt;&lt;P&gt;I have a custom board with an i.mx 6sx which is based on the sabresd desgin.&lt;/P&gt;&lt;P&gt;I've connected a n25Q256a QSPI device to QSPI 1B.&lt;/P&gt;&lt;P&gt;Is it possible to boot from this device?&amp;nbsp;&lt;/P&gt;&lt;P&gt;In my tests i see that on POR (or with bmode) only the QSPI 1A or QSPI2A are accessed be the boot ROM.&lt;/P&gt;&lt;P&gt;also, the fuses / GPIOS can only be configured for QSPI1 or QSPI2 and does not give an option to configure A or B inside a specific controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Asaf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Mar 2017 08:25:15 GMT</pubDate>
    <dc:creator>asafelias</dc:creator>
    <dc:date>2017-03-15T08:25:15Z</dc:date>
    <item>
      <title>i.mx solox boot from QSPI1B</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx-solox-boot-from-QSPI1B/m-p/652762#M99916</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey&lt;/P&gt;&lt;P&gt;I have a custom board with an i.mx 6sx which is based on the sabresd desgin.&lt;/P&gt;&lt;P&gt;I've connected a n25Q256a QSPI device to QSPI 1B.&lt;/P&gt;&lt;P&gt;Is it possible to boot from this device?&amp;nbsp;&lt;/P&gt;&lt;P&gt;In my tests i see that on POR (or with bmode) only the QSPI 1A or QSPI2A are accessed be the boot ROM.&lt;/P&gt;&lt;P&gt;also, the fuses / GPIOS can only be configured for QSPI1 or QSPI2 and does not give an option to configure A or B inside a specific controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Asaf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Mar 2017 08:25:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx-solox-boot-from-QSPI1B/m-p/652762#M99916</guid>
      <dc:creator>asafelias</dc:creator>
      <dc:date>2017-03-15T08:25:15Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx solox boot from QSPI1B</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx-solox-boot-from-QSPI1B/m-p/652763#M99917</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Asaf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;presence port B is defined in Table 8-26. QuadSPI configuration parameters &lt;BR /&gt;i.MX6SX Reference Manual (rev.1&amp;nbsp; 6/2016)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Serial Flash Port B Selection&amp;nbsp; :&amp;nbsp;&amp;nbsp; Port A is always available. This field informs the device&lt;/P&gt;&lt;P&gt;ROM about the availability of Port B.&lt;/P&gt;&lt;P&gt;&lt;A class="" href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf" title="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So seems port A is always needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Mar 2017 11:20:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx-solox-boot-from-QSPI1B/m-p/652763#M99917</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-03-15T11:20:08Z</dc:date>
    </item>
  </channel>
</rss>