<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: ask help about IMX6Q/D PWM for LVDS backlight</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ask-help-about-IMX6Q-D-PWM-for-LVDS-backlight/m-p/652575#M99873</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I have fixed this case.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Actually, it is caused by a gpio controller to a power chip for LVDS, while not caused by the PWM. gpio6-15 is used here. We used hannstart_cabc function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------&lt;/P&gt;&lt;P&gt;&amp;nbsp; hannstar_cabc {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;compatible = "hannstar,cabc";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;lvds0 {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;gpios = &amp;lt;&amp;amp;gpio6 15 GPIO_ACTIVE_HIGH&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; cabc-enable;&amp;nbsp;&amp;nbsp;&amp;nbsp;//It is very&amp;nbsp;important here. Or it will reverse&amp;nbsp;the configuration.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;};&lt;BR /&gt;&amp;nbsp;&amp;nbsp;lvds1 {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;gpios = &amp;lt;&amp;amp;gpio6 16 GPIO_ACTIVE_HIGH&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;};&lt;BR /&gt;&amp;nbsp;};&lt;/P&gt;&lt;P&gt;----------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; And we have noticed that we should add a 'cabc-enable' here. Or the PIN will be set to LOW if you define ACTIVE_HIGH here.&amp;nbsp;It is not easy to add it, as there is no reference to configure the hannstart_cabc. I just checked and found it in the source code of kernel. It is suggest that NXP&amp;nbsp;could add some introduction in the txt file, to make it easy&amp;nbsp;to user. :smileyhappy:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR//Denny&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Jan 2017 14:28:39 GMT</pubDate>
    <dc:creator>dennyzhou</dc:creator>
    <dc:date>2017-01-03T14:28:39Z</dc:date>
    <item>
      <title>ask help about IMX6Q/D PWM for LVDS backlight</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ask-help-about-IMX6Q-D-PWM-for-LVDS-backlight/m-p/652574#M99872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP engineers,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; We are using IMX6D/Q to drive a 7' LVDS&amp;amp;TS display, with resolution 1024x600.&amp;nbsp;There is some problem about the PWM setting for the backlight. We use PWM3(SD1_DAT1) instead of the PWM1(SD1_DAT3). So we add some configuration data in 'imx6qdl-sabresd.dtsi'.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;... ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;pwm-backlight {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;compatible = "pwm-backlight";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;pwms = &amp;lt;&amp;amp;pwm3 0 50000&amp;gt;; //50us,20k&lt;BR /&gt;&amp;nbsp;&amp;nbsp;brightness-levels = &amp;lt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;0&amp;nbsp; /*1&amp;nbsp; 2&amp;nbsp; 3&amp;nbsp; 4&amp;nbsp; 5&amp;nbsp; 6*/&amp;nbsp; 7&amp;nbsp; 8&amp;nbsp; 9&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;10 11 12 13 14 15 16 17 18 19&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;20 21 22 23 24 25 26 27 28 29&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;30 31 32 33 34 35 36 37 38 39&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;40 41 42 43 44 45 46 47 48 49&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;50 51 52 53 54 55 56 57 58 59&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;60 61 62 63 64 65 66 67 68 69&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;70 71 72 73 74 75 76 77 78 79&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;80 81 82 83 84 85 86 87 88 89&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;90 91 92 93 94 95 96 97 98 99&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;100&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;default-brightness-level = &amp;lt;84&amp;gt;; //90, means 90% duty cycle&lt;BR /&gt;&amp;nbsp;&amp;nbsp;status = "okay";&lt;/P&gt;&lt;P&gt;... ...&lt;/P&gt;&lt;P&gt;... ...&lt;/P&gt;&lt;P&gt;pinctrl_pwm3: pwm3grp {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;fsl,pins = &amp;lt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;MX6QDL_PAD_SD1_DAT1__PWM3_OUT&amp;nbsp;&amp;nbsp;0x1b0b1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;};&lt;/P&gt;&lt;P&gt;... ...&lt;/P&gt;&lt;P&gt;... ...&lt;/P&gt;&lt;P&gt;&amp;amp;pwm3 {&lt;BR /&gt;&amp;nbsp;pinctrl-names = "default";&lt;BR /&gt;&amp;nbsp;pinctrl-0 = &amp;lt;&amp;amp;pinctrl_pwm3&amp;gt;;&lt;BR /&gt;&amp;nbsp;status = "okay";&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;... ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;amp;ldb {&lt;BR /&gt;&amp;nbsp;status = "okay";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;A href="mailto:lvds-channel@0"&gt;lvds-channel@0&lt;/A&gt; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;fsl,data-mapping = "spwg";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;fsl,data-width = &amp;lt;24&amp;gt;; /*&amp;lt;24&amp;gt;;*/ /*&amp;lt;18&amp;gt;;*/ /*Row1-&amp;gt;GP7',Row2-&amp;gt;GP10.1',Row3-&amp;gt;NXP*/&lt;BR /&gt;&amp;nbsp;&amp;nbsp;primary;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;status = "okay";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;display-timings {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;native-mode = &amp;lt;&amp;amp;timing0&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;timing0: hsd100pxn1 {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;clock-frequency = &amp;lt;51200000&amp;gt;; /*&amp;lt;71100000&amp;gt;;*/ /*&amp;lt;65000000&amp;gt;;*/&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;hactive = &amp;lt;1024&amp;gt;; /*&amp;lt;1280&amp;gt;;*/ /*&amp;lt;1024&amp;gt;;*/&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;vactive = &amp;lt;600&amp;gt;; /*&amp;lt;800&amp;gt;;*/ /*&amp;lt;768&amp;gt;;*/&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;hback-porch = &amp;lt;80&amp;gt;; /*&amp;lt;40&amp;gt;;*/ /*&amp;lt;220&amp;gt;;*/&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;hfront-porch = &amp;lt;80&amp;gt;; /*&amp;lt;40&amp;gt;;*/ /*&amp;lt;40&amp;gt;;*/&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;vback-porch = &amp;lt;20&amp;gt;; /*&amp;lt;10&amp;gt;;*/ /*&amp;lt;21&amp;gt;;*/&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;vfront-porch = &amp;lt;5&amp;gt;; /*&amp;lt;3&amp;gt;;*/ /*&amp;lt;7&amp;gt;;*/&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;hsync-len = &amp;lt;160&amp;gt;; /*&amp;lt;80&amp;gt;;*/ /*&amp;lt;60&amp;gt;;*/&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;vsync-len = &amp;lt;10&amp;gt;; /*&amp;lt;10&amp;gt;;*/ /*&amp;lt;10&amp;gt;;*/&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;};&lt;BR /&gt;&amp;nbsp;&amp;nbsp;};&lt;BR /&gt;&amp;nbsp;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, some interesting things happened,&lt;/P&gt;&lt;P&gt;1. The PWM will have an output with a 20Khz/50us, 45us for +width and 5us for -width firstly. But in a few minutes, It will change to another duty cycle, about 22us for + width and 28us for - width. I don't know the root cause. It seems this 22:28us duty cycle is a 'ghost' cycle. I have changed my configurtation to 10:90 but also PWM will also change to the 'ghost' cycle, 22:28, in a few minutes. And this 'ghost' cycle is also the one on PWM1 of demo board. Why?&lt;/P&gt;&lt;P&gt;2. Another thing, We add a Triode S8550 to reverse the PWM TTL. So I need to reverse the PWM output,&amp;nbsp;by setting&amp;nbsp;0&amp;nbsp;for backlight ON while 1 for backlight OFF. How to setting the PWM3 by DTS?&lt;/P&gt;&lt;P&gt;3. The demo board is IMX6Q, we are using IMX6D, they are sharing 'imx6qdl-sabresd.dtsi'.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Currently, the display just light on&amp;nbsp;for a frame and then the backlight will be OFF quickly. Anyone can help to give some commnmets?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;BR//Denny&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Jan 2017 04:46:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ask-help-about-IMX6Q-D-PWM-for-LVDS-backlight/m-p/652574#M99872</guid>
      <dc:creator>dennyzhou</dc:creator>
      <dc:date>2017-01-02T04:46:59Z</dc:date>
    </item>
    <item>
      <title>Re: ask help about IMX6Q/D PWM for LVDS backlight</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ask-help-about-IMX6Q-D-PWM-for-LVDS-backlight/m-p/652575#M99873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I have fixed this case.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Actually, it is caused by a gpio controller to a power chip for LVDS, while not caused by the PWM. gpio6-15 is used here. We used hannstart_cabc function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------&lt;/P&gt;&lt;P&gt;&amp;nbsp; hannstar_cabc {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;compatible = "hannstar,cabc";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;lvds0 {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;gpios = &amp;lt;&amp;amp;gpio6 15 GPIO_ACTIVE_HIGH&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; cabc-enable;&amp;nbsp;&amp;nbsp;&amp;nbsp;//It is very&amp;nbsp;important here. Or it will reverse&amp;nbsp;the configuration.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;};&lt;BR /&gt;&amp;nbsp;&amp;nbsp;lvds1 {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;gpios = &amp;lt;&amp;amp;gpio6 16 GPIO_ACTIVE_HIGH&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;};&lt;BR /&gt;&amp;nbsp;};&lt;/P&gt;&lt;P&gt;----------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; And we have noticed that we should add a 'cabc-enable' here. Or the PIN will be set to LOW if you define ACTIVE_HIGH here.&amp;nbsp;It is not easy to add it, as there is no reference to configure the hannstart_cabc. I just checked and found it in the source code of kernel. It is suggest that NXP&amp;nbsp;could add some introduction in the txt file, to make it easy&amp;nbsp;to user. :smileyhappy:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR//Denny&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jan 2017 14:28:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ask-help-about-IMX6Q-D-PWM-for-LVDS-backlight/m-p/652575#M99873</guid>
      <dc:creator>dennyzhou</dc:creator>
      <dc:date>2017-01-03T14:28:39Z</dc:date>
    </item>
    <item>
      <title>Re: ask help about IMX6Q/D PWM for LVDS backlight</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ask-help-about-IMX6Q-D-PWM-for-LVDS-backlight/m-p/652576#M99874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for sharing Denny.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jan 2017 16:31:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ask-help-about-IMX6Q-D-PWM-for-LVDS-backlight/m-p/652576#M99874</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-01-03T16:31:51Z</dc:date>
    </item>
  </channel>
</rss>