<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: build krogoth yocto</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/build-krogoth-yocto/m-p/652423#M99832</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Moh Zahra,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem in this case is that there is no core-image-weston recipe available. This issue has been reported but there is no information yet on a possible fix.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you wish to build a Weston image you should be able to use Wayland as backend on the local.conf file and then build a compatible image. This is supported on the BSP release, I’ll check if it’s available also on the Yocto Community BSP (the Krogoth branch in particular).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 07 Jan 2017 00:11:52 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2017-01-07T00:11:52Z</dc:date>
    <item>
      <title>build krogoth yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/build-krogoth-yocto/m-p/652422#M99831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;I use use flowing command to get krogoth yocto version&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV class=""&gt;&lt;UL class=""&gt;&lt;LI&gt;mkdir ~/bin&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;curl &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcommondatastorage.googleapis.com%2Fgit-repo-downloads%2Frepo" rel="nofollow" target="_blank"&gt;http://commondatastorage.googleapis.com/git-repo-downloads/repo&lt;/A&gt;&lt;SPAN&gt; &amp;gt; ~/bin/repo&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;chmod a+x ~/bin/repo&lt;/LI&gt;&lt;/UL&gt;&lt;/DIV&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;Download the source code:&lt;/P&gt;&lt;DIV class=""&gt;&lt;UL class=""&gt;&lt;LI&gt;PATH=${PATH}:~/bin&lt;/LI&gt;&lt;LI&gt;mkdir fsl-community-bsp&lt;/LI&gt;&lt;LI&gt;cd fsl-community-bsp&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;repo init -u &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fgithub.com%2FFreescale%2Ffsl-community-bsp-platform" rel="nofollow" target="_blank"&gt;https://github.com/Freescale/fsl-community-bsp-platform&lt;/A&gt;&lt;SPAN&gt; -b krogoth&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;repo sync&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;then i used&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;MACHINE=imx6qpsabresd source setup-environment build-wayland&lt;/P&gt;&lt;P&gt;to set environment to build wayland weston&lt;/P&gt;&lt;P&gt;but when i run &amp;nbsp;&lt;STRONG&gt;bitbake core-image-weston &lt;/STRONG&gt;i face with following error&lt;/P&gt;&lt;P&gt;NOTE: Your conf/bblayers.conf has been automatically updated.&lt;BR /&gt;Loading cache: 100% |########################################################################################################################################################################| ETA: 00:00:00&lt;BR /&gt;Loaded 2198 entries from dependency cache.&lt;BR /&gt;ERROR: Nothing PROVIDES 'core-image-weston'&lt;BR /&gt;ERROR: core-image-weston was skipped: conflicting distro feature 'x11' (in DISTRO_FEATURES)&lt;/P&gt;&lt;P&gt;Summary: There was 1 ERROR message shown, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what step am i missed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 31 Dec 2016 08:27:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/build-krogoth-yocto/m-p/652422#M99831</guid>
      <dc:creator>mohsen2013</dc:creator>
      <dc:date>2016-12-31T08:27:58Z</dc:date>
    </item>
    <item>
      <title>Re: build krogoth yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/build-krogoth-yocto/m-p/652423#M99832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Moh Zahra,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem in this case is that there is no core-image-weston recipe available. This issue has been reported but there is no information yet on a possible fix.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you wish to build a Weston image you should be able to use Wayland as backend on the local.conf file and then build a compatible image. This is supported on the BSP release, I’ll check if it’s available also on the Yocto Community BSP (the Krogoth branch in particular).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Jan 2017 00:11:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/build-krogoth-yocto/m-p/652423#M99832</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-01-07T00:11:52Z</dc:date>
    </item>
  </channel>
</rss>