<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 ENET &amp; RGMII</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ENET-RGMII/m-p/651731#M99733</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm Intending to use&amp;nbsp;&amp;nbsp;RGMII periphery, Does&amp;nbsp;NVCC_ENET and NVCC_RGMII &amp;nbsp;must be tied to the same supply&amp;nbsp;?&lt;/P&gt;&lt;P&gt;&amp;nbsp;In the SABRE schematics I see that MDC from ENET is going to the RGMII PHY so which voltage does it take ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Eli&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 01 Jan 2017 13:53:29 GMT</pubDate>
    <dc:creator>eliaz</dc:creator>
    <dc:date>2017-01-01T13:53:29Z</dc:date>
    <item>
      <title>ENET &amp; RGMII</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ENET-RGMII/m-p/651731#M99733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm Intending to use&amp;nbsp;&amp;nbsp;RGMII periphery, Does&amp;nbsp;NVCC_ENET and NVCC_RGMII &amp;nbsp;must be tied to the same supply&amp;nbsp;?&lt;/P&gt;&lt;P&gt;&amp;nbsp;In the SABRE schematics I see that MDC from ENET is going to the RGMII PHY so which voltage does it take ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Eli&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 01 Jan 2017 13:53:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ENET-RGMII/m-p/651731#M99733</guid>
      <dc:creator>eliaz</dc:creator>
      <dc:date>2017-01-01T13:53:29Z</dc:date>
    </item>
    <item>
      <title>Re: ENET &amp; RGMII</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ENET-RGMII/m-p/651732#M99734</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jan 2017 16:14:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ENET-RGMII/m-p/651732#M99734</guid>
      <dc:creator>eliaz</dc:creator>
      <dc:date>2017-01-03T16:14:15Z</dc:date>
    </item>
    <item>
      <title>Re: ENET &amp; RGMII</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ENET-RGMII/m-p/651733#M99735</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes,&amp;nbsp; NVCC_ENET and NVCC_RGMII&amp;nbsp; can be attach both to the same power supply if the PHY that you are planning to use it is using the same power levels. It can be different since NVCC_ENET it is refer to the Ethernet Controller + Phy and NVCC_RGMII it is only for the Ethernet Controller no internal Phy to use.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jaime&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jan 2017 17:53:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ENET-RGMII/m-p/651733#M99735</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2017-01-03T17:53:42Z</dc:date>
    </item>
  </channel>
</rss>