<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 LTIB_problem at boot with SD/MMC: Warning - bad CRC or MMC, using default environment</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-problem-at-boot-with-SD-MMC-Warning-bad-CRC-or-MMC-using/m-p/193049#M9955</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi..&lt;/P&gt;&lt;P&gt;I'm working with iMX28 using LTIB environment.&lt;/P&gt;&lt;P&gt;I've a problem with u-boot-2009.08 when i make the boot from SD card.&lt;/P&gt;&lt;P&gt;The default speed was 50MHz and i've reduced it until 5MHz, but the problem remains.&lt;/P&gt;&lt;P&gt;Using SDHC verbatim there aren't problems under 25MHz of clock...with other sdhc cards the problem remains also using 5MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There's also a list of command sent to the SDHC when it works in 4bits bus width.&lt;/P&gt;&lt;P&gt;I print the serial log...(I added some printf )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;*********START BOOTLET power_prep******************&lt;/P&gt;&lt;P&gt;PowerPrep start initialize power...&lt;/P&gt;&lt;P&gt;Configured for 5v only power source. Battery powered oper ation disabled.&lt;BR /&gt; Dec 1 201116:49:02&lt;BR /&gt; FRAC 0x92925552&lt;BR /&gt; memory type is DDR2&lt;BR /&gt; Wait for ddr ready 1power 0x00820616&lt;BR /&gt; Frac 0x92925552&lt;BR /&gt; start change cpu freq&lt;BR /&gt; hbus 0x00000003&lt;BR /&gt; cpu 0x00010001&lt;BR /&gt; start test memory accress&lt;BR /&gt; ddr2 0x40000000&lt;BR /&gt; finish simple test&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; U-Boot 2009.08 (Dec 01 2011 - 12:11:56)&lt;/P&gt;&lt;P&gt;Freescale i.MX28 family&lt;BR /&gt; CPU: 454 MHz&lt;BR /&gt; BUS: 151 MHz&lt;BR /&gt; EMI: 205 MHz&lt;BR /&gt; GPMI: 24 MHz&lt;BR /&gt; DRAM: 128 MB&lt;BR /&gt; MMC: ***imx_ssp_mmc_initialize***&lt;BR /&gt; ***imx_ssp_mmc_initialize***&lt;BR /&gt; IMX_SSP_MMC: 0, IMX_SSP_MMC: 1&lt;BR /&gt; MMC0: Set clock rate to 400 KHz (requested 400 KHz)&lt;BR /&gt; ***ssp_mmc_init***&lt;/P&gt;&lt;P&gt;MMC0: Set 1 bits bus width&lt;BR /&gt; MMC0: Set clock rate to 400 KHz (requested 400 KHz)&lt;BR /&gt; MMC0: Set 1 bits bus width&lt;BR /&gt; MMC0: CMD0&lt;BR /&gt; MMC0: CMD8&lt;BR /&gt; MMC0: CMD55&lt;BR /&gt; MMC0: CMD41&lt;BR /&gt; MMC0: CMD55&lt;BR /&gt; MMC0: CMD41&lt;BR /&gt; MMC0: CMD2&lt;BR /&gt; MMC0: CMD3&lt;BR /&gt; MMC0: CMD9&lt;BR /&gt; MMC0: CMD7&lt;BR /&gt; MMC0: CMD55&lt;BR /&gt; MMC0: CMD51&lt;BR /&gt; MMC0: CMD6&lt;BR /&gt; MMC0: CMD6&lt;BR /&gt; MMC0: CMD55&lt;BR /&gt; MMC0: CMD6&lt;BR /&gt; MMC0: Set clock rate to 400 KHz (requested 400 KHz)&lt;BR /&gt; MMC0: Set 4 bits bus width&lt;BR /&gt; u-boot-2009.08/driver/mmc/mmc.c *** mmc_set_clock: 20MHz ***&lt;BR /&gt; MMC0: Set clock rate to 4965 KHz (requested 5000 KHz)&lt;BR /&gt; MMC0: Set 4 bits bus width&lt;BR /&gt; MMC0: CMD16&lt;BR /&gt; MMC0: CMD17&lt;BR /&gt; MMC0: CMD16&lt;BR /&gt; MMC0: CMD18&lt;BR /&gt; MMC0: CMD12&lt;BR /&gt; &lt;SPAN class="font-size-4" style="color: #ff0000;"&gt;&lt;STRONG&gt;*** Warning - bad CRC or MMC, using default environment&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In: serial&lt;BR /&gt; Out: serial&lt;BR /&gt; Err: serial&lt;BR /&gt; Net: got MAC address from IIM: 00:04:00:00:00:00&lt;BR /&gt; FEC0&lt;BR /&gt; Hit any key to stop autoboot: 3&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Dec 2011 08:16:49 GMT</pubDate>
    <dc:creator>Nico</dc:creator>
    <dc:date>2011-12-06T08:16:49Z</dc:date>
    <item>
      <title>LTIB_problem at boot with SD/MMC: Warning - bad CRC or MMC, using default environment</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-problem-at-boot-with-SD-MMC-Warning-bad-CRC-or-MMC-using/m-p/193049#M9955</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi..&lt;/P&gt;&lt;P&gt;I'm working with iMX28 using LTIB environment.&lt;/P&gt;&lt;P&gt;I've a problem with u-boot-2009.08 when i make the boot from SD card.&lt;/P&gt;&lt;P&gt;The default speed was 50MHz and i've reduced it until 5MHz, but the problem remains.&lt;/P&gt;&lt;P&gt;Using SDHC verbatim there aren't problems under 25MHz of clock...with other sdhc cards the problem remains also using 5MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There's also a list of command sent to the SDHC when it works in 4bits bus width.&lt;/P&gt;&lt;P&gt;I print the serial log...(I added some printf )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;*********START BOOTLET power_prep******************&lt;/P&gt;&lt;P&gt;PowerPrep start initialize power...&lt;/P&gt;&lt;P&gt;Configured for 5v only power source. Battery powered oper ation disabled.&lt;BR /&gt; Dec 1 201116:49:02&lt;BR /&gt; FRAC 0x92925552&lt;BR /&gt; memory type is DDR2&lt;BR /&gt; Wait for ddr ready 1power 0x00820616&lt;BR /&gt; Frac 0x92925552&lt;BR /&gt; start change cpu freq&lt;BR /&gt; hbus 0x00000003&lt;BR /&gt; cpu 0x00010001&lt;BR /&gt; start test memory accress&lt;BR /&gt; ddr2 0x40000000&lt;BR /&gt; finish simple test&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; U-Boot 2009.08 (Dec 01 2011 - 12:11:56)&lt;/P&gt;&lt;P&gt;Freescale i.MX28 family&lt;BR /&gt; CPU: 454 MHz&lt;BR /&gt; BUS: 151 MHz&lt;BR /&gt; EMI: 205 MHz&lt;BR /&gt; GPMI: 24 MHz&lt;BR /&gt; DRAM: 128 MB&lt;BR /&gt; MMC: ***imx_ssp_mmc_initialize***&lt;BR /&gt; ***imx_ssp_mmc_initialize***&lt;BR /&gt; IMX_SSP_MMC: 0, IMX_SSP_MMC: 1&lt;BR /&gt; MMC0: Set clock rate to 400 KHz (requested 400 KHz)&lt;BR /&gt; ***ssp_mmc_init***&lt;/P&gt;&lt;P&gt;MMC0: Set 1 bits bus width&lt;BR /&gt; MMC0: Set clock rate to 400 KHz (requested 400 KHz)&lt;BR /&gt; MMC0: Set 1 bits bus width&lt;BR /&gt; MMC0: CMD0&lt;BR /&gt; MMC0: CMD8&lt;BR /&gt; MMC0: CMD55&lt;BR /&gt; MMC0: CMD41&lt;BR /&gt; MMC0: CMD55&lt;BR /&gt; MMC0: CMD41&lt;BR /&gt; MMC0: CMD2&lt;BR /&gt; MMC0: CMD3&lt;BR /&gt; MMC0: CMD9&lt;BR /&gt; MMC0: CMD7&lt;BR /&gt; MMC0: CMD55&lt;BR /&gt; MMC0: CMD51&lt;BR /&gt; MMC0: CMD6&lt;BR /&gt; MMC0: CMD6&lt;BR /&gt; MMC0: CMD55&lt;BR /&gt; MMC0: CMD6&lt;BR /&gt; MMC0: Set clock rate to 400 KHz (requested 400 KHz)&lt;BR /&gt; MMC0: Set 4 bits bus width&lt;BR /&gt; u-boot-2009.08/driver/mmc/mmc.c *** mmc_set_clock: 20MHz ***&lt;BR /&gt; MMC0: Set clock rate to 4965 KHz (requested 5000 KHz)&lt;BR /&gt; MMC0: Set 4 bits bus width&lt;BR /&gt; MMC0: CMD16&lt;BR /&gt; MMC0: CMD17&lt;BR /&gt; MMC0: CMD16&lt;BR /&gt; MMC0: CMD18&lt;BR /&gt; MMC0: CMD12&lt;BR /&gt; &lt;SPAN class="font-size-4" style="color: #ff0000;"&gt;&lt;STRONG&gt;*** Warning - bad CRC or MMC, using default environment&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In: serial&lt;BR /&gt; Out: serial&lt;BR /&gt; Err: serial&lt;BR /&gt; Net: got MAC address from IIM: 00:04:00:00:00:00&lt;BR /&gt; FEC0&lt;BR /&gt; Hit any key to stop autoboot: 3&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Dec 2011 08:16:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LTIB-problem-at-boot-with-SD-MMC-Warning-bad-CRC-or-MMC-using/m-p/193049#M9955</guid>
      <dc:creator>Nico</dc:creator>
      <dc:date>2011-12-06T08:16:49Z</dc:date>
    </item>
    <item>
      <title>Re: LTIB_problem at boot with SD/MMC: Warning - bad CRC or MMC, using default environment</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-problem-at-boot-with-SD-MMC-Warning-bad-CRC-or-MMC-using/m-p/193050#M9956</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nico,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First you have to change your environment variables from default.&lt;/P&gt;&lt;P&gt;Then the problem will be solved.&lt;/P&gt;&lt;P&gt;Link is here&amp;nbsp;&amp;nbsp; ::&amp;nbsp; &lt;A href="http://imxcommunity.org/group/imx53quickstartboard/forum/topics/user-experience-with-1109-binaries-warning-bad-crc-or-mmc?xg_source=activity" target="_self"&gt;http://imxcommunity.org/group/imx53quickstartboard/forum/topics/user-experience-with-1109-binaries-warning-bad-crc-or-mmc?xg_source=activity&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Try to figure out respective args for your i.MX from user manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&amp;nbsp; ::&amp;nbsp;&amp;nbsp; Krishna Pavan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Dec 2011 06:53:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LTIB-problem-at-boot-with-SD-MMC-Warning-bad-CRC-or-MMC-using/m-p/193050#M9956</guid>
      <dc:creator>KrishnaPavan</dc:creator>
      <dc:date>2011-12-08T06:53:23Z</dc:date>
    </item>
  </channel>
</rss>