<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: I have Sabre board(MCIMX6SX-SDB) from NXP, now require full source code or link to download</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-have-Sabre-board-MCIMX6SX-SDB-from-NXP-now-require-full-source/m-p/649756#M99424</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Anil Kumar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can build customized images for the i.MX6SX SABRE Board using the Linux BSP Release (link below, please note that you may need to login in order to download this file).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS"&gt;https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please follow the Yocto User’s Guide document contained in this bundle. Since Yocto is used as a means of distribution the source code is fetched on demand. You may, however, fetch the required sources for a given image by using the following command:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bitbake &amp;lt;image_or_recipe&amp;gt; -c fetchall&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may also extract the toolchain using:&lt;/P&gt;&lt;P&gt;bitbake meta-toolchain&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once fetched you can find the source code on the work directory:&lt;/P&gt;&lt;P&gt;/&amp;lt;BSP_DIR&amp;gt;/&amp;lt;BUILD_DIR&amp;gt;/tmp/work/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, the source for the kernel would be on:&lt;/P&gt;&lt;P&gt;/&amp;lt;BSP_DIR&amp;gt;/&amp;lt;BUILD_DIR&amp;gt;/tmp/work/&amp;lt;MACHINE&amp;gt;/linux-imx/&amp;lt;KERNEL_VER&amp;gt;/git/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The sources are located depending on the recipes that compiles and install the packages so it may not be very straightforward.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information helps!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Mar 2017 18:35:51 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2017-03-14T18:35:51Z</dc:date>
    <item>
      <title>I have Sabre board(MCIMX6SX-SDB) from NXP, now require full source code or link to download</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-have-Sabre-board-MCIMX6SX-SDB-from-NXP-now-require-full-source/m-p/649755#M99423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have Sabre board(MCIMX6SX-SDB), with this only bootable images but i don't not full source code. So we require the full source code which include toolchain and &amp;nbsp;A9 and M4 source to compile and build. Please share the source also related links.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;&lt;P&gt;-Anil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Mar 2017 11:44:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-have-Sabre-board-MCIMX6SX-SDB-from-NXP-now-require-full-source/m-p/649755#M99423</guid>
      <dc:creator>anilchowdary</dc:creator>
      <dc:date>2017-03-14T11:44:37Z</dc:date>
    </item>
    <item>
      <title>Re: I have Sabre board(MCIMX6SX-SDB) from NXP, now require full source code or link to download</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-have-Sabre-board-MCIMX6SX-SDB-from-NXP-now-require-full-source/m-p/649756#M99424</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Anil Kumar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can build customized images for the i.MX6SX SABRE Board using the Linux BSP Release (link below, please note that you may need to login in order to download this file).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS"&gt;https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please follow the Yocto User’s Guide document contained in this bundle. Since Yocto is used as a means of distribution the source code is fetched on demand. You may, however, fetch the required sources for a given image by using the following command:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bitbake &amp;lt;image_or_recipe&amp;gt; -c fetchall&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may also extract the toolchain using:&lt;/P&gt;&lt;P&gt;bitbake meta-toolchain&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once fetched you can find the source code on the work directory:&lt;/P&gt;&lt;P&gt;/&amp;lt;BSP_DIR&amp;gt;/&amp;lt;BUILD_DIR&amp;gt;/tmp/work/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, the source for the kernel would be on:&lt;/P&gt;&lt;P&gt;/&amp;lt;BSP_DIR&amp;gt;/&amp;lt;BUILD_DIR&amp;gt;/tmp/work/&amp;lt;MACHINE&amp;gt;/linux-imx/&amp;lt;KERNEL_VER&amp;gt;/git/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The sources are located depending on the recipes that compiles and install the packages so it may not be very straightforward.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information helps!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Mar 2017 18:35:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-have-Sabre-board-MCIMX6SX-SDB-from-NXP-now-require-full-source/m-p/649756#M99424</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-03-14T18:35:51Z</dc:date>
    </item>
  </channel>
</rss>