<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX6: Ethernet PHY TX not working</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Ethernet-PHY-TX-not-working/m-p/649753#M99421</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have a custom board that has IMX-6 connected to Micrel PHY (KSZ9031RNX).&lt;/P&gt;&lt;P&gt;This is a Magnatics less system that is 100BaseT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Linux boots up fine, but the eth0 interface show activity only on RX side. all TX side is 0 bytes.&lt;/P&gt;&lt;P&gt;This leads to no dhcp address getting assigned to eth0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# ifconfig eth0&lt;BR /&gt;eth0 Link encap:Ethernet HWaddr fa:fc:7e:7f:b5:92 &lt;BR /&gt; inet6 addr: fe80::f8fc:7eff:fe7f:b592/64 Scope:Link&lt;BR /&gt; UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1&lt;BR /&gt; RX packets:220 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt; TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt; collisions:0 txqueuelen:1000 &lt;BR /&gt; RX bytes:35227 (34.4 KiB) TX bytes:0 (0.0 B)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;I read some threads where it was mentioned that skew rate adjustments could solve such problem.&lt;/P&gt;&lt;P&gt;Following are our skew register settings.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could anyone point why TX side is not working? Any pointers would help us to make progress. We are stuck on this issue for around a month now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# ./mmd 2 4 &lt;BR /&gt;0x0000&lt;BR /&gt;# ./mmd 2 5&lt;BR /&gt;0x0000&lt;BR /&gt;# ./mmd 2 8&lt;BR /&gt;0xf3ff&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Sep 2016 05:58:42 GMT</pubDate>
    <dc:creator>vicpandit</dc:creator>
    <dc:date>2016-09-26T05:58:42Z</dc:date>
    <item>
      <title>IMX6: Ethernet PHY TX not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Ethernet-PHY-TX-not-working/m-p/649753#M99421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have a custom board that has IMX-6 connected to Micrel PHY (KSZ9031RNX).&lt;/P&gt;&lt;P&gt;This is a Magnatics less system that is 100BaseT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Linux boots up fine, but the eth0 interface show activity only on RX side. all TX side is 0 bytes.&lt;/P&gt;&lt;P&gt;This leads to no dhcp address getting assigned to eth0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# ifconfig eth0&lt;BR /&gt;eth0 Link encap:Ethernet HWaddr fa:fc:7e:7f:b5:92 &lt;BR /&gt; inet6 addr: fe80::f8fc:7eff:fe7f:b592/64 Scope:Link&lt;BR /&gt; UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1&lt;BR /&gt; RX packets:220 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt; TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt; collisions:0 txqueuelen:1000 &lt;BR /&gt; RX bytes:35227 (34.4 KiB) TX bytes:0 (0.0 B)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;I read some threads where it was mentioned that skew rate adjustments could solve such problem.&lt;/P&gt;&lt;P&gt;Following are our skew register settings.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could anyone point why TX side is not working? Any pointers would help us to make progress. We are stuck on this issue for around a month now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# ./mmd 2 4 &lt;BR /&gt;0x0000&lt;BR /&gt;# ./mmd 2 5&lt;BR /&gt;0x0000&lt;BR /&gt;# ./mmd 2 8&lt;BR /&gt;0xf3ff&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Sep 2016 05:58:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Ethernet-PHY-TX-not-working/m-p/649753#M99421</guid>
      <dc:creator>vicpandit</dc:creator>
      <dc:date>2016-09-26T05:58:42Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6: Ethernet PHY TX not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Ethernet-PHY-TX-not-working/m-p/649754#M99422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We finally found the issue. &lt;BR /&gt;Our design had not correctly connected the ENET_CRS_DV reset line from IMX-6q to the PHY.&lt;BR /&gt;Once we fixed this, both tx/rx is working fine at 100BaseT now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problem solved.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Sep 2016 05:38:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Ethernet-PHY-TX-not-working/m-p/649754#M99422</guid>
      <dc:creator>vicpandit</dc:creator>
      <dc:date>2016-09-27T05:38:19Z</dc:date>
    </item>
  </channel>
</rss>