<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic about memory copy using iMX53 IPU  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/about-memory-copy-using-iMX53-IPU/m-p/649567#M99358</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;Please tell me about memory copy using iMX53 IPU. I copied data from Buffer1 to Buffer2 using CH 11 and CH 22 (Post processing). But, I would like to copy memory using PreProcessing VeiwFider. I also want to resize.&lt;/P&gt;&lt;P&gt;Is it possible to copy the buffer using PreProcessing ViewFinder? If possible, Can it be realized by using the CH12 and 21? I am experimenting with various settings, but I can not copy it. Please tell me what kind of register should be set.&lt;/P&gt;&lt;P&gt;By the way, when using CH11, CH22 (PostProcessing), I was setting the following registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IPU_IC_IDMAC_1&lt;BR /&gt;IPU_IC_IDMAC_2&lt;BR /&gt;IPU_IC_IDMAC_3&lt;BR /&gt;IPU_IC_PP_RSC&lt;BR /&gt;IPU_IC_CONF&lt;BR /&gt;IPU_IDMAC_CH_EN_1&lt;BR /&gt;IPU_CONF&lt;BR /&gt;IPU_INT_CTRL_1&lt;BR /&gt;IPU_CH_BUF0_RDY0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPMEM&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;kyuugo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Jan 2017 05:44:32 GMT</pubDate>
    <dc:creator>kyuugosato</dc:creator>
    <dc:date>2017-01-27T05:44:32Z</dc:date>
    <item>
      <title>about memory copy using iMX53 IPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-memory-copy-using-iMX53-IPU/m-p/649567#M99358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;Please tell me about memory copy using iMX53 IPU. I copied data from Buffer1 to Buffer2 using CH 11 and CH 22 (Post processing). But, I would like to copy memory using PreProcessing VeiwFider. I also want to resize.&lt;/P&gt;&lt;P&gt;Is it possible to copy the buffer using PreProcessing ViewFinder? If possible, Can it be realized by using the CH12 and 21? I am experimenting with various settings, but I can not copy it. Please tell me what kind of register should be set.&lt;/P&gt;&lt;P&gt;By the way, when using CH11, CH22 (PostProcessing), I was setting the following registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IPU_IC_IDMAC_1&lt;BR /&gt;IPU_IC_IDMAC_2&lt;BR /&gt;IPU_IC_IDMAC_3&lt;BR /&gt;IPU_IC_PP_RSC&lt;BR /&gt;IPU_IC_CONF&lt;BR /&gt;IPU_IDMAC_CH_EN_1&lt;BR /&gt;IPU_CONF&lt;BR /&gt;IPU_INT_CTRL_1&lt;BR /&gt;IPU_CH_BUF0_RDY0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPMEM&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;kyuugo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jan 2017 05:44:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-memory-copy-using-iMX53-IPU/m-p/649567#M99358</guid>
      <dc:creator>kyuugosato</dc:creator>
      <dc:date>2017-01-27T05:44:32Z</dc:date>
    </item>
    <item>
      <title>Re: about memory copy using iMX53 IPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-memory-copy-using-iMX53-IPU/m-p/649568#M99359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can perform rotation, color conversion and resizing image using PreProcessing VeiwFider.&lt;BR /&gt;Please refer chapter 45 "Image Processing Unit" of i.MX53 Multimedia Applications Processor Reference Manual for the details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2017 04:34:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-memory-copy-using-iMX53-IPU/m-p/649568#M99359</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2017-01-30T04:34:43Z</dc:date>
    </item>
    <item>
      <title>Re: about memory copy using iMX53 IPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-memory-copy-using-iMX53-IPU/m-p/649569#M99360</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Victor.&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;Please refer chapter 45 "Image Processing Unit" of i.MX53 Multimedia&lt;/P&gt;&lt;P&gt;Yes, I confirmed the manual.&lt;/P&gt;&lt;P&gt;And I have successfully copied from Buffer 1 to Buffer 2 using CH 11 and CH 22(Post Processing).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;You can perform rotation, color conversion and resizing image using&lt;BR /&gt;&amp;gt;&amp;gt; PreProcessing ViewFider.&lt;/P&gt;&lt;P&gt;How can I do it using CH12 and CH21 ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made the following settings to use ViewFinder.&lt;/P&gt;&lt;P&gt;---------------------------------------------------------------------&lt;BR /&gt;IPU_IC_IDMAC_1------Select CH12 (CB6) and CH21 (CB1)&lt;/P&gt;&lt;P&gt;IPU_IC_IDMAC_2------Set T2_FR_HEIGHT&lt;/P&gt;&lt;P&gt;IPU_IC_IDMAC_3------Set T2_FR_HEIGHT&lt;/P&gt;&lt;P&gt;IPU_IC_PRP_VF_RSC---Perform the same setting as when using CH 11 and CH 22&lt;/P&gt;&lt;P&gt;IPU_IC_CONF---------Set PRPVF_EN to enable&lt;/P&gt;&lt;P&gt;IPU_IDMAC_CH_EN_1---Set IDMAC_CH_EN_12 and IDMAC_CH_EN_21 to enable&lt;/P&gt;&lt;P&gt;IPU_CONF------------Set IC_EN to enable&lt;/P&gt;&lt;P&gt;IPU_INT_CTRL_1------Perform setting of CH12 and CH21&lt;/P&gt;&lt;P&gt;IPU_CH_BUF0_RDY0----Perform setting of CH12 and CH21&lt;BR /&gt;---------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;But I can not make memory copies.&lt;/P&gt;&lt;P&gt;Please tell me which setting is different from when setting CH11 and CH22 (PostProcessing).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;kyuugo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2017 05:59:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-memory-copy-using-iMX53-IPU/m-p/649569#M99360</guid>
      <dc:creator>kyuugosato</dc:creator>
      <dc:date>2017-01-30T05:59:45Z</dc:date>
    </item>
    <item>
      <title>Re: about memory copy using iMX53 IPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-memory-copy-using-iMX53-IPU/m-p/649570#M99361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was able to solve this problem.&lt;BR /&gt;I was able to do it by adding the following settings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;IC_CONF 0x40000100&lt;BR /&gt;&amp;nbsp;IPU_FS_PROC_FLOW1&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x80000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The channels I used were CH12 and CH21（ViewFider）.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Feb 2017 01:22:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-memory-copy-using-iMX53-IPU/m-p/649570#M99361</guid>
      <dc:creator>kyuugosato</dc:creator>
      <dc:date>2017-02-09T01:22:55Z</dc:date>
    </item>
  </channel>
</rss>