<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 IMx7 Solo M4 boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMx7-Solo-M4-boot/m-p/649216#M99277</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible on IMx7 Solo to run application only for M4 core and not boot linux&amp;nbsp;on A7 core?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Sep 2016 00:10:30 GMT</pubDate>
    <dc:creator>makrist</dc:creator>
    <dc:date>2016-09-26T00:10:30Z</dc:date>
    <item>
      <title>IMx7 Solo M4 boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMx7-Solo-M4-boot/m-p/649216#M99277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible on IMx7 Solo to run application only for M4 core and not boot linux&amp;nbsp;on A7 core?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Sep 2016 00:10:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMx7-Solo-M4-boot/m-p/649216#M99277</guid>
      <dc:creator>makrist</dc:creator>
      <dc:date>2016-09-26T00:10:30Z</dc:date>
    </item>
    <item>
      <title>Re: IMx7 Solo M4 boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMx7-Solo-M4-boot/m-p/649217#M99278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lukaz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;processor boot options are given in sect.6.6 System Boot i.MX7D Reference Manual&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf"&gt;http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;there is no option to boot directly M4, so some code should be run from&lt;/P&gt;&lt;P&gt;A7 to load code to M4 and run it. One can check AN5317&lt;/P&gt;&lt;P&gt;Loading Code on Cortex-M4 from Linux for the i.MX 6SoloX and i.MX 7Dual/7Solo Application Processors&lt;/P&gt;&lt;P&gt;cache.nxp.com/files/soft_dev_tools/doc/app_note/AN5317.pdf&lt;/P&gt;&lt;P&gt;In general one can develop custom code for such purpose and&lt;/P&gt;&lt;P&gt;run M4 from Uboot in similar way as in sect.4.7.6 Running the ARM&lt;/P&gt;&lt;P&gt;Cortex-M4 image attached Linux Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Sep 2016 06:04:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMx7-Solo-M4-boot/m-p/649217#M99278</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-09-26T06:04:07Z</dc:date>
    </item>
    <item>
      <title>Re: IMx7 Solo M4 boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMx7-Solo-M4-boot/m-p/649218#M99279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a few problems with loading the code for the M4 from Linux. how exactly can you move the code to a specific address in memory? This part isn't mentioned in the AN5317.pdf&lt;/P&gt;&lt;P&gt;Setting single bits is possible with devmem, so the rest of the procedure is fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I need to write a script or is there a super convenient command for this purpose I am unable to find?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Load the code for the Cortex-M4 processor into the TCM_L memory." - But how?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erik&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Aug 2018 06:51:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMx7-Solo-M4-boot/m-p/649218#M99279</guid>
      <dc:creator>erikfriedel</dc:creator>
      <dc:date>2018-08-20T06:51:27Z</dc:date>
    </item>
  </channel>
</rss>