<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX6SX - Wake up from Stop mode with USB</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SX-Wake-up-from-Stop-mode-with-USB/m-p/648739#M99179</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to wake up the i.MX6SX from stop mode when I plug in USB.&lt;/P&gt;&lt;P&gt;The USB is configured as a device and I want the i.MX6 to wake up when I plug it to a host.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to do this with the i.MX6SX?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to configure the USB PHY so a wake up IRQ triggers once activity is detected on DP/DM lines, but the SoC never wakes up when I plug the USB to a Host. Maybe I'm missing something in clocks and/or power configuration before entering stop mode. I didn't find any information on Stop mode exit in the USB PHY chapter in the i.MX6SX reference manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Mar 2017 14:26:51 GMT</pubDate>
    <dc:creator>davidjaouen</dc:creator>
    <dc:date>2017-03-14T14:26:51Z</dc:date>
    <item>
      <title>i.MX6SX - Wake up from Stop mode with USB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SX-Wake-up-from-Stop-mode-with-USB/m-p/648739#M99179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to wake up the i.MX6SX from stop mode when I plug in USB.&lt;/P&gt;&lt;P&gt;The USB is configured as a device and I want the i.MX6 to wake up when I plug it to a host.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to do this with the i.MX6SX?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to configure the USB PHY so a wake up IRQ triggers once activity is detected on DP/DM lines, but the SoC never wakes up when I plug the USB to a Host. Maybe I'm missing something in clocks and/or power configuration before entering stop mode. I didn't find any information on Stop mode exit in the USB PHY chapter in the i.MX6SX reference manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Mar 2017 14:26:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SX-Wake-up-from-Stop-mode-with-USB/m-p/648739#M99179</guid>
      <dc:creator>davidjaouen</dc:creator>
      <dc:date>2017-03-14T14:26:51Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6SX - Wake up from Stop mode with USB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SX-Wake-up-from-Stop-mode-with-USB/m-p/648740#M99180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check sect.39.3.6 USB Wakeup Usage attached Linux Manual and&lt;/P&gt;&lt;P&gt;imx-test package, folder ../mxc_usb_test/doc&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz"&gt;www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Mar 2017 23:07:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SX-Wake-up-from-Stop-mode-with-USB/m-p/648740#M99180</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-03-14T23:07:44Z</dc:date>
    </item>
  </channel>
</rss>