<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Audio DDR frequency on iMX6ULL in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Audio-DDR-frequency-on-iMX6ULL/m-p/648629#M99165</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This document is a bit outdated in point of list of processors.&lt;BR /&gt;Please refer to chapter 24 "Dynamic Bus Frequency Driver" of i.MX Linux Reference Manual you can get from L4.1.15_2.0.0_LINUX_DOCS bundle.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Apr 2017 04:11:57 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2017-04-28T04:11:57Z</dc:date>
    <item>
      <title>Audio DDR frequency on iMX6ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-DDR-frequency-on-iMX6ULL/m-p/648628#M99164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are trying to save power on our iMX6ULL custom platform during lower computation periods. The idea would be to reduce DDR frequency which is a high power consumption budget.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have tried to use low power idle DDR frequency mode (24MHz) but it is too slow for our computations, we cannot reach real time target.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We would like to run an intermediary DDR frequency (100MHz?) which seems to be named as "Audio DDR frequency" on Linux User guide (see below)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;• Normal DDR frequency – Default frequency in U-Boot&lt;BR /&gt;• Audio DDR frequency – 50 MHz on i.MX 6Quad, i.MX 6DualLite, and i.MX 6SoloX, 100 MHz on i.MX 6SoloLite,&lt;BR /&gt;and 100 MHz on i.MX 7Dual&lt;BR /&gt;• Low power idle DDR frequency – 24 MHz&lt;BR /&gt;• Ultra Low power IDLE DDR frequency – 1 MHz (only on i.MX 6SoloLite)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, iMX6ULL specific intermediary frequency does not appear on this document (L4.1.15_2.0.0-ga). Is document out of date?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When we try to force driver to pass into "&lt;SPAN&gt;Audio DDR frequency", DDR frequency stays at its default&amp;nbsp;value (400MHz). Is iMX6ULL DDR controller able to run at an intermediary frequency? If yes, why isn't it available on current BSP? If not, is the limitation HW or SW?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you for your help.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Sam&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Apr 2017 12:57:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-DDR-frequency-on-iMX6ULL/m-p/648628#M99164</guid>
      <dc:creator>samuelrythm</dc:creator>
      <dc:date>2017-04-27T12:57:33Z</dc:date>
    </item>
    <item>
      <title>Re: Audio DDR frequency on iMX6ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-DDR-frequency-on-iMX6ULL/m-p/648629#M99165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This document is a bit outdated in point of list of processors.&lt;BR /&gt;Please refer to chapter 24 "Dynamic Bus Frequency Driver" of i.MX Linux Reference Manual you can get from L4.1.15_2.0.0_LINUX_DOCS bundle.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Apr 2017 04:11:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-DDR-frequency-on-iMX6ULL/m-p/648629#M99165</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2017-04-28T04:11:57Z</dc:date>
    </item>
  </channel>
</rss>