<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: I.MX6 MIPI DSI problem with platform SDK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-DSI-problem-with-platform-SDK/m-p/647975#M98996</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;I have tried to run these tests but they didnt work. I have changed the LCD_INIT fuction according to the display panel used(hx8363A) and also display panel channel structure to update timings. I guess that my problem is with &lt;/SPAN&gt;&lt;SPAN&gt;CCM &lt;/SPAN&gt;&lt;SPAN&gt;configuration. What are the necessary clock setting(values, clock route etc.) for proper operation of MIPI DSI and IPU?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Jan 2017 11:01:26 GMT</pubDate>
    <dc:creator>hakanakis</dc:creator>
    <dc:date>2017-01-27T11:01:26Z</dc:date>
    <item>
      <title>I.MX6 MIPI DSI problem with platform SDK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-DSI-problem-with-platform-SDK/m-p/647973#M98994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="padding: 0px;"&gt;Hello,&lt;/P&gt;&lt;P style="padding: 0px;"&gt;I am using &amp;nbsp;i.mx6dl sabre sd board and MIPI DSI display connected by MIPI expansion port. Display panel has HX8363A controller on it.&lt;/P&gt;&lt;P style="padding: 0px;"&gt;I have configured linux dts files and bootcmd, wrote new display panel driver for HX8363A display panel. It is working as intented. However, I cannot be able to display image with baremetal sofware.&lt;/P&gt;&lt;P style="padding: 0px;"&gt;&lt;/P&gt;&lt;P style="padding: 0px;"&gt;I have to achieve this with baremeral software. With platform SDK software, I am conducting ipu tests. LDB tests are succesful. There is also MIPI DSI tests under Platform SDK. I am wondering whether MIPI DSI tests under Platform SDK is working or not? I have modified MIPI DSI tests for HX8363A display panel, but tests are failed. No image is displayed. I don't know what i am missing. What can be the problem?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jan 2017 20:52:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-DSI-problem-with-platform-SDK/m-p/647973#M98994</guid>
      <dc:creator>hakanakis</dc:creator>
      <dc:date>2017-01-26T20:52:25Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 MIPI DSI problem with platform SDK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-DSI-problem-with-platform-SDK/m-p/647974#M98995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi hakan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to run these tests on Sabre SD reference board using&lt;/P&gt;&lt;P&gt;sect.5. MIPI test SDK Unit Test Procedures.pdf included in SDK /doc&lt;/P&gt;&lt;P&gt;folder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jan 2017 05:12:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-DSI-problem-with-platform-SDK/m-p/647974#M98995</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-27T05:12:04Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 MIPI DSI problem with platform SDK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-DSI-problem-with-platform-SDK/m-p/647975#M98996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;I have tried to run these tests but they didnt work. I have changed the LCD_INIT fuction according to the display panel used(hx8363A) and also display panel channel structure to update timings. I guess that my problem is with &lt;/SPAN&gt;&lt;SPAN&gt;CCM &lt;/SPAN&gt;&lt;SPAN&gt;configuration. What are the necessary clock setting(values, clock route etc.) for proper operation of MIPI DSI and IPU?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jan 2017 11:01:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-DSI-problem-with-platform-SDK/m-p/647975#M98996</guid>
      <dc:creator>hakanakis</dc:creator>
      <dc:date>2017-01-27T11:01:26Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 MIPI DSI problem with platform SDK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-DSI-problem-with-platform-SDK/m-p/647976#M98997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SDK provided "as is", without support.&lt;/P&gt;&lt;P&gt;In general one can printf DSI registers in linux and compare with SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jan 2017 11:21:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-DSI-problem-with-platform-SDK/m-p/647976#M98997</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-27T11:21:56Z</dc:date>
    </item>
  </channel>
</rss>