<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MMPF0200 F6 - SWBST, VGEN2</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0200-F6-SWBST-VGEN2/m-p/647283#M98880</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you, that answers my question!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Feb 2017 16:00:36 GMT</pubDate>
    <dc:creator>max123</dc:creator>
    <dc:date>2017-02-02T16:00:36Z</dc:date>
    <item>
      <title>MMPF0200 F6 - SWBST, VGEN2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0200-F6-SWBST-VGEN2/m-p/647281#M98878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we use the MMPF0200 (F6 configuration) for the supply of a custom i.MX6 solo board.&lt;/P&gt;&lt;P&gt;On my Board, SWBST and VGEN2 are not starting up. I get 0V at VGEN2, and 3.6V at SWBST (no switching).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think, this may be correct for the F6 configuration. According to table 8, the sequence for this voltages is "-", so this voltages will never start up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this correct?&lt;/P&gt;&lt;P&gt;Are there any details available for this configuration, aside from table 8 in the datasheet?&lt;/P&gt;&lt;P&gt;This is not a issue, since these voltages are unused on my board. But i need to verify, this is not due to an error in my circuit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any help in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jan 2017 14:37:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMPF0200-F6-SWBST-VGEN2/m-p/647281#M98878</guid>
      <dc:creator>max123</dc:creator>
      <dc:date>2017-01-26T14:37:20Z</dc:date>
    </item>
    <item>
      <title>Re: MMPF0200 F6 - SWBST, VGEN2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0200-F6-SWBST-VGEN2/m-p/647282#M98879</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Maximilian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for writing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please note that the "-" in the &lt;STRONG&gt;Table 8&lt;/STRONG&gt; from the &lt;A href="http://www.nxp.com/assets/documents/data/en/data-sheets/MMPF0200.pdf"&gt;datasheet&lt;/A&gt;, means that the corresponding regulator will be OFF by default, so if you want to use it, you have to turn it ON.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So 0V at the VGEN2 is expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case of the SWBST, I assume you have the incorrect connection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please review the &lt;STRONG&gt;Table 1&lt;/STRONG&gt; from the application note &lt;A href="http://www.nxp.com/assets/documents/data/en/application-notes/AN4751.pdf"&gt;AN4751&lt;/A&gt; in order to know the recommended connection when not used.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: red;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12813i577B7483FF713BC2/image-size/large?v=v2&amp;amp;px=999" title="table1.jpg" alt="table1.jpg" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please let me know if this information helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jan 2017 18:41:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMPF0200-F6-SWBST-VGEN2/m-p/647282#M98879</guid>
      <dc:creator>david_diaz</dc:creator>
      <dc:date>2017-01-31T18:41:31Z</dc:date>
    </item>
    <item>
      <title>Re: MMPF0200 F6 - SWBST, VGEN2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0200-F6-SWBST-VGEN2/m-p/647283#M98880</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you, that answers my question!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Feb 2017 16:00:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMPF0200-F6-SWBST-VGEN2/m-p/647283#M98880</guid>
      <dc:creator>max123</dc:creator>
      <dc:date>2017-02-02T16:00:36Z</dc:date>
    </item>
  </channel>
</rss>