<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx6q uboot logo problem in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-uboot-logo-problem/m-p/646462#M98703</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've patched the patch logo。&lt;/P&gt;&lt;P&gt;bsp:uboot2009 linux-3.0.35.&lt;/P&gt;&lt;P&gt;Such as the picture should be displayed in the red box on the left side of the show, now displayed on the right side of the display, which is what causes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17233i2115E7226C592116/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.jpg" alt="pastedImage_3.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Apr 2017 10:28:05 GMT</pubDate>
    <dc:creator>yuhundehao</dc:creator>
    <dc:date>2017-04-26T10:28:05Z</dc:date>
    <item>
      <title>imx6q uboot logo problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-uboot-logo-problem/m-p/646462#M98703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've patched the patch logo。&lt;/P&gt;&lt;P&gt;bsp:uboot2009 linux-3.0.35.&lt;/P&gt;&lt;P&gt;Such as the picture should be displayed in the red box on the left side of the show, now displayed on the right side of the display, which is what causes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17233i2115E7226C592116/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.jpg" alt="pastedImage_3.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Apr 2017 10:28:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-uboot-logo-problem/m-p/646462#M98703</guid>
      <dc:creator>yuhundehao</dc:creator>
      <dc:date>2017-04-26T10:28:05Z</dc:date>
    </item>
    <item>
      <title>Re: imx6q uboot logo problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-uboot-logo-problem/m-p/646463#M98704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi yuhundehao&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please try uboot logo patches from&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://community.freescale.com/docs/DOC-98109" title="https://community.freescale.com/docs/DOC-98109"&gt;https://community.freescale.com/docs/DOC-98109&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Apr 2017 10:33:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-uboot-logo-problem/m-p/646463#M98704</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-04-26T10:33:06Z</dc:date>
    </item>
    <item>
      <title>Re: imx6q uboot logo problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-uboot-logo-problem/m-p/646464#M98705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do I have a problem with this &amp;nbsp;&lt;SPAN&gt;0001-Enable-uboot-logo-for-HDMI-LCD-and-LVDS.patch&lt;/SPAN&gt;?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Apr 2017 11:01:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-uboot-logo-problem/m-p/646464#M98705</guid>
      <dc:creator>yuhundehao</dc:creator>
      <dc:date>2017-04-26T11:01:43Z</dc:date>
    </item>
    <item>
      <title>Re: imx6q uboot logo problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-uboot-logo-problem/m-p/646465#M98706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;had you adjusted timings for custom lcd:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/373763"&gt;How to change SABRE-SD screen resolution in LOLLIPOP(5.0.0?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Apr 2017 11:23:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-uboot-logo-problem/m-p/646465#M98706</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-04-26T11:23:58Z</dc:date>
    </item>
    <item>
      <title>Re: imx6q uboot logo problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-uboot-logo-problem/m-p/646466#M98707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem has been solved for the following reasons：&lt;/P&gt;&lt;P&gt;&amp;lt;CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mmcblk0 bs=1 seek=6291456 skip=70"&amp;gt;Write Log&amp;lt;/CMD&amp;gt;&lt;/P&gt;&lt;P&gt;Skip patch requirements are 54, first changed to 70, up to the big demand。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jul 2017 01:24:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-uboot-logo-problem/m-p/646466#M98707</guid>
      <dc:creator>yuhundehao</dc:creator>
      <dc:date>2017-07-10T01:24:00Z</dc:date>
    </item>
  </channel>
</rss>