<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX25 SIM module stops working</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX25-SIM-module-stops-working/m-p/646300#M98661</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, my company has a product that uses the IMX25 with Linux 2.6.31-207-g7286c01&lt;BR /&gt;with some units we are having a problem that the SIM module just stops working.&lt;BR /&gt;It seems that no register configuration makes it work again, the only way to return operation, is by cutting the microprocessor battery power supply.&lt;BR /&gt;After that, when started again the SIM module will start to work.&lt;BR /&gt;I compared the SIM configuration registers of a board with the problem and a board where the SIM is working. In both, the registers values seems to be the same.&lt;BR /&gt;I also compared the signals, and found out that the clock and reset signal seems to be fine, but the data signal never goes up.&lt;BR /&gt;The 3Volt bit in the port control register is at 1 and the od_config for the SIM (port0) is also at 1.&lt;BR /&gt;So maybe is a GPIO configuration.&lt;BR /&gt;Searching in the kernel source code, i found that the pin is configured with these parameters&lt;BR /&gt;/* SIM1 TX */&lt;BR /&gt;{&lt;BR /&gt; MX25_PIN_CSI_D5, MUX_CONFIG_ALT4,&lt;BR /&gt; PAD_CTL_SRE_FAST |&lt;BR /&gt; PAD_CTL_DRV_HIGH | PAD_CTL_DRV_3_3V |&lt;BR /&gt; PAD_CTL_HYS_CMOS | PAD_CTL_22K_PU |&lt;BR /&gt; PAD_CTL_PUE_PULL | PAD_CTL_ODE_OpenDrain | PAD_CTL_PKE_ENABLE,&lt;BR /&gt; },&lt;/P&gt;&lt;P&gt;The thing is, nothing seems wrong. So is there any other configuration that could cause something like this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Lucas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Apr 2017 18:01:19 GMT</pubDate>
    <dc:creator>lucasgomes</dc:creator>
    <dc:date>2017-04-26T18:01:19Z</dc:date>
    <item>
      <title>IMX25 SIM module stops working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX25-SIM-module-stops-working/m-p/646300#M98661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, my company has a product that uses the IMX25 with Linux 2.6.31-207-g7286c01&lt;BR /&gt;with some units we are having a problem that the SIM module just stops working.&lt;BR /&gt;It seems that no register configuration makes it work again, the only way to return operation, is by cutting the microprocessor battery power supply.&lt;BR /&gt;After that, when started again the SIM module will start to work.&lt;BR /&gt;I compared the SIM configuration registers of a board with the problem and a board where the SIM is working. In both, the registers values seems to be the same.&lt;BR /&gt;I also compared the signals, and found out that the clock and reset signal seems to be fine, but the data signal never goes up.&lt;BR /&gt;The 3Volt bit in the port control register is at 1 and the od_config for the SIM (port0) is also at 1.&lt;BR /&gt;So maybe is a GPIO configuration.&lt;BR /&gt;Searching in the kernel source code, i found that the pin is configured with these parameters&lt;BR /&gt;/* SIM1 TX */&lt;BR /&gt;{&lt;BR /&gt; MX25_PIN_CSI_D5, MUX_CONFIG_ALT4,&lt;BR /&gt; PAD_CTL_SRE_FAST |&lt;BR /&gt; PAD_CTL_DRV_HIGH | PAD_CTL_DRV_3_3V |&lt;BR /&gt; PAD_CTL_HYS_CMOS | PAD_CTL_22K_PU |&lt;BR /&gt; PAD_CTL_PUE_PULL | PAD_CTL_ODE_OpenDrain | PAD_CTL_PKE_ENABLE,&lt;BR /&gt; },&lt;/P&gt;&lt;P&gt;The thing is, nothing seems wrong. So is there any other configuration that could cause something like this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Lucas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Apr 2017 18:01:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX25-SIM-module-stops-working/m-p/646300#M98661</guid>
      <dc:creator>lucasgomes</dc:creator>
      <dc:date>2017-04-26T18:01:19Z</dc:date>
    </item>
    <item>
      <title>Re: IMX25 SIM module stops working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX25-SIM-module-stops-working/m-p/646301#M98662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The issue mostly looks like not to be software-defined, but as some external effect like ESD, for example, or unstable supply voltage. Please check.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, does the issue occur only on selected units, or it can occur randomly on any unit? How often the issue occurs? Please check.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Apr 2017 09:59:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX25-SIM-module-stops-working/m-p/646301#M98662</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2017-04-30T09:59:26Z</dc:date>
    </item>
    <item>
      <title>Re: IMX25 SIM module stops working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX25-SIM-module-stops-working/m-p/646302#M98663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Artur, thanks for the answer, I will run some more tests. The problem seems to be random.&lt;/P&gt;&lt;P&gt;One thing that I noticed is&amp;nbsp;like I said, the problem is related to CSI_D5, so I tried using this pin as GPIO, but it simply doesnt work, i cant raise the pin signal if the test is running in a unit with the problem.&lt;/P&gt;&lt;P&gt;Anyway, I'll try to get some more info.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Lucas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 May 2017 17:33:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX25-SIM-module-stops-working/m-p/646302#M98663</guid>
      <dc:creator>lucasgomes</dc:creator>
      <dc:date>2017-05-03T17:33:19Z</dc:date>
    </item>
    <item>
      <title>Re: IMX25 SIM module stops working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX25-SIM-module-stops-working/m-p/646303#M98664</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok. We are trying to test for external effects like ESD or supply voltage. Is there any other factor that could cause something similar so that we can include in our tests?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Lucas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 May 2017 12:24:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX25-SIM-module-stops-working/m-p/646303#M98664</guid>
      <dc:creator>lucasgomes</dc:creator>
      <dc:date>2017-05-16T12:24:16Z</dc:date>
    </item>
  </channel>
</rss>