<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I need to trigger ENET_1588_EVENT2_OUT from the Freescale MAC to generate a 1PPS. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-need-to-trigger-ENET-1588-EVENT2-OUT-from-the-Freescale-MAC-to/m-p/646128#M98634</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to generate a 1PPS from the Freescale Ethernet chip.&amp;nbsp; I believe I can attach the ENET counter/timer interrupt to ENET_1588_EVENT2_OUT which is attached to Pad AD22 via the device tree (MX6QDL_PAD_ENET_RX_ER__ENET_1588_EVENT2_OUT).&amp;nbsp; The code I am looking at is /freescale/fec_ptp.c but I am unsure where to call the initialisation with the correct parameters or what code I may have to change or how to build the code into a Kernal Object (fec.ko).&amp;nbsp; The 1PPS must occur on the second boundary.&lt;/P&gt;&lt;P&gt;My goal is to measure the latency of this 1PPS output against an incoming 1PPS from a GPS. I am sure people have done this sort of thing before, probably on PTP projects like myself.&amp;nbsp; Any help would be appreciated to point me in the right direction.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Feb 2017 12:03:12 GMT</pubDate>
    <dc:creator>nxpcatt</dc:creator>
    <dc:date>2017-02-17T12:03:12Z</dc:date>
    <item>
      <title>I need to trigger ENET_1588_EVENT2_OUT from the Freescale MAC to generate a 1PPS.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-need-to-trigger-ENET-1588-EVENT2-OUT-from-the-Freescale-MAC-to/m-p/646128#M98634</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to generate a 1PPS from the Freescale Ethernet chip.&amp;nbsp; I believe I can attach the ENET counter/timer interrupt to ENET_1588_EVENT2_OUT which is attached to Pad AD22 via the device tree (MX6QDL_PAD_ENET_RX_ER__ENET_1588_EVENT2_OUT).&amp;nbsp; The code I am looking at is /freescale/fec_ptp.c but I am unsure where to call the initialisation with the correct parameters or what code I may have to change or how to build the code into a Kernal Object (fec.ko).&amp;nbsp; The 1PPS must occur on the second boundary.&lt;/P&gt;&lt;P&gt;My goal is to measure the latency of this 1PPS output against an incoming 1PPS from a GPS. I am sure people have done this sort of thing before, probably on PTP projects like myself.&amp;nbsp; Any help would be appreciated to point me in the right direction.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Feb 2017 12:03:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-need-to-trigger-ENET-1588-EVENT2-OUT-from-the-Freescale-MAC-to/m-p/646128#M98634</guid>
      <dc:creator>nxpcatt</dc:creator>
      <dc:date>2017-02-17T12:03:12Z</dc:date>
    </item>
  </channel>
</rss>