<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic use eim in userspace in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/use-eim-in-userspace/m-p/646019#M98604</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;yesterday i configured eim in our board to communicate with fpga, and use /unit_test/memtools （./memtools -16 0x0800000a=0x000f）tool to test it ,and i successfully read the &amp;nbsp;data(0x000f) in fpga , so eim is configured correctly. but i have a problem：how to use eim without memtools. i found in board_init function ，when configuring eim interface , i register a platform device (physmap-flash) into the system, and the resource of it is start with CS0_BASE_ADDR and end with CS0_BASE_ADDR+0x02000000-1 which is just the memory space of eim, so i check the /sys/devices/platform/physmap-flash.0 but there is no driver, &lt;STRONG&gt;does it mean if i want to use eim as a device, i have to write a driver for it? or nxp support the driver ,and i didn't find it？or there is other way to use it?&lt;/STRONG&gt; i have checked rm and firmware guide,and got nothing. i use imx6q-sabresd board and linux-3.0.35.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Thank you very much!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jay&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Oct 2016 13:59:37 GMT</pubDate>
    <dc:creator>vvjay</dc:creator>
    <dc:date>2016-10-18T13:59:37Z</dc:date>
    <item>
      <title>use eim in userspace</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/use-eim-in-userspace/m-p/646019#M98604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;yesterday i configured eim in our board to communicate with fpga, and use /unit_test/memtools （./memtools -16 0x0800000a=0x000f）tool to test it ,and i successfully read the &amp;nbsp;data(0x000f) in fpga , so eim is configured correctly. but i have a problem：how to use eim without memtools. i found in board_init function ，when configuring eim interface , i register a platform device (physmap-flash) into the system, and the resource of it is start with CS0_BASE_ADDR and end with CS0_BASE_ADDR+0x02000000-1 which is just the memory space of eim, so i check the /sys/devices/platform/physmap-flash.0 but there is no driver, &lt;STRONG&gt;does it mean if i want to use eim as a device, i have to write a driver for it? or nxp support the driver ,and i didn't find it？or there is other way to use it?&lt;/STRONG&gt; i have checked rm and firmware guide,and got nothing. i use imx6q-sabresd board and linux-3.0.35.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Thank you very much!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jay&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Oct 2016 13:59:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/use-eim-in-userspace/m-p/646019#M98604</guid>
      <dc:creator>vvjay</dc:creator>
      <dc:date>2016-10-18T13:59:37Z</dc:date>
    </item>
    <item>
      <title>Re: use eim in userspace</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/use-eim-in-userspace/m-p/646020#M98605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jay&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for available drivers please look at attached Linux Manual Chapter 26&lt;BR /&gt;SPI NOR Flash Memory Technology Device (MTD) Driver. Seems for custom&lt;/P&gt;&lt;P&gt;purposes one will have to write a driver for it and add sys/ entries using&lt;/P&gt;&lt;P&gt;approaches described in linux documents.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://stackoverflow.com/questions/16245100/how-to-create-a-simple-sysfs-class-attribute-in-linux-kernel-v3-2" title="http://stackoverflow.com/questions/16245100/how-to-create-a-simple-sysfs-class-attribute-in-linux-kernel-v3-2"&gt;c - How to create a simple sysfs class attribute in Linux kernel v3.2 - Stack Overflow&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Oct 2016 23:51:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/use-eim-in-userspace/m-p/646020#M98605</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-18T23:51:07Z</dc:date>
    </item>
  </channel>
</rss>