<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックAndroid / Boot device SATA can't use saveenv command under U-boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-Boot-device-SATA-can-t-use-saveenv-command-under-U-boot/m-p/645211#M98507</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I'm Using i.MX&lt;SPAN&gt;6Q&lt;/SPAN&gt; SabreSD board&amp;nbsp;with&amp;nbsp;&lt;SPAN style="font-size: 11.5pt; color: black; background: white;"&gt;Android (M6.0.1_2.1.0,4.1 kernel)&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Choosing SATA for Boot device , the problem is When using saveenv command under U-boot , can't save environmental variables into SATA , the console shows below :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; sata init&lt;BR /&gt;AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode&lt;BR /&gt;flags: ncq stag pm led clo only pmp pio slum part&lt;BR /&gt;SATA Device Info:&lt;BR /&gt;S/N: WD-WX41A156HFSS&lt;BR /&gt;Product model number: WDC WD5000LPVX-22V0TT0&lt;BR /&gt;Firmware version: 01.01A01&lt;BR /&gt;Capacity: 976773168 sectors&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; =&amp;gt; pri&lt;BR /&gt; baudrate=115200&lt;BR /&gt; bootdelay=1&lt;BR /&gt; ethact=FEC&lt;BR /&gt; ethaddr=00:04:9f:04:19:ad&lt;BR /&gt; ethprime=FEC&lt;BR /&gt; fdt_high=0xffffffff&lt;BR /&gt; initrd_high=0xffffffff&lt;BR /&gt; loadaddr=0x12000000&lt;BR /&gt; splashpos=m,m&lt;BR /&gt; stderr=serial&lt;BR /&gt; stdin=serial&lt;BR /&gt; stdout=serial&lt;BR /&gt; &lt;BR /&gt; =&amp;gt; setenv test TEST&lt;BR /&gt; =&amp;gt; saveenv &lt;BR /&gt; Saving Environment to MMC...&lt;BR /&gt; Writing to MMC(1)... failed &lt;BR /&gt; &lt;BR /&gt;Seems like i&lt;SPAN&gt;t &lt;/SPAN&gt;choose MMC1 (SD card) for saving the environmental variables, can't save environmental variables into SATA, is there any way to let variables stored into SATA ?&lt;BR /&gt; Please help / Thanks in advance &lt;BR /&gt; &lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Apr 2017 06:38:48 GMT</pubDate>
    <dc:creator>jackywu</dc:creator>
    <dc:date>2017-04-26T06:38:48Z</dc:date>
    <item>
      <title>Android / Boot device SATA can't use saveenv command under U-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Boot-device-SATA-can-t-use-saveenv-command-under-U-boot/m-p/645211#M98507</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I'm Using i.MX&lt;SPAN&gt;6Q&lt;/SPAN&gt; SabreSD board&amp;nbsp;with&amp;nbsp;&lt;SPAN style="font-size: 11.5pt; color: black; background: white;"&gt;Android (M6.0.1_2.1.0,4.1 kernel)&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Choosing SATA for Boot device , the problem is When using saveenv command under U-boot , can't save environmental variables into SATA , the console shows below :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; sata init&lt;BR /&gt;AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode&lt;BR /&gt;flags: ncq stag pm led clo only pmp pio slum part&lt;BR /&gt;SATA Device Info:&lt;BR /&gt;S/N: WD-WX41A156HFSS&lt;BR /&gt;Product model number: WDC WD5000LPVX-22V0TT0&lt;BR /&gt;Firmware version: 01.01A01&lt;BR /&gt;Capacity: 976773168 sectors&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; =&amp;gt; pri&lt;BR /&gt; baudrate=115200&lt;BR /&gt; bootdelay=1&lt;BR /&gt; ethact=FEC&lt;BR /&gt; ethaddr=00:04:9f:04:19:ad&lt;BR /&gt; ethprime=FEC&lt;BR /&gt; fdt_high=0xffffffff&lt;BR /&gt; initrd_high=0xffffffff&lt;BR /&gt; loadaddr=0x12000000&lt;BR /&gt; splashpos=m,m&lt;BR /&gt; stderr=serial&lt;BR /&gt; stdin=serial&lt;BR /&gt; stdout=serial&lt;BR /&gt; &lt;BR /&gt; =&amp;gt; setenv test TEST&lt;BR /&gt; =&amp;gt; saveenv &lt;BR /&gt; Saving Environment to MMC...&lt;BR /&gt; Writing to MMC(1)... failed &lt;BR /&gt; &lt;BR /&gt;Seems like i&lt;SPAN&gt;t &lt;/SPAN&gt;choose MMC1 (SD card) for saving the environmental variables, can't save environmental variables into SATA, is there any way to let variables stored into SATA ?&lt;BR /&gt; Please help / Thanks in advance &lt;BR /&gt; &lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Apr 2017 06:38:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Boot-device-SATA-can-t-use-saveenv-command-under-U-boot/m-p/645211#M98507</guid>
      <dc:creator>jackywu</dc:creator>
      <dc:date>2017-04-26T06:38:48Z</dc:date>
    </item>
    <item>
      <title>Re: Android / Boot device SATA can't use saveenv command under U-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Boot-device-SATA-can-t-use-saveenv-command-under-U-boot/m-p/645212#M98508</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;did you set the boot configure switch and set the partition correcly? for more detailed information, pls refer to the document as below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-328196"&gt;https://community.nxp.com/docs/DOC-328196&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 May 2017 08:02:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Boot-device-SATA-can-t-use-saveenv-command-under-U-boot/m-p/645212#M98508</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2017-05-03T08:02:39Z</dc:date>
    </item>
  </channel>
</rss>