<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX6 Watchdog Timer in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Watchdog-Timer/m-p/645061#M98487</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It appears from reading the Applications Processor Reference Manual for the i.MX6 Quad, that once the Watchdog Timer (WDOG) is enabled, it cannot be disabled until a POR has occurred.&amp;nbsp; Has anyone been successful in disabling the watchdog after it's been disabled, without going through a POR?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Apr 2017 20:29:13 GMT</pubDate>
    <dc:creator>morganbadgett</dc:creator>
    <dc:date>2017-04-26T20:29:13Z</dc:date>
    <item>
      <title>i.MX6 Watchdog Timer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Watchdog-Timer/m-p/645061#M98487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It appears from reading the Applications Processor Reference Manual for the i.MX6 Quad, that once the Watchdog Timer (WDOG) is enabled, it cannot be disabled until a POR has occurred.&amp;nbsp; Has anyone been successful in disabling the watchdog after it's been disabled, without going through a POR?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Apr 2017 20:29:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Watchdog-Timer/m-p/645061#M98487</guid>
      <dc:creator>morganbadgett</dc:creator>
      <dc:date>2017-04-26T20:29:13Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 Watchdog Timer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Watchdog-Timer/m-p/645062#M98488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no way to clear the Watchdog Enable (WDE) bit of the Watchdog Control Register (WCR) in software once it is set. Only the Power-On Reset or Watchdog Reset events can clear it.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Apr 2017 08:32:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Watchdog-Timer/m-p/645062#M98488</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2017-04-30T08:32:09Z</dc:date>
    </item>
  </channel>
</rss>