<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx6d fec buffer descriptor update incoherent in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6d-fec-buffer-descriptor-update-incoherent/m-p/645004#M98478</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Klaus, I will try to test&amp;nbsp;4.8 on a sabre quad and see if we can reproduce.&lt;/P&gt;&lt;P&gt;If it does come up on sabre it will be easier to debug.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sinan Akman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Sep 2016 16:18:49 GMT</pubDate>
    <dc:creator>sinanakman</dc:creator>
    <dc:date>2016-09-28T16:18:49Z</dc:date>
    <item>
      <title>imx6d fec buffer descriptor update incoherent</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6d-fec-buffer-descriptor-update-incoherent/m-p/645000#M98474</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using Linux 4.8-rc3 we have some trouble with fec ethernet on our imx6 board. Our driver instrumentation in fec_main.c shows that sporadically the BD_ENET_RX_EMPTY bit in the current receive buffer descriptor state word is kept set in case of a receive interrupt. On the next frame receptions the next buffer descriptors are updated correctly. After a few seconds the BD_ENET_RX_EMPTY bit disappears and the driver continues frame rx processing.&lt;BR /&gt;Also, for txing frames, BD_ENET_TX_READY is kept set but the frame is on wire. I think this is the cause for the kernel warning "NETDEV WATCHDOG: eth0 (fec): transmit queue 0 timed".&lt;BR /&gt;Any help would be greatly appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Sep 2016 05:41:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6d-fec-buffer-descriptor-update-incoherent/m-p/645000#M98474</guid>
      <dc:creator>goozle</dc:creator>
      <dc:date>2016-09-23T05:41:01Z</dc:date>
    </item>
    <item>
      <title>Re: imx6d fec buffer descriptor update incoherent</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6d-fec-buffer-descriptor-update-incoherent/m-p/645001#M98475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;It makes sense suggest to post the issue on linux mail list, since NXP does not officially &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;support 4.8 kernel. Supported BSPs are located on official web product page&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors/i.mx-software-and-tools:IMXSW_HOME" title="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors/i.mx-software-and-tools:IMXSW_HOME"&gt;i.MX Software and Tools|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Sep 2016 06:31:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6d-fec-buffer-descriptor-update-incoherent/m-p/645001#M98475</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-09-27T06:31:31Z</dc:date>
    </item>
    <item>
      <title>Re: imx6d fec buffer descriptor update incoherent</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6d-fec-buffer-descriptor-update-incoherent/m-p/645002#M98476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hallo Klaus, which imx6 SoC you are observing this with? I'd like test here to see if we can reproduce.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sinan Akman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Sep 2016 17:47:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6d-fec-buffer-descriptor-update-incoherent/m-p/645002#M98476</guid>
      <dc:creator>sinanakman</dc:creator>
      <dc:date>2016-09-27T17:47:25Z</dc:date>
    </item>
    <item>
      <title>Re: imx6d fec buffer descriptor update incoherent</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6d-fec-buffer-descriptor-update-incoherent/m-p/645003#M98477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sinan,&lt;BR /&gt;we observe that problem with an i.MX6D integrated on a DFI FS700 board. The SoC marking is&lt;/P&gt;&lt;P&gt;MCIMX6D5EYM10AC&lt;/P&gt;&lt;P&gt;SBDQ1350&lt;/P&gt;&lt;P&gt;KOREA ZXDQSBG&lt;/P&gt;&lt;P&gt;We did not observe the problem with an i.MX6 Solo.&lt;BR /&gt;Our test application is simple:&lt;/P&gt;&lt;P&gt;Every 5 ms a UDP frame is sent to the i.MX6D device. The&amp;nbsp;direct response of&amp;nbsp;the i.MX5D device is&amp;nbsp;a UDP Frame also. The UDP frames used have a length of 64 bytes. There is no other ethernet traffic and&amp;nbsp;no special CPU load, the system is almost idle.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Klaus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Sep 2016 05:45:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6d-fec-buffer-descriptor-update-incoherent/m-p/645003#M98477</guid>
      <dc:creator>goozle</dc:creator>
      <dc:date>2016-09-28T05:45:34Z</dc:date>
    </item>
    <item>
      <title>Re: imx6d fec buffer descriptor update incoherent</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6d-fec-buffer-descriptor-update-incoherent/m-p/645004#M98478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Klaus, I will try to test&amp;nbsp;4.8 on a sabre quad and see if we can reproduce.&lt;/P&gt;&lt;P&gt;If it does come up on sabre it will be easier to debug.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sinan Akman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Sep 2016 16:18:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6d-fec-buffer-descriptor-update-incoherent/m-p/645004#M98478</guid>
      <dc:creator>sinanakman</dc:creator>
      <dc:date>2016-09-28T16:18:49Z</dc:date>
    </item>
    <item>
      <title>Re: imx6d fec buffer descriptor update incoherent</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6d-fec-buffer-descriptor-update-incoherent/m-p/645005#M98479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'd like to inform you that setting the kernel configuration option CONFIG_DMA_CMA solves the problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Mar 2017 05:32:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6d-fec-buffer-descriptor-update-incoherent/m-p/645005#M98479</guid>
      <dc:creator>goozle</dc:creator>
      <dc:date>2017-03-09T05:32:59Z</dc:date>
    </item>
  </channel>
</rss>