<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX6 FCB block</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-FCB-block/m-p/644740#M98408</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What are the requirements on the OOB area when writing the FCB block? Can I write whatever I want in the OOB area associated with the FCB block or does it have to be empty?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Apr 2017 13:55:33 GMT</pubDate>
    <dc:creator>rickardandersso</dc:creator>
    <dc:date>2017-04-03T13:55:33Z</dc:date>
    <item>
      <title>IMX6 FCB block</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-FCB-block/m-p/644740#M98408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What are the requirements on the OOB area when writing the FCB block? Can I write whatever I want in the OOB area associated with the FCB block or does it have to be empty?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Apr 2017 13:55:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-FCB-block/m-p/644740#M98408</guid>
      <dc:creator>rickardandersso</dc:creator>
      <dc:date>2017-04-03T13:55:33Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 FCB block</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-FCB-block/m-p/644741#M98409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; It is highly recommended to use the kobs-ng utility for writing NAND FCB.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Please refer to MFG tool "NAND Flash" configuration in ucl2.xml &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Kong-ng is part of NXP Linux BSP.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Apr 2017 04:46:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-FCB-block/m-p/644741#M98409</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-04-05T04:46:57Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 FCB block</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-FCB-block/m-p/644742#M98410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I understand, but it would be really nice to know if I am allowed to put other information in the OOB area of the FCB block? Also do I really have to write the FCB block with raw write? Or can I write it with standard ECC?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Apr 2017 08:06:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-FCB-block/m-p/644742#M98410</guid>
      <dc:creator>rickardandersso</dc:creator>
      <dc:date>2017-04-05T08:06:51Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 FCB block</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-FCB-block/m-p/644743#M98411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; i.MX6 specifics are shown in section&amp;nbsp;8.5.2.5 (Bad Block Handling in the ROM)&lt;/P&gt;&lt;P&gt;of i.MX6 D/Q RM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Apr 2017 07:53:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-FCB-block/m-p/644743#M98411</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-04-28T07:53:28Z</dc:date>
    </item>
  </channel>
</rss>