<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SD_CD Pin in i.Mx7 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SD-CD-Pin-in-i-Mx7/m-p/644567#M98355</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The SD card is not detected in our board after power up. In our schematics, we have assigned the SD_CD pin to No Connect. We use the micro controller MCIMX7D7DVM10SC&lt;/P&gt;&lt;P&gt;But when we go in detail through the user manual its written, for embedded memory it should be tied to ground if not used. Will this cause an issue?&lt;/P&gt;&lt;P&gt;Kindly share your thoughts in this regard!!!!&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Regards,&lt;BR /&gt;Meria Jacob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Mar 2017 08:15:57 GMT</pubDate>
    <dc:creator>meriajacob</dc:creator>
    <dc:date>2017-03-13T08:15:57Z</dc:date>
    <item>
      <title>SD_CD Pin in i.Mx7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SD-CD-Pin-in-i-Mx7/m-p/644567#M98355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The SD card is not detected in our board after power up. In our schematics, we have assigned the SD_CD pin to No Connect. We use the micro controller MCIMX7D7DVM10SC&lt;/P&gt;&lt;P&gt;But when we go in detail through the user manual its written, for embedded memory it should be tied to ground if not used. Will this cause an issue?&lt;/P&gt;&lt;P&gt;Kindly share your thoughts in this regard!!!!&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Regards,&lt;BR /&gt;Meria Jacob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Mar 2017 08:15:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SD-CD-Pin-in-i-Mx7/m-p/644567#M98355</guid>
      <dc:creator>meriajacob</dc:creator>
      <dc:date>2017-03-13T08:15:57Z</dc:date>
    </item>
    <item>
      <title>Re: SD_CD Pin in i.Mx7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SD-CD-Pin-in-i-Mx7/m-p/644568#M98356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Meria,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, this is a problem if you do not have this pin in a low level,&amp;nbsp; it is never going to generate the proper interrupt event to detect the SD Card.&amp;nbsp; An option can be enable the pulldown resistor internally of the PAD.&amp;nbsp; and test.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jaime&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Mar 2017 18:12:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SD-CD-Pin-in-i-Mx7/m-p/644568#M98356</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2017-03-28T18:12:31Z</dc:date>
    </item>
  </channel>
</rss>